TIOVX User Guide
|
Internal APIs for utility operations.
Defines | |
#define | TIVX_ALIGN(value, align) ((((value)+((align)-1U))/(align))*(align)) |
Macro to align a 'value' to 'align' units. | |
#define | TIVX_FLOOR(value, align) (((value)/(align))*(align)) |
Macro to floor a 'value' to 'align' units. | |
#define | TIVX_DEFAULT_STRIDE_Y_ALIGN (16U) |
Macro to specify default alignment to use for stride in Y-direction. More... | |
#define | TIVX_TYPE_IS_SCALAR(type) (((vx_enum)VX_TYPE_INVALID < (type)) && ((type) < (vx_enum)VX_TYPE_SCALAR_MAX)) |
Used to determine if a type is a scalar. | |
#define | TIVX_TYPE_IS_STRUCT(type) (((type) >= (vx_enum)VX_TYPE_RECTANGLE) && ((type) < (vx_enum)VX_TYPE_KHRONOS_STRUCT_MAX)) |
Used to determine if a type is a struct. | |
#define | TIVX_TYPE_IS_OBJECT(type) (((type) >= (vx_enum)VX_TYPE_REFERENCE) && ((type) < (vx_enum)VX_TYPE_KHRONOS_OBJECT_END)) |
Used to determine if a type is an Khronos defined object. | |
#define | TIVX_TYPE_IS_TI_OBJECT(type) (((type) >= (vx_enum)VX_TYPE_VENDOR_OBJECT_START) && ((type) < (vx_enum)VX_TYPE_VENDOR_OBJECT_END)) |
Used to determine if a type is TI defined object. | |
#define | TIVX_MAGIC (0xFACEC0DEU) |
A magic value to look for and set in references. | |
#define | TIVX_BAD_MAGIC (42U) |
A magic value to look for and set in references. Used to indicate a free'ed reference. | |
#define | VX_CHECK_PARAM(ptr, size, type, align) ((NULL != ptr) && (size == sizeof(type)) && (((vx_size)ptr & align) == 0U)) |
A parameter checker for size and alignment. | |
Enumerations | |
enum | tivx_type_e { , TIVX_TYPE_ARRAY_MAP_INFO = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 1, TIVX_TYPE_IMAGE_MAP_INFO = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 2, TIVX_TYPE_RAW_IMAGE_MAP_INFO = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 3, TIVX_TYPE_TENSOR_MAP_INFO = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 4, TIVX_TYPE_USER_DATA_OBJECT_MAP_INFO = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 5, TIVX_TYPE_EVENT_QUEUE_ELEMENT = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 6, TIVX_TYPE_TARGET = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 7, TIVX_TYPE_TARGET_KERNEL_INSTANCE = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 8, TIVX_TYPE_TARGET_KERNEL = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 9, TIVX_TYPE_DELAY_PARAM = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 10, TIVX_TYPE_EVENT = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 11, TIVX_TYPE_UINTPTR = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 12, TIVX_TYPE_CONTEXT_USER_STRUCTS = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 13, TIVX_TYPE_GRAPH_PARAMETERS = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 14, TIVX_TYPE_DATA_REF_QUEUE_LIST = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 15, TIVX_TYPE_DELAY_DATA_REF_QUEUE_LIST = (vx_enum)VX_TYPE_VENDOR_STRUCT_START + 16 } |
TIVX defined reference types. More... | |
Functions | |
static void | tivx_uint32_to_uint64 (volatile uint64_t *val, uint32_t h, uint32_t l) |
Macro to convert 2x uint32 to uint64. | |
static void | tivx_uint64_to_uint32 (uint64_t val, volatile uint32_t *h, volatile uint32_t *l) |
Macro to convert uint64 to 2x uint32. | |
#define TIVX_DEFAULT_STRIDE_Y_ALIGN (16U) |
Macro to specify default alignment to use for stride in Y-direction.
HWA nodes require 16 byte alignment
Definition at line 105 of file vx_internal.h.
enum tivx_type_e |
TIVX defined reference types.
Enumerator | |
---|---|
TIVX_TYPE_ARRAY_MAP_INFO | Data reference queue type. |
TIVX_TYPE_IMAGE_MAP_INFO | A |
TIVX_TYPE_RAW_IMAGE_MAP_INFO | A |
TIVX_TYPE_TENSOR_MAP_INFO | A |
TIVX_TYPE_USER_DATA_OBJECT_MAP_INFO | A |
TIVX_TYPE_EVENT_QUEUE_ELEMENT | A |
TIVX_TYPE_TARGET | A |
TIVX_TYPE_TARGET_KERNEL_INSTANCE | A |
TIVX_TYPE_TARGET_KERNEL | |
TIVX_TYPE_DELAY_PARAM | |
TIVX_TYPE_EVENT | A |
TIVX_TYPE_UINTPTR | A |
TIVX_TYPE_CONTEXT_USER_STRUCTS | A |
TIVX_TYPE_GRAPH_PARAMETERS | A |
TIVX_TYPE_DATA_REF_QUEUE_LIST | A |
TIVX_TYPE_DELAY_DATA_REF_QUEUE_LIST | A |
Definition at line 140 of file vx_internal.h.