TIOVX User Guide

The configuration data structure used by the TIVX_KERNEL_VISS kernel. More...

#include <hwa_vpac_viss1.h>

Data Fields

uint32_t sensor_dcc_id
 
uint32_t use_case
 
uint32_t fcp1_config
 
tivx_vpac_viss_fcp_params_t fcp [TIVX_VPAC_VISS_FCP_NUM_INSTANCES]
 
uint32_t output_fcp_mapping [5]
 
uint32_t bypass_cac
 
uint32_t bypass_dwb
 
uint32_t bypass_nsf4
 
uint32_t bypass_glbce
 
uint32_t h3a_in
 
uint32_t h3a_aewb_af_mode
 
uint32_t enable_ctx
 
uint32_t channel_id
 
uint32_t enable_error_events
 
uint32_t enable_psa
 
uint32_t wdtimer_timeout_cycles
 
uint32_t enable_ir_op
 
uint32_t ir_output
 
uint32_t bypass_pcid
 

Detailed Description

The configuration data structure used by the TIVX_KERNEL_VISS kernel.

Definition at line 93 of file hwa_vpac_viss1.h.


The documentation for this struct was generated from the following files: