![]() |
TIOVX User Guide
|
The Flex Color Processing (FCP) data structure used in the tivx_vpac_viss_params_t structure for programming the TIVX_KERNEL_VISS kernel. More...
#include <hwa_vpac_viss_fcp.h>
Data Fields | |
| uint32_t | mux_output0 |
| uint32_t | mux_output1 |
| uint32_t | mux_output2 |
| uint32_t | mux_output3 |
| uint32_t | mux_output4 |
| uint32_t | ee_mode |
| uint32_t | chroma_mode |
The Flex Color Processing (FCP) data structure used in the tivx_vpac_viss_params_t structure for programming the TIVX_KERNEL_VISS kernel.
Below table provides output format supported on different outputs of each FCP unit in the VISS for the corresponding mux value in this structure.
| val | mux_output0 | mux_output1 | mux_output2 | mux_output3 | mux_output4 |
|---|---|---|---|---|---|
| 0 | Y12(P12/U16) | UV12(P12/U16) | Y8(U8) | UV8(P12/U16) | Invalid |
| 1 | Invalid | Invalid | R8(U8) | G8(U8) | B8(U8) |
| 2 | Invalid | C1(P12/U16) | C2(P12/U16) | C3(P12/U16) | C4(P12/U16) |
| 3 | Value(P12/U16) | Invalid | Value(U8) | Invalid | Saturation(U8) |
| 4 | NV12_P12 | Invalid | NV12 | Invalid | Invalid |
| 5 | Invalid | Invalid | YUV422 | Invalid | Invalid |
Definition at line 181 of file hwa_vpac_viss_fcp.h.
| uint32_t tivx_vpac_viss_fcp_params_t::mux_output0 |
Mux to select the output format for the output0 parameter of an FCP.
Valid values for this mux are:
| Enum | Description |
|---|---|
| TIVX_VPAC_VISS_MUX0_Y12 | Luma 12bit output either in U16 or P12 format |
| TIVX_VPAC_VISS_MUX0_VALUE12 | Value output form the HSV module either in U16 or P12 format |
| TIVX_VPAC_VISS_MUX0_NV12_P12 | NV12 output format in P12 format. |
Definition at line 194 of file hwa_vpac_viss_fcp.h.
| uint32_t tivx_vpac_viss_fcp_params_t::mux_output1 |
Mux to select the output format for the output1 parameter of an FCP.
Valid values for this mux are:
| Enum | Description |
|---|---|
| TIVX_VPAC_VISS_MUX1_UV12 | Chroma 12bit output either in U16 or P12 format |
| TIVX_VPAC_VISS_MUX1_C1 | C1 output from CFA either in U16 or P12 format |
Definition at line 206 of file hwa_vpac_viss_fcp.h.
| uint32_t tivx_vpac_viss_fcp_params_t::mux_output2 |
Mux to select the output format for the output2 parameter of an FCP.
Valid values for this mux are:
| Enum | Description |
|---|---|
| TIVX_VPAC_VISS_MUX2_Y8 | Luma in U8 format |
| TIVX_VPAC_VISS_MUX2_RED | Red color component in U8 format |
| TIVX_VPAC_VISS_MUX2_C2 | C2 output from CFA either in U16 or P12 format |
| TIVX_VPAC_VISS_MUX2_VALUE8 | Value output form the HSV module in U8 format |
| TIVX_VPAC_VISS_MUX2_NV12 | NV12 output format in 8bit format |
| TIVX_VPAC_VISS_MUX2_YUV422 | YUV422 interleaved in UYVY or YUYV format |
Definition at line 227 of file hwa_vpac_viss_fcp.h.
| uint32_t tivx_vpac_viss_fcp_params_t::mux_output3 |
Mux to select the output format for the output3 parameter of an FCP.
Valid values for this mux are:
| Enum | Description |
|---|---|
| TIVX_VPAC_VISS_MUX3_UV8 | Chroma in U8 format |
| TIVX_VPAC_VISS_MUX3_GREEN | Green color component in U8 format |
| TIVX_VPAC_VISS_MUX3_C3 | C3 output from CFA either in U16 or P12 format |
Definition at line 240 of file hwa_vpac_viss_fcp.h.
| uint32_t tivx_vpac_viss_fcp_params_t::mux_output4 |
Mux to select the output format for the output4 parameter of an FCP.
Valid values for this mux are:
| Enum | Description |
|---|---|
| TIVX_VPAC_VISS_MUX4_BLUE | Blue color component in U8 format |
| TIVX_VPAC_VISS_MUX4_C4 | C4 output from CFA either in U16 or P12 format |
| TIVX_VPAC_VISS_MUX4_SAT | Saturation from HSV module in U8 format |
Definition at line 251 of file hwa_vpac_viss_fcp.h.
| uint32_t tivx_vpac_viss_fcp_params_t::ee_mode |
Enables/Disables Edge Enhancer (EE) and also selects the Luma channel on which the EE to be enabled.
Valid values are
| Enum | Description |
|---|---|
| TIVX_VPAC_VISS_EE_MODE_OFF | Edge Enhancer is disabled |
| TIVX_VPAC_VISS_EE_MODE_FCP0_Y12 | Edge Enhancer is enabled on Y12 output (output0) |
| TIVX_VPAC_VISS_EE_MODE_FCP0_Y8 | Edge Enhancer is enabled on Y8 output (output2) |
Definition at line 263 of file hwa_vpac_viss_fcp.h.
| uint32_t tivx_vpac_viss_fcp_params_t::chroma_mode |
Selects the chroma output format, when chroma only output is selected in mux_output1 or mux_output3.
Valid Values are
| Enum | Description |
|---|---|
| TIVX_VPAC_VISS_CHROMA_MODE_420 | 420 Mode |
| TIVX_VPAC_VISS_CHROMA_MODE_422 | 422 Mode |
Definition at line 281 of file hwa_vpac_viss_fcp.h.