TIOVX User Guide
|
TI Vendor Extension Kernels.
The Khronos specification includes a list of supported kernels. This section lists the additional kernels TI has added.
Modules | |
TIDL (TI Deep Learning) Kernel APIs | |
TIDL Network Kernels. | |
TI VPAC NF (Noise filter) Kernel APIs | |
VPAC Noise Filter Kernels. | |
TI VPAC MSC (Multi-scaler) Kernel APIs | |
VPAC Multi-scaler Kernels. | |
TI VPAC VISS (Vision Imaging Sub System) Kernel APIs | |
VPAC Vision Imaging Sub System Kernels. | |
TI VPAC LDC (Lens Distortion Correction) Kernel APIs | |
VPAC Lens Distortion Correction Kernels. | |
TI DMPAC DOF (Dense Optical Flow) Kernel APIs | |
DMPAC Dense Optical Flow Kernels. | |
TI DMPAC SDE (Stereo Disparity Engine) Kernel APIs | |
DMPAC Stereo Disparity Engine Kernels. | |
TI Capture Kernel APIs | |
Capture (Source Node) Kernels. | |
TI Display Kernel APIs | |
Display (Sink Node) Kernels. | |
TI Video Decoder Kernel APIs | |
Video Decoder Kernels. | |
TI Video Encoder Kernel APIs | |
Video Encoder Kernels. | |
TI CSITX Kernel APIs | |
CSITX (Sink Node) Kernels. | |
TI Display M2M Kernel APIs | |
Display M2M Kernels. | |
TVM (Tensor Virtual Machine) Kernel APIs | |
TVM Network Kernels. | |
Defines | |
#define | TIVX_KERNEL_OBJ_ARRAY_SPLIT_NAME "com.ti.hwa.obj_array_split" |
Object Array Split Kernel Name. | |
Functions | |
void | tivxHwaLoadKernels (vx_context context) |
Used for the Application to load the hwa kernels into the context. More... | |
void | tivxHwaUnLoadKernels (vx_context context) |
Used for the Application to unload the hwa kernels from the context. More... | |
void | tivxTIDLLoadKernels (vx_context context) |
Used for the Application to load the tidl kernels into the context. | |
void | tivxTIDLUnLoadKernels (vx_context context) |
Used for the Application to unload the tidl kernels from the context. | |
void tivxHwaLoadKernels | ( | vx_context | context | ) |
Used for the Application to load the hwa kernels into the context.
End of group_vision_function_hwa
This includes Capture, Display, VPAC, and DMPAC kernels
void tivxHwaUnLoadKernels | ( | vx_context | context | ) |
Used for the Application to unload the hwa kernels from the context.
This includes Capture, Display, VPAC, and DMPAC kernels