![]() |
TIOVX User Guide
|
CSITX (Sink Node) Kernels.
Data Structures | |
| struct | tivx_csitx_inst_params_t |
| The CSITX DRV instance configuration data structure used by the TIVX_KERNEL_CSITX kernel. More... | |
| struct | tivx_csitx_params_t |
| The configuration data structure used by the TIVX_KERNEL_CSITX kernel. More... | |
| struct | tivx_csitx_statistics_t |
| Csitx status structure used to get the current status. More... | |
Defines | |
| #define | TIVX_KERNEL_CSITX_NAME "com.ti.csitx" |
| csitx kernel name | |
| #define | TIVX_CSITX_PRINT_STATISTICS (0x40000000u) |
| Control Command to print csitx statistics No argument is needed to query statistics. | |
| #define | TIVX_CSITX_GET_STATISTICS (0x40000001u) |
| Control Command to return csitx statistics to application. More... | |
| #define | TIVX_CSITX_MAX_CH (4U) |
| Maximum number of channels supported in the csitx node. | |
| #define | TIVX_CSITX_MAX_INST (1U) |
| Maximum number of instances supported in the csitx node. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_80_TO_100_MBPS ((uint32_t) 0x00U) |
| Lane Band Speed: 80 Mbps to 100 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_100_TO_120_MBPS ((uint32_t) 0x01U) |
| Lane Band Speed: 100 Mbps to 120 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_120_TO_160_MBPS ((uint32_t) 0x02U) |
| Lane Band Speed: 120 Mbps to 160 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_160_TO_200_MBPS ((uint32_t) 0x03U) |
| Lane Band Speed: 160 Mbps to 200 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_200_TO_240_MBPS ((uint32_t) 0x04U) |
| Lane Band Speed: 200 Mbps to 240 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_240_TO_320_MBPS ((uint32_t) 0x05U) |
| Lane Band Speed: 240 Mbps to 320 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_320_TO_390_MBPS ((uint32_t) 0x06U) |
| Lane Band Speed: 320 Mbps to 390 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_390_TO_450_MBPS ((uint32_t) 0x07U) |
| Lane Band Speed: 390 Mbps to 450 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_450_TO_510_MBPS ((uint32_t) 0x08U) |
| Lane Band Speed: 450 Mbps to 510 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_510_TO_560_MBPS ((uint32_t) 0x09U) |
| Lane Band Speed: 510 Mbps to 560 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_560_TO_640_MBPS ((uint32_t) 0x0AU) |
| Lane Band Speed: 560 Mbps to 640 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_640_TO_690_MBPS ((uint32_t) 0x0BU) |
| Lane Band Speed: 640 Mbps to 690 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_690_TO_770_MBPS ((uint32_t) 0x0CU) |
| Lane Band Speed: 690 Mbps to 770 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_770_TO_870_MBPS ((uint32_t) 0x0DU) |
| Lane Band Speed: 770 Mbps to 870 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_870_TO_950_MBPS ((uint32_t) 0x0EU) |
| Lane Band Speed: 870 Mbps to 950 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_950_TO_1000_MBPS ((uint32_t) 0x0FU) |
| Lane Band Speed: 950 Mbps to 1000 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_1000_TO_1200_MBPS ((uint32_t) 0x10U) |
| Lane Band Speed: 1000 Mbps to 1200 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_1200_TO_1400_MBPS ((uint32_t) 0x11U) |
| Lane Band Speed: 1200 Mbps to 1400 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_1400_TO_1600_MBPS ((uint32_t) 0x12U) |
| Lane Band Speed: 1400 Mbps to 1600 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_1600_TO_1800_MBPS ((uint32_t) 0x13U) |
| Lane Band Speed: 1600 Mbps to 1800 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_1800_TO_2000_MBPS ((uint32_t) 0x14U) |
| Lane Band Speed: 1800 Mbps to 2000 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_2000_TO_2200_MBPS ((uint32_t) 0x15U) |
| Lane Band Speed: 2000 Mbps to 2200 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_2200_TO_2500_MBPS ((uint32_t) 0x16U) |
| Lane Band Speed: 2200 Mbps to 2500 Mbps. | |
| #define | TIVX_CSITX_LANE_BAND_SPEED_RESERVED ((uint32_t) 0x17U) |
| Lane Band Speed: Reserved. | |
| #define | TIVX_CSITX_LANE_SPEED_MBPS_RESERVED ((uint32_t) 0xFFFFFFFFU) |
| Lane Speed: Reserved. | |
Functions | |
| VX_API_ENTRY vx_node VX_API_CALL | tivxCsitxNode (vx_graph graph, vx_user_data_object configuration, vx_object_array input) |
| [Graph] Creates a CSI Tx node. More... | |
| void | tivx_csitx_params_init (tivx_csitx_params_t *prms) |
| Function to initialize Csitx Parameters. More... | |
| #define TIVX_CSITX_GET_STATISTICS (0x40000001u) |
Control Command to return csitx statistics to application.
This control command returns the status of the csitx node. Please refer to tivx_csitx_statistics_t structure.
Definition at line 102 of file j7_csitx.h.
| VX_API_ENTRY vx_node VX_API_CALL tivxCsitxNode | ( | vx_graph | graph, |
| vx_user_data_object | configuration, | ||
| vx_object_array | input | ||
| ) |
[Graph] Creates a CSI Tx node.
The csitx node takes in a user data object of type tivx_csitx_params_t to configure one or more csitx channels.The input must be of type vx_object_array, which contain an array of either vx_image or tivx_raw_image data types. vx_image is used for transmitting processed image formats, while tivx_raw_image is used for raw sensor outputs.
| [in] | graph | The reference to the graph. |
| [in] | configuration | The input user data object of a single csitx params structure of type tivx_csitx_params_t. |
| [in] | input | Object array input which has been created from an exemplar of either vx_image or tivx_raw_image. If using vx_image, the image type MUST be one of the following formats: VX_DF_IMAGE_RGBX, VX_DF_IMAGE_U16, VX_DF_IMAGE_UYVY or VX_DF_IMAGE_YUYV. |
TIVX_KERNEL_CSITX_NAMEvx_node. | vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
| void tivx_csitx_params_init | ( | tivx_csitx_params_t * | prms | ) |
Function to initialize Csitx Parameters.
| prms | [in] Pointer to csitx params configuration structure |