TIOVX User Guide
|
VPAC Lens Distortion Correction Kernels.
Modules | |
Enumerations | |
Enumerations for configuration parameters in VPAC LDC structures. | |
Data Structures | |
struct | tivx_vpac_ldc_region_params_t |
The region_params data structure used by the TIVX_KERNEL_VPAC_LDC kernel. More... | |
struct | tivx_vpac_ldc_multi_region_params_t |
The alternative region_params data structure used by the TIVX_KERNEL_VPAC_LDC kernel. More... | |
struct | tivx_vpac_ldc_mesh_params_t |
The mesh data structure in the configuration data structure used by the TIVX_KERNEL_VPAC_LDC kernel. More... | |
struct | tivx_vpac_ldc_params_t |
The configuration data structure used by the TIVX_KERNEL_VPAC_LDC kernel. More... | |
struct | tivx_vpac_ldc_bandwidth_params_t |
The bandwidth params structure used by the TIVX_KERNEL_VPAC_LDC kernel. Passed as argument to TIVX_VPAC_LDC_CMD_SET_READ_BW_LIMIT_PARAMS command. More... | |
struct | tivx_vpac_ldc_bit_depth_conv_lut_params_t |
The remap params structure used by the TIVX_KERNEL_VPAC_LDC kernel. Passed as argument to TIVX_VPAC_LDC_CMD_SET_BIT_DEPTH_CONV_LUT_PARAMS command. Used to set Remap/Tone Map Lut in LDC. More... | |
Defines | |
#define | TIVX_KERNEL_VPAC_LDC_NAME "com.ti.hwa.vpac_ldc" |
vpac_ldc kernel name | |
#define | TIVX_VPAC_LDC_CMD_SET_READ_BW_LIMIT_PARAMS (0x10000000u) |
Control Command to set LDC Read Bandwidth limit parameters User data object tivx_vpac_ldc_bandwidth_params_t is passed as argument with this control command. | |
#define | TIVX_VPAC_LDC_CMD_SET_BIT_DEPTH_CONV_LUT_PARAMS (0x10000001u) |
Control Command to set LDC Lut parameters This LUT is used in bit depth conversion for output 2 & 3. An array of tivx_vpac_ldc_bit_depth_conv_lut_params_t is used an an argument to this command. Params at index-0 is used for setting Luma output (output2) and Params at index-1 is used for setting Chroma output (output3). Both entries are optional and can be null if no change is required. | |
#define | TIVX_VPAC_LDC_CMD_GET_ERR_STATUS (0x10000002u) |
Control Command to get the error status Returns the error status of the last processed frame. Reference to vx_scalar is passed as argument with this control command. Node returns bit-mask of error status in u32 variable of vx_scalar. | |
#define | TIVX_VPAC_LDC_CMD_SET_LDC_PARAMS (0x10000003u) |
Control Command to set the LDC Parameters. More... | |
#define | TIVX_VPAC_LDC_CMD_SET_LDC_DCC_PARAMS (0x30000000u) |
Control Command to set the DCC (Dynamic Camera Configuration) information to the given LDC Node. More... | |
#define | TIVX_VPAC_LDC_CALC_MESH_LINE_OFFSET(width, subsample_factor) ((((((width)/(subsample_factor))+1) + 15U) & ~15U) * (4U)) |
Macro to calculate mesh line offset for the given width and down scaling factor. | |
Functions | |
void | tivxRegisterHwaTargetVpacLdcKernels (void) |
Function to register HWA Kernels on the vpac_ldc Target. | |
void | tivxUnRegisterHwaTargetVpacLdcKernels (void) |
Function to un-register HWA Kernels on the vpac_ldc Target. | |
VX_API_ENTRY vx_node VX_API_CALL | tivxVpacLdcNode (vx_graph graph, vx_user_data_object configuration, vx_matrix warp_matrix, vx_user_data_object region_prms, vx_user_data_object mesh_prms, vx_image mesh_img, vx_user_data_object dcc_db, vx_image in_img, vx_image out0_img, vx_image out1_img) |
[Graph] Creates a VPAC_LDC Node. More... | |
void | tivx_vpac_ldc_region_params_init (tivx_vpac_ldc_region_params_t *prms) |
Function to initialize LDC Region parameters. More... | |
void | tivx_vpac_ldc_multi_region_params_init (tivx_vpac_ldc_multi_region_params_t *prms) |
Function to initialize LDC Multi Region parameters. More... | |
void | tivx_vpac_ldc_mesh_params_init (tivx_vpac_ldc_mesh_params_t *prms) |
Function to initialize LDC Mesh parameters. More... | |
void | tivx_vpac_ldc_bandwidth_params_init (tivx_vpac_ldc_bandwidth_params_t *prms) |
Function to initialize Bandwidth limiter parameters. More... | |
void | tivx_vpac_ldc_params_init (tivx_vpac_ldc_params_t *prms) |
Function to initialize LDC parameters with the default values. More... | |
#define TIVX_VPAC_LDC_CMD_SET_LDC_PARAMS (0x10000003u) |
Control Command to set the LDC Parameters.
This command takes an array of vx_references as an argument, where each index contains a reference to a parameter to update.
The following are the supported paramters: index 0 : vx_matrix reference for updating warp matrix.
Definition at line 130 of file j7_vpac_ldc.h.
#define TIVX_VPAC_LDC_CMD_SET_LDC_DCC_PARAMS (0x30000000u) |
Control Command to set the DCC (Dynamic Camera Configuration) information to the given LDC Node.
Ldc node gets the pointer to DCC buffer containing LDC configuration. It uses DCC parser to parse and map DCC parameters into LDC configuration and sets it in the driver.
User data object containing DCC buffer is passed as argument with this control command.
The ID of this command must be the same as TIVX_VPAC_VISS_CMD_SET_DCC_PARAMS
Definition at line 147 of file j7_vpac_ldc.h.
VX_API_ENTRY vx_node VX_API_CALL tivxVpacLdcNode | ( | vx_graph | graph, |
vx_user_data_object | configuration, | ||
vx_matrix | warp_matrix, | ||
vx_user_data_object | region_prms, | ||
vx_user_data_object | mesh_prms, | ||
vx_image | mesh_img, | ||
vx_user_data_object | dcc_db, | ||
vx_image | in_img, | ||
vx_image | out0_img, | ||
vx_image | out1_img | ||
) |
[Graph] Creates a VPAC_LDC Node.
Valid input/output format combinations:
Input Format | Output Format |
---|---|
VX_DF_IMAGE_U8 | VX_DF_IMAGE_U8 |
TIVX_DF_IMAGE_P12 | |
VX_DF_IMAGE_U16 | VX_DF_IMAGE_U16 |
TIVX_DF_IMAGE_P12 | TIVX_DF_IMAGE_P12 |
VX_DF_IMAGE_U8 | |
VX_DF_IMAGE_NV12 | VX_DF_IMAGE_NV12 |
TIVX_DF_IMAGE_NV12_P12 | |
TIVX_DF_IMAGE_NV12_P12 | TIVX_DF_IMAGE_NV12_P12 |
VX_DF_IMAGE_NV12 | |
VX_DF_IMAGE_UYVY | VX_DF_IMAGE_UYVY |
VX_DF_IMAGE_YUYV | |
VX_DF_IMAGE_NV12 | |
TIVX_DF_IMAGE_NV12_P12 |
[in] | graph | The reference to the graph. |
[in] | configuration | The input object of a single params structure of type tivx_vpac_ldc_params_t . |
[in] | warp_matrix | (optional) Input warp_matrix of type vx_matrix for affine or perspective transform configuration. Must be 2x3 (affine) or 3x3 (perspective), and of type VX_TYPE_INT16 if using HW register values, or VX_TYPE_FLOAT32 if using matrix values defined in OpenVX warp functions ( vxWarpAffineNode, vxWarpPerspectiveNode). |
[in] | region_prms | (optional) The input object of a single params structure of type tivx_vpac_ldc_region_params_t or tivx_vpac_ldc_multi_region_params_t . If set to null, default block size (TIVX_VPAC_LDC_DEF_BLOCK_WIDTH x TIVX_VPAC_LDC_DEF_BLOCK_HEIGHT) and pixel padding (TIVX_VPAC_LDC_DEF_PIXEL_PAD) is used. |
[in] | mesh_prms | (optional) Mesh Configuration, the input object of type tivx_vpac_ldc_mesh_params_t . It is used to provide frame size and downsampling factor of mesh_img. If set to null, back mapping is disabled. |
[in] | mesh_img | (optional) Mesh image containing mesh 2D coordinate offset lookup table. This can be a full remap table per output pixel, but is typically sub-sampled by a power of 2 as per tivx_vpac_ldc_mesh_params_t.subsample_factor to save memory footprint and bandwidth. The pitch/line offset for the mesh can be calculated using TIVX_VPAC_LDC_CALC_MESH_LINE_OFFSET. The coordinate offsets are of type S16Q3, and are stored as X,Y pairs of type VX_DF_IMAGE_U32 .
|
[in] | dcc_db | (optional) DCC tuning database for the given sensor vx_user_data_object |
[in] | in_img | The input image in VX_DF_IMAGE_NV12 , TIVX_DF_IMAGE_NV12_P12 , VX_DF_IMAGE_UYVY , VX_DF_IMAGE_U8 (8bit Luma only), VX_DF_IMAGE_U16 (12bit in 16bit container Luma only), or TIVX_DF_IMAGE_P12 (12bit packed Luma only) format. |
[out] | out0_img | The output image in VX_DF_IMAGE_NV12 , TIVX_DF_IMAGE_NV12_P12 , VX_DF_IMAGE_UYVY , VX_DF_IMAGE_YUYV , VX_DF_IMAGE_U8 (8bit Luma only), VX_DF_IMAGE_U16 (12bit in 16bit container Luma only), or TIVX_DF_IMAGE_P12 (12bit packed Luma only) format. |
[out] | out1_img | (optional) The output image in VX_DF_IMAGE_NV12 , VX_DF_IMAGE_UYVY , VX_DF_IMAGE_YUYV , VX_DF_IMAGE_U8 (8bit Luma only) format. |
TIVX_KERNEL_VPAC_LDC_NAME
vx_node
.vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
void tivx_vpac_ldc_region_params_init | ( | tivx_vpac_ldc_region_params_t * | prms | ) |
Function to initialize LDC Region parameters.
prms | [IN] Pointer to LDC region parameter structure |
void tivx_vpac_ldc_multi_region_params_init | ( | tivx_vpac_ldc_multi_region_params_t * | prms | ) |
Function to initialize LDC Multi Region parameters.
prms | [IN] Pointer to LDC multi region parameter structure |
void tivx_vpac_ldc_mesh_params_init | ( | tivx_vpac_ldc_mesh_params_t * | prms | ) |
Function to initialize LDC Mesh parameters.
prms | [IN] Pointer to LDC mesh parameter structure |
void tivx_vpac_ldc_bandwidth_params_init | ( | tivx_vpac_ldc_bandwidth_params_t * | prms | ) |
Function to initialize Bandwidth limiter parameters.
prms | [IN] Pointer to LDC bandwidth limiter parameter structure |
void tivx_vpac_ldc_params_init | ( | tivx_vpac_ldc_params_t * | prms | ) |
Function to initialize LDC parameters with the default values.
prms | [IN] Pointer to LDC parameter structure |