TIOVX User Guide
|
Display M2M Kernels.
Data Structures | |
struct | tivx_display_m2m_params_t |
The configuration data structure used by the TIVX_KERNEL_DISPLAY_M2M kernel. More... | |
struct | tivx_display_m2m_statistics_t |
Display M2M status structure used to get the current status. More... | |
Defines | |
#define | TIVX_KERNEL_DISPLAY_M2M_NAME "com.ti.hwa.displaym2m" |
Display M2M kernel name. | |
#define | TIVX_DISPLAY_M2M_GET_STATISTICS (0x40000001u) |
Control Command to return Display M2M statistics to application. More... | |
#define | TIVX_DISPLAY_M2M_MAX_PIPE (1U) |
Maximum number of display pipe-line supported in the DSS M2M node. Multiple number of pipe-lines are needed to support blending. | |
Functions | |
VX_API_ENTRY vx_node VX_API_CALL | tivxDisplayM2MNode (vx_graph graph, vx_user_data_object configuration, vx_image input, vx_image output) |
[Graph] Creates a DISPLAY_M2M Node. This node can be used to do color space conversion like YUV422 to YUV420 OR RGB888 to YUV420 and vice versa. This node operates in Memory to Memory mode. More... | |
void | tivx_display_m2m_params_init (tivx_display_m2m_params_t *prms) |
Function to initialize Display M2M Parameters. More... | |
#define TIVX_DISPLAY_M2M_GET_STATISTICS (0x40000001u) |
Control Command to return Display M2M statistics to application.
This control command returns the status of the Display M2M node. Please refer to tivx_display_m2m_statistics_t structure.
Definition at line 92 of file j7_display_m2m.h.
VX_API_ENTRY vx_node VX_API_CALL tivxDisplayM2MNode | ( | vx_graph | graph, |
vx_user_data_object | configuration, | ||
vx_image | input, | ||
vx_image | output | ||
) |
[Graph] Creates a DISPLAY_M2M Node. This node can be used to do color space conversion like YUV422 to YUV420 OR RGB888 to YUV420 and vice versa. This node operates in Memory to Memory mode.
[in] | graph | The reference to the graph. |
[in] | configuration | |
[in] | input | |
[out] | output |
TIVX_KERNEL_DISPLAY_M2M_NAME
vx_node
. vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
void tivx_display_m2m_params_init | ( | tivx_display_m2m_params_t * | prms | ) |
Function to initialize Display M2M Parameters.
prms | [in] Pointer to display M2M params configuration structure |