![]() |
PDK API Guide for J721E
|
Go to the source code of this file.
Data Structures | |
struct | tisci_msg_set_clock_req |
Mark a clock as required/not required. More... | |
struct | tisci_msg_set_clock_resp |
Empty response for TISCI_MSG_SET_CLOCK. More... | |
struct | tisci_msg_get_clock_req |
Get the current state of a clock. More... | |
struct | tisci_msg_get_clock_resp |
Clock state response. More... | |
struct | tisci_msg_set_clock_parent_req |
Set the clock parent. More... | |
struct | tisci_msg_set_clock_parent_resp |
Empty response for TISCI_MSG_SET_CLOCK_PARENT. More... | |
struct | tisci_msg_get_clock_parent_req |
Return the current clock parent. More... | |
struct | tisci_msg_get_clock_parent_resp |
Clock parent response. More... | |
struct | tisci_msg_get_num_clock_parents_req |
Return the number of possible parents for a clock. More... | |
struct | tisci_msg_get_num_clock_parents_resp |
Num clock parents response. More... | |
struct | tisci_msg_set_freq_req |
Set the desired frequency for a clock. More... | |
struct | tisci_msg_set_freq_resp |
Empty response for TISCI_MSG_SET_FREQ. More... | |
struct | tisci_msg_query_freq_req |
Determine the result of a hypothetical set frequency operation. More... | |
struct | tisci_msg_query_freq_resp |
Result of a query operation. More... | |
struct | tisci_msg_get_freq_req |
Get the current frequency of a device's clock. More... | |
struct | tisci_msg_get_freq_resp |
Result of get frequency request. More... | |
Macros | |
#define | TISCI_MSG_VALUE_CLOCK_SW_STATE_UNREQ 0 |
This file contains: More... | |
#define | TISCI_MSG_VALUE_CLOCK_SW_STATE_AUTO 1 |
#define | TISCI_MSG_VALUE_CLOCK_SW_STATE_REQ 2 |
#define | TISCI_MSG_VALUE_CLOCK_HW_STATE_NOT_READY 0 |
#define | TISCI_MSG_VALUE_CLOCK_HW_STATE_READY 1 |
#define | TISCI_MSG_FLAG_CLOCK_ALLOW_SSC TISCI_BIT(8) |
#define | TISCI_MSG_FLAG_CLOCK_ALLOW_FREQ_CHANGE TISCI_BIT(9) |
#define | TISCI_MSG_FLAG_CLOCK_INPUT_TERM TISCI_BIT(10) |
#define | TISCI_MSG_FLAG_CLOCK_SSC_ACTIVE TISCI_BIT(11) |
Functions | |
struct tisci_msg_set_clock_req | __attribute__ ((__packed__)) |
Variables | |
struct tisci_header | hdr |
uint32_t | device |
uint8_t | clk |
uint8_t | state |
uint32_t | clk32 |
uint8_t | programmed_state |
uint8_t | current_state |
uint8_t | parent |
uint32_t | parent32 |
uint8_t | num_parents |
uint32_t | num_parentint32_t |
uint64_t | min_freq_hz |
uint64_t | target_freq_hz |
uint64_t | max_freq_hz |
uint64_t | freq_hz |
struct tisci_header hdr |
uint32_t device |
uint8_t clk |
uint8_t state |
uint32_t clk32 |
uint8_t programmed_state |
uint8_t current_state |
uint8_t parent |
uint32_t parent32 |
uint8_t num_parents |
uint32_t num_parentint32_t |
uint64_t min_freq_hz |
uint64_t target_freq_hz |
uint64_t max_freq_hz |
uint64_t freq_hz |