PDK API Guide for J721E
tisci_msg_get_clock_parent_req Struct Reference

Detailed Description

Return the current clock parent.

If the hardware value indicating the current clock parent contains a reserved value, a NAK is returned for this message. Once a valid parent is programmed via a successful SET_CLOCK_PARENT call, calls to GET_CLOCK_PARENT will succeed.

Parameters
hdrTISCI header
deviceThe device ID that the clock is connected to.
clkEach device has its own set of clock inputs. This indexes which clock input to get.

If the clock index is 255 or greater, this field should be set to 255 and the full value placed in the clk32 field. This is kept for backwards compatibility with older firmwares.

Parameters
clk32Stores the actual clock index if clk field is set to 255. This field is ignored otherwise. This field can hold the full range of possible clock indexes, but for compatibility with older firmwares should only be used when the index is 255 or greater.

Data Fields

struct tisci_header hdr
 
uint32_t device
 
uint8_t clk
 
uint32_t clk32
 

Field Documentation

◆ hdr

struct tisci_header tisci_msg_get_clock_parent_req::hdr

◆ device

uint32_t tisci_msg_get_clock_parent_req::device

◆ clk

uint8_t tisci_msg_get_clock_parent_req::clk

◆ clk32

uint32_t tisci_msg_get_clock_parent_req::clk32