![]() |
PDK API Guide for J721E
|
Clock parent response.
hdr | TISCI header |
parent | The current clock parent. |
If the parent clock index is 255 or greater, this field will be set to 255 and the full value placed in the parent32 field. This is for backwards compatibility with older firmwares.
parent32 | Parent Clock index if 255 or greater and parent field is set to 255. This field will contain 0xFFFFFFFF otherwise. |
Data Fields | |
struct tisci_header | hdr |
uint8_t | parent |
uint32_t | parent32 |
struct tisci_header tisci_msg_get_clock_parent_resp::hdr |
uint8_t tisci_msg_get_clock_parent_resp::parent |
uint32_t tisci_msg_get_clock_parent_resp::parent32 |