This is VISS NSF4 Configuration file
|
file | nsf4_cfg.h |
| Interface file for NSF4 module, Defines the structures / control operations that could be used to configure / control NSF4 module in VISS NSF4 is independent module, between RAW FE and FCFA. This is why a separate interface file is used for controlling NSF4.
|
|
◆ IOCTL_NSF4_GET_CONFIG
Ioctl for getting NSF4 parameters. Refer to structure Nsf4v_Config.
- Returns
- FVID2_SOK on success, else error code.
◆ IOCTL_NSF4_SET_CONFIG
Ioctl for setting NSF4 parameters. Refer to structure Nsf4v_Config.
- Returns
- FVID2_SOK on success, else error code.
◆ NSF4_LSCC_MAX_SET
#define NSF4_LSCC_MAX_SET (2U) |
Maximum number of PWL Sets for LSCC.
◆ NSF4_LSCC_MAX_SEGMENT
#define NSF4_LSCC_MAX_SEGMENT (16U) |
Maximum number of segments in PWL curve for LSCC.
◆ NSF4_MAX_SCALE
#define NSF4_MAX_SCALE (3U) |
◆ NSF4_TN_MAX_SEGMENT
#define NSF4_TN_MAX_SEGMENT (12U) |
Maximum number of segments in PWL curve for TN.
◆ Nsf4vConfig_init()
This function should be used to initialize variable of type Nsf4v_Config.
- Parameters
-
- Returns
- None