PDK API Guide for J721E
|
Common configuration/API
Files | |
file | vhwa_common.h |
File containning defination for common configuration/API used across all VHWA modules. | |
Data Structures | |
struct | Vhwa_LutConfig |
Companding Lut configuration Structure LUT based companding is used at many places in RAWFE This structure is common and used for configuring these Luts. More... | |
struct | Vhwa_FocoPrms |
These are advanced parameters adn should not be modified in most cases. Used by DMPAC module. More... | |
struct | Vhwa_HtsLimiter |
Bandwith limiter configuration for HTS. This is used to slowed down the HTS by introducing clock cycles between internal start signals. These are advanced parameters and should not be modified in most cases. More... | |
Functions | |
uint32_t | Vhwa_calcHorzSizeInBytes (uint32_t width, uint32_t ccsf) |
Function to width of image in Bytes. More... | |
Typedefs | |
typedef uint64_t(* | Vhwa_GetTimeStamp) (void) |
VHWA FVID2 Driver IDs | |
#define | FVID2_VHWA_M2M_LDC_DRV_ID (FVID2_VHWA_DRV_BASE + 0x00U) |
FVID2 Driver Id for LDC Memory to Memory. More... | |
#define | FVID2_VHWA_M2M_NF_DRV_ID (FVID2_VHWA_M2M_LDC_DRV_ID + 0x01U) |
FVID2 Driver Id for NF Memory to Memory. More... | |
#define | FVID2_VHWA_M2M_MSC_DRV_ID (FVID2_VHWA_M2M_NF_DRV_ID + 0x01U) |
FVID2 Driver Id for MSC Memory to Memory. More... | |
#define | FVID2_VHWA_M2M_VISS_DRV_ID (FVID2_VHWA_M2M_MSC_DRV_ID + 0x01U) |
FVID2 Driver Id for VISS Memory to Memory. More... | |
#define | FVID2_VHWA_M2M_DOF_DRV_ID (FVID2_VHWA_M2M_VISS_DRV_ID + 0x01U) |
FVID2 Driver Id for DOF Memory to Memory. More... | |
#define | FVID2_VHWA_M2M_SDE_DRV_ID (FVID2_VHWA_M2M_DOF_DRV_ID + 0x01U) |
FVID2 Driver Id for SDE Memory to Memory. More... | |
#define | FVID2_VHWA_M2M_VISS_OTF_DRV_ID (FVID2_VHWA_M2M_SDE_DRV_ID + 0x01U) |
FVID2 Driver Id for VISS-OTF Memory to Memory. More... | |
#define | FVID2_VHWA_M2M_FC_DRV_ID (FVID2_VHWA_M2M_SDE_DRV_ID + 0x01U) |
FVID2 Driver Id for Flex-connect Memory to Memory. More... | |
VHWA Output IRQ Numbers | |
VHWA VPAC module outputs 6 IRQs and DMPAC outputs 2 IRQs. These Irq numbers should be passed as init parameters along with the core irq number to enable them in INTD module. | |
#define | VHWA_M2M_IRQ_NUM_0 (0u) |
#define | VHWA_M2M_IRQ_NUM_1 (1u) |
#define | VHWA_M2M_IRQ_NUM_2 (2u) |
#define | VHWA_M2M_IRQ_NUM_3 (3u) |
#define | VHWA_M2M_IRQ_NUM_4 (4u) |
#define | VHWA_M2M_IRQ_NUM_5 (5u) |
#define | VHWA_M2M_DMPAC_IRQ_NUM_0 (0u) |
#define | VHWA_M2M_DMPAC_IRQ_NUM_1 (1u) |
#define FVID2_VHWA_M2M_LDC_DRV_ID (FVID2_VHWA_DRV_BASE + 0x00U) |
FVID2 Driver Id for LDC Memory to Memory.
#define FVID2_VHWA_M2M_NF_DRV_ID (FVID2_VHWA_M2M_LDC_DRV_ID + 0x01U) |
FVID2 Driver Id for NF Memory to Memory.
#define FVID2_VHWA_M2M_MSC_DRV_ID (FVID2_VHWA_M2M_NF_DRV_ID + 0x01U) |
FVID2 Driver Id for MSC Memory to Memory.
#define FVID2_VHWA_M2M_VISS_DRV_ID (FVID2_VHWA_M2M_MSC_DRV_ID + 0x01U) |
FVID2 Driver Id for VISS Memory to Memory.
#define FVID2_VHWA_M2M_DOF_DRV_ID (FVID2_VHWA_M2M_VISS_DRV_ID + 0x01U) |
FVID2 Driver Id for DOF Memory to Memory.
#define FVID2_VHWA_M2M_SDE_DRV_ID (FVID2_VHWA_M2M_DOF_DRV_ID + 0x01U) |
FVID2 Driver Id for SDE Memory to Memory.
#define FVID2_VHWA_M2M_VISS_OTF_DRV_ID (FVID2_VHWA_M2M_SDE_DRV_ID + 0x01U) |
FVID2 Driver Id for VISS-OTF Memory to Memory.
#define FVID2_VHWA_M2M_FC_DRV_ID (FVID2_VHWA_M2M_SDE_DRV_ID + 0x01U) |
FVID2 Driver Id for Flex-connect Memory to Memory.
#define VHWA_IOCTL_COMMON_IOCTL_BASE (FVID2_VHWA_DRV_IOCTL_BASE) |
#define VHWA_IOCTL_COMMON_IOCTL_NUM (0x0000000AU) |
#define VHWA_IOCTL_COMMON_IOCTL_END |
#define VHWA_IOCTL_NF_IOCTL_BASE (VHWA_IOCTL_COMMON_IOCTL_END) |
NF Ioctl base
#define VHWA_IOCTL_NF_IOCTL_NUM (0x0000000AU) |
Number of control commands for NF
#define VHWA_IOCTL_NF_IOCTL_END |
#define VHWA_IOCTL_LDC_IOCTL_BASE (VHWA_IOCTL_NF_IOCTL_END) |
LDC Ioctl base
#define VHWA_IOCTL_LDC_IOCTL_NUM (0x0000000AU) |
Number of control commands for LDC
#define VHWA_IOCTL_LDC_IOCTL_END |
#define VHWA_IOCTL_MSC_IOCTL_BASE (VHWA_IOCTL_LDC_IOCTL_END) |
MSC Ioctl base
#define VHWA_IOCTL_MSC_IOCTL_NUM (0x0000000AU) |
Number of control commands for MSC
#define VHWA_IOCTL_MSC_IOCTL_END |
#define VHWA_IOCTL_RFE_IOCTL_BASE (VHWA_IOCTL_MSC_IOCTL_END) |
VISS Ioctl base
#define VHWA_IOCTL_RFE_IOCTL_NUM (0x0000000AU) |
Number of control commands for VISS
#define VHWA_IOCTL_RFE_IOCTL_END |
#define VHWA_IOCTL_FCP_IOCTL_BASE (VHWA_IOCTL_RFE_IOCTL_END) |
VISS Ioctl base
#define VHWA_IOCTL_FCP_IOCTL_NUM (0x0000000AU) |
Number of control commands for VISS
#define VHWA_IOCTL_FCP_IOCTL_END |
#define VHWA_IOCTL_NSF4_IOCTL_BASE (VHWA_IOCTL_FCP_IOCTL_END) |
VISS Ioctl base
#define VHWA_IOCTL_NSF4_IOCTL_NUM (0x0000000AU) |
Number of control commands for VISS
#define VHWA_IOCTL_NSF4_IOCTL_END |
#define VHWA_IOCTL_GLBCE_IOCTL_BASE (VHWA_IOCTL_NSF4_IOCTL_END) |
VISS Ioctl base
#define VHWA_IOCTL_GLBCE_IOCTL_NUM (0x0000000AU) |
Number of control commands for VISS
#define VHWA_IOCTL_GLBCE_IOCTL_END |
#define VHWA_IOCTL_H3A_IOCTL_BASE (VHWA_IOCTL_GLBCE_IOCTL_END) |
VISS Ioctl base
#define VHWA_IOCTL_H3A_IOCTL_NUM (0x0000000AU) |
Number of control commands for VISS
#define VHWA_IOCTL_H3A_IOCTL_END |
#define VHWA_IOCTL_CAC_IOCTL_BASE (VHWA_IOCTL_H3A_IOCTL_END) |
VISS Ioctl base
#define VHWA_IOCTL_CAC_IOCTL_NUM (0x0000000AU) |
Number of control commands for VISS
#define VHWA_IOCTL_CAC_IOCTL_END |
#define VHWA_IOCTL_DOF_IOCTL_BASE (VHWA_IOCTL_CAC_IOCTL_END) |
DOF Ioctl base
#define VHWA_IOCTL_DOF_IOCTL_NUM (0x0000000AU) |
Number of control commands for DOF
#define VHWA_IOCTL_DOF_IOCTL_END |
#define VHWA_IOCTL_SDE_IOCTL_BASE (VHWA_IOCTL_DOF_IOCTL_BASE) |
SDE Ioctl base
#define VHWA_IOCTL_SDE_IOCTL_NUM (0x0000000AU) |
Number of control commands for SDE
#define VHWA_IOCTL_SDE_IOCTL_END |
#define VHWA_IOCTL_M2M_MSC_IOCTL_BASE (VHWA_IOCTL_DOF_IOCTL_END) |
MSC M2M Driver Ioctl base
#define VHWA_IOCTL_M2M_MSC_IOCTL_NUM (0x00000008U) |
Number of control commands for MSC M2M Driver
#define VHWA_IOCTL_M2M_MSC_IOCTL_END |
Last control command for MSC M2M Driver
#define VHWA_IOCTL_M2M_LDC_IOCTL_BASE (VHWA_IOCTL_M2M_MSC_IOCTL_END) |
LDC M2M Driver Ioctl base
#define VHWA_IOCTL_M2M_LDC_IOCTL_NUM (0x00000008U) |
Number of control commands for LDC M2M Driver
#define VHWA_IOCTL_M2M_LDC_IOCTL_END |
Last control command for LDC M2M Driver
#define VHWA_IOCTL_M2M_VISS_IOCTL_BASE (VHWA_IOCTL_M2M_LDC_IOCTL_END) |
VISS M2M Driver Ioctl base
#define VHWA_IOCTL_M2M_VISS_IOCTL_NUM (0x0000000AU) |
Number of control commands for VISS M2M Driver
#define VHWA_IOCTL_M2M_VISS_IOCTL_END |
Last control command for VISS M2M Driver
#define VHWA_IOCTL_M2M_NF_IOCTL_BASE (VHWA_IOCTL_M2M_VISS_IOCTL_END) |
NF M2M Driver Ioctl base
#define VHWA_IOCTL_M2M_NF_IOCTL_NUM (0x00000008U) |
Number of control commands for NF M2M Driver
#define VHWA_IOCTL_M2M_NF_IOCTL_END |
Last control command for NF M2M Driver
#define VHWA_IOCTL_M2M_DOF_IOCTL_BASE (VHWA_IOCTL_M2M_NF_IOCTL_END) |
DOF M2M Driver Ioctl base
#define VHWA_IOCTL_M2M_DOF_IOCTL_NUM (0x00000010U) |
Number of control commands for DOF M2M Driver
#define VHWA_IOCTL_M2M_DOF_IOCTL_END |
Last control command for DOF M2M Driver
#define VHWA_IOCTL_M2M_SDE_IOCTL_BASE (VHWA_IOCTL_M2M_DOF_IOCTL_END) |
SDE M2M Driver Ioctl base
#define VHWA_IOCTL_M2M_SDE_IOCTL_NUM (0x00000008U) |
Number of control commands for SDE M2M Driver
#define VHWA_IOCTL_M2M_SDE_IOCTL_END |
Last control command for SDE M2M Driver
#define VHWA_IOCTL_FC_IOCTL_BASE (VHWA_IOCTL_M2M_SDE_IOCTL_END) |
Flex-connect Driver Ioctl base
#define VHWA_IOCTL_FC_IOCTL_NUM (0x00000010U) |
Number of control commands for Flex-connect Driver
#define VHWA_IOCTL_FC_IOCTL_END |
Last control command for Flex-connect Driver
#define VHWA_IOCTL_FC_VISS_IOCTL_BASE (VHWA_IOCTL_FC_IOCTL_END) |
Flex-connect Driver Ioctl base
#define VHWA_IOCTL_FC_VISS_IOCTL_NUM (0x0000004U) |
Number of control commands for Flex-connect Driver
#define VHWA_IOCTL_FC_VISS_IOCTL_END |
Last control command for VISS used by Flex-connect Driver
#define VHWA_IOCTL_FC_MSC_IOCTL_BASE (VHWA_IOCTL_FC_VISS_IOCTL_END) |
Flex-connect Driver Ioctl base
#define VHWA_IOCTL_FC_MSC_IOCTL_NUM (0x0000004U) |
Number of control commands for Flex-connect Driver
#define VHWA_IOCTL_FC_MSC_IOCTL_END |
Last control command for MSC used by Flex-connect Driver
#define VHWA_M2M_IRQ_NUM_0 (0u) |
#define VHWA_M2M_IRQ_NUM_1 (1u) |
#define VHWA_M2M_IRQ_NUM_2 (2u) |
#define VHWA_M2M_IRQ_NUM_3 (3u) |
#define VHWA_M2M_IRQ_NUM_4 (4u) |
#define VHWA_M2M_IRQ_NUM_5 (5u) |
#define VHWA_M2M_DMPAC_IRQ_NUM_0 (0u) |
#define VHWA_M2M_DMPAC_IRQ_NUM_1 (1u) |
typedef uint64_t(* Vhwa_GetTimeStamp) (void) |
MACRO to be defined to start all modules together < Function pointer for getting time stamp
uint32_t Vhwa_calcHorzSizeInBytes | ( | uint32_t | width, |
uint32_t | ccsf | ||
) |
Function to width of image in Bytes.
width | Width of Image in Pixels |
ccsf | Image Storeage format. Ref to Fvid2_ColorCompStorageFmt. Only Following format are supported
|