PDK API Guide for J721E
|
File containning defination for common configuration/API used across all VHWA modules.
Go to the source code of this file.
Data Structures | |
struct | Vhwa_LutConfig |
Companding Lut configuration Structure LUT based companding is used at many places in RAWFE This structure is common and used for configuring these Luts. More... | |
struct | Vhwa_FocoPrms |
These are advanced parameters adn should not be modified in most cases. Used by DMPAC module. More... | |
struct | Vhwa_HtsLimiter |
Bandwith limiter configuration for HTS. This is used to slowed down the HTS by introducing clock cycles between internal start signals. These are advanced parameters and should not be modified in most cases. More... | |
Typedefs | |
typedef uint64_t(* | Vhwa_GetTimeStamp) (void) |
Functions | |
uint32_t | Vhwa_calcHorzSizeInBytes (uint32_t width, uint32_t ccsf) |
Function to width of image in Bytes. More... | |