![]() |
PDK API Guide for J721E
|
Defines the structures / control operations that could be used to configure / control DOF M2M driver.
Go to the source code of this file.
Data Structures | |
struct | Vhwa_M2mDofPrms |
Connfiguration parameters of DOF. More... | |
struct | Vhwa_M2mDofCreateArgs |
Parameters required to create a new handle. More... | |
struct | Vhwa_M2mDofInitParams |
Initialization Parameters for DOF M2M Driver. More... | |
struct | Vhwa_M2mDofSl2AllocPrms |
Init Parameters required to allocate DOF driver. More... | |
Functions | |
static void | Vhwa_m2mDofInitParamsInit (Vhwa_M2mDofInitParams *dofInitPrms) |
Vhwa_M2mDofInitParams structure init function. More... | |
static void | Vhwa_m2mDofConfigInit (Vhwa_M2mDofPrms *dofCfg) |
Function to initialize the DOF configuration parameters to default. More... | |
static void | Vhwa_m2mDofCreateArgsInit (Vhwa_M2mDofCreateArgs *createArgs) |
Function to initialize the DOF create argument parameters to default. More... | |
int32_t | Vhwa_m2mDofInit (Vhwa_M2mDofInitParams *pInitPrms) |
DOF initialization function. This function initializes the DOF hardware and drivers. This function should be called before calling any driver APIs and only once. More... | |
void | Vhwa_m2mDofDeInit (void) |
DOF de-initialization function. This function un-initializes the DOF hardware and drivers. This function should be called during system shutdown if Vhwa_m2mDofDeInit() was called by the application. More... | |
int32_t | Vhwa_m2mDofAllocSl2 (const Vhwa_M2mDofSl2AllocPrms *sl2allocPrms) |
Function to allocate Sl2 memory for input and output buffers. Both DOF and SDE SL2 memory should be freed before reallocating. More... | |
int32_t | Vhwa_m2mDofFreeSl2 (void) |
Function to free allocated SL2. More... | |
void | Vhwa_m2mConfScoreParamInit (Dof_ConfScoreParam *csPrms) |
Function to Initialize the confidence score with default value. More... | |
static void | Vhwa_M2mDofSl2AllocPrmsInit (Vhwa_M2mDofSl2AllocPrms *sl2Prms) |