![]() |
PDK API Guide for J721E
|
Interface file for DOF M2M FVID2 driver
Files | |
file | vhwa_m2mDof.h |
Defines the structures / control operations that could be used to configure / control DOF M2M driver. | |
Data Structures | |
struct | Vhwa_M2mDofPrms |
Connfiguration parameters of DOF. More... | |
struct | Vhwa_M2mDofCreateArgs |
Parameters required to create a new handle. More... | |
struct | Vhwa_M2mDofInitParams |
Initialization Parameters for DOF M2M Driver. More... | |
struct | Vhwa_M2mDofSl2AllocPrms |
Init Parameters required to allocate DOF driver. More... | |
Functions | |
static void | Vhwa_m2mDofInitParamsInit (Vhwa_M2mDofInitParams *dofInitPrms) |
Vhwa_M2mDofInitParams structure init function. More... | |
static void | Vhwa_m2mDofConfigInit (Vhwa_M2mDofPrms *dofCfg) |
Function to initialize the DOF configuration parameters to default. More... | |
static void | Vhwa_m2mDofCreateArgsInit (Vhwa_M2mDofCreateArgs *createArgs) |
Function to initialize the DOF create argument parameters to default. More... | |
int32_t | Vhwa_m2mDofInit (Vhwa_M2mDofInitParams *pInitPrms) |
DOF initialization function. This function initializes the DOF hardware and drivers. This function should be called before calling any driver APIs and only once. More... | |
void | Vhwa_m2mDofDeInit (void) |
DOF de-initialization function. This function un-initializes the DOF hardware and drivers. This function should be called during system shutdown if Vhwa_m2mDofDeInit() was called by the application. More... | |
int32_t | Vhwa_m2mDofAllocSl2 (const Vhwa_M2mDofSl2AllocPrms *sl2allocPrms) |
Function to allocate Sl2 memory for input and output buffers. Both DOF and SDE SL2 memory should be freed before reallocating. More... | |
int32_t | Vhwa_m2mDofFreeSl2 (void) |
Function to free allocated SL2. More... | |
void | Vhwa_m2mConfScoreParamInit (Dof_ConfScoreParam *csPrms) |
Function to Initialize the confidence score with default value. More... | |
static void | Vhwa_M2mDofSl2AllocPrmsInit (Vhwa_M2mDofSl2AllocPrms *sl2Prms) |
Macros | |
#define | VHWA_M2M_DOF_MAX_IN_BUFFER (5U) |
#define | VHWA_M2M_DOF_MAX_OUT_BUFFER (1U) |
#define | VHWA_M2M_DOF_MAX_BUFFER |
#define | VHWA_M2M_DOF_DRV_INST_ID (0U) |
#define | VHWA_M2M_DOF_MAX_HANDLES (4u) |
Max Number of handles supported by DOF M2M Driver. More... | |
VHWA DOF IOCTL macros | |
#define | VHWA_M2M_IOCTL_DOF_SET_PARAMS (VHWA_IOCTL_DOF_IOCTL_BASE) |
IOCTL for setting DOF configuration. More... | |
#define | VHWA_M2M_IOCTL_DOF_SET_CONF_SCORE_PARAMS (VHWA_M2M_IOCTL_DOF_SET_PARAMS + 1u) |
IOCTL for setting Confidence score parameters. More... | |
#define | VHWA_M2M_IOCTL_DOF_SET_HTS_LIMIT (VHWA_M2M_IOCTL_DOF_SET_CONF_SCORE_PARAMS + 1u) |
IOCTL for setting bandwidth limiter. More... | |
#define | VHWA_M2M_IOCTL_DOF_SET_NEXT_PYR (VHWA_M2M_IOCTL_DOF_SET_HTS_LIMIT + 1u) |
IOCTL for setting next Pyramid level to be processsed this IOCTL should be called bfore process request. More... | |
#define | VHWA_M2M_IOCTL_DOF_GET_PERFORMANCE (VHWA_M2M_IOCTL_DOF_SET_NEXT_PYR + 1u) |
IOCTL for getting IP performance. More... | |
#define | VHWA_M2M_IOCTL_DOF_GET_PSA_SIGN (VHWA_M2M_IOCTL_DOF_GET_PERFORMANCE + 1u) |
IOCTL for getting the PSA signature. More... | |
#define | VHWA_M2M_IOCTL_DOF_GET_HISTOGRAM (VHWA_M2M_IOCTL_DOF_GET_PSA_SIGN + 1u) |
IOCTL for getting flow vector histogram. More... | |
#define | VHWA_M2M_IOCTL_DOF_REGISTER_ERR_CB (VHWA_M2M_IOCTL_DOF_GET_HISTOGRAM + 1u) |
IOCTL for registering the Error Callback. More... | |
#define | VHWA_M2M_IOCTL_DOF_SYNC_START (VHWA_M2M_IOCTL_DOF_REGISTER_ERR_CB + 1u) |
IOCTL to sync start each module This IOCTL doesn't configure any register and only enable pipeline to start processing. More... | |
VHWA DOF IO buffer indexes | |
#define | DOF_INPUT_REFERENCE_IMG (0U) |
#define | DOF_INPUT_CURRENT_IMG (1U) |
#define | DOF_INPUT_TEMPORAL_PRED (2U) |
#define | DOF_INPUT_PYRAMID_PRED (3U) |
#define | DOF_INPUT_SOF (4U) |
#define | DOF_OUTPUT (5U) |
#define | DOF_INPUT_FOCO_REF_IMG (6U) |
#define | DOF_INPUT_FOCO_CURR_IMG (7U) |
VHWA DOF Default Init Paramters | |
#define | DOF_DEFAULT_IMG_WIDTH (1312U) |
#define | DOF_DEFAULT_CCSF (FVID2_CCSF_BITS12_UNPACKED16) |
#define | DOF_DEFAULT_REF_BUFF_DEPTH (2U) |
#define | DOF_DEFAULT_CUR_BUFF_DEPTH (2U) |
#define | DOF_DEFAULT_FV_BUFF_DEPTH (4U) |
#define | DOF_DEFAULT_TOP_SR (48U) |
#define | DOF_DEFAULT_BOT_SR (48U) |
#define VHWA_M2M_IOCTL_DOF_SET_PARAMS (VHWA_IOCTL_DOF_IOCTL_BASE) |
IOCTL for setting DOF configuration.
#define VHWA_M2M_IOCTL_DOF_SET_CONF_SCORE_PARAMS (VHWA_M2M_IOCTL_DOF_SET_PARAMS + 1u) |
IOCTL for setting Confidence score parameters.
#define VHWA_M2M_IOCTL_DOF_SET_HTS_LIMIT (VHWA_M2M_IOCTL_DOF_SET_CONF_SCORE_PARAMS + 1u) |
IOCTL for setting bandwidth limiter.
#define VHWA_M2M_IOCTL_DOF_SET_NEXT_PYR (VHWA_M2M_IOCTL_DOF_SET_HTS_LIMIT + 1u) |
IOCTL for setting next Pyramid level to be processsed this IOCTL should be called bfore process request.
#define VHWA_M2M_IOCTL_DOF_GET_PERFORMANCE (VHWA_M2M_IOCTL_DOF_SET_NEXT_PYR + 1u) |
IOCTL for getting IP performance.
#define VHWA_M2M_IOCTL_DOF_GET_PSA_SIGN (VHWA_M2M_IOCTL_DOF_GET_PERFORMANCE + 1u) |
IOCTL for getting the PSA signature.
#define VHWA_M2M_IOCTL_DOF_GET_HISTOGRAM (VHWA_M2M_IOCTL_DOF_GET_PSA_SIGN + 1u) |
IOCTL for getting flow vector histogram.
#define VHWA_M2M_IOCTL_DOF_REGISTER_ERR_CB (VHWA_M2M_IOCTL_DOF_GET_HISTOGRAM + 1u) |
IOCTL for registering the Error Callback.
#define VHWA_M2M_IOCTL_DOF_SYNC_START (VHWA_M2M_IOCTL_DOF_REGISTER_ERR_CB + 1u) |
IOCTL to sync start each module This IOCTL doesn't configure any register and only enable pipeline to start processing.
#define VHWA_M2M_DOF_MAX_IN_BUFFER (5U) |
Maximim number of inputs DOF buffers
#define VHWA_M2M_DOF_MAX_OUT_BUFFER (1U) |
Maximim number of output DOF buffers
#define VHWA_M2M_DOF_MAX_BUFFER |
Maximim number of total DOF buffers Instance ID for the DOF M2m driver
#define VHWA_M2M_DOF_DRV_INST_ID (0U) |
#define VHWA_M2M_DOF_MAX_HANDLES (4u) |
Max Number of handles supported by DOF M2M Driver.
#define DOF_INPUT_REFERENCE_IMG (0U) |
#define DOF_INPUT_CURRENT_IMG (1U) |
#define DOF_INPUT_TEMPORAL_PRED (2U) |
#define DOF_INPUT_PYRAMID_PRED (3U) |
#define DOF_INPUT_SOF (4U) |
#define DOF_OUTPUT (5U) |
#define DOF_INPUT_FOCO_REF_IMG (6U) |
#define DOF_INPUT_FOCO_CURR_IMG (7U) |
#define DOF_DEFAULT_IMG_WIDTH (1312U) |
#define DOF_DEFAULT_CCSF (FVID2_CCSF_BITS12_UNPACKED16) |
#define DOF_DEFAULT_REF_BUFF_DEPTH (2U) |
#define DOF_DEFAULT_CUR_BUFF_DEPTH (2U) |
#define DOF_DEFAULT_FV_BUFF_DEPTH (4U) |
#define DOF_DEFAULT_TOP_SR (48U) |
#define DOF_DEFAULT_BOT_SR (48U) |
|
inlinestatic |
Vhwa_M2mDofInitParams structure init function.
dofInitPrms | Pointer to Vhwa_M2mDofInitParams structure. |
|
inlinestatic |
Function to initialize the DOF configuration parameters to default.
dofCfg | Pointer to a Vhwa_M2mDofPrms containing DOF configuration |
|
inlinestatic |
Function to initialize the DOF create argument parameters to default.
createArgs | Pointer to a Vhwa_M2mDofCreateArgs containing DOF create arguments |
int32_t Vhwa_m2mDofInit | ( | Vhwa_M2mDofInitParams * | pInitPrms | ) |
DOF initialization function. This function initializes the DOF hardware and drivers. This function should be called before calling any driver APIs and only once.
pInitPrms | Pointer to a Vhwa_M2mDofInitParams structure containing the DOF driver initialization parameters |
void Vhwa_m2mDofDeInit | ( | void | ) |
DOF de-initialization function. This function un-initializes the DOF hardware and drivers. This function should be called during system shutdown if Vhwa_m2mDofDeInit() was called by the application.
int32_t Vhwa_m2mDofAllocSl2 | ( | const Vhwa_M2mDofSl2AllocPrms * | sl2allocPrms | ) |
Function to allocate Sl2 memory for input and output buffers. Both DOF and SDE SL2 memory should be freed before reallocating.
sl2allocPrms | Pointer to a Vhwa_M2mDofSl2AllocPrms structure containing the SL2 allocation parameters |
int32_t Vhwa_m2mDofFreeSl2 | ( | void | ) |
Function to free allocated SL2.
void Vhwa_m2mConfScoreParamInit | ( | Dof_ConfScoreParam * | csPrms | ) |
Function to Initialize the confidence score with default value.
csPrms | Pointer to a Dof_ConfScoreParam structure which needs to be initialized |
|
inlinestatic |