![]() |
PDK API Guide for J721E
|
Init Parameters required to allocate DOF driver.
struct Vhwa_m2mDofSl2AllocPrms
Data Fields | |
uint32_t | maxImgWidth |
uint32_t | inCcsf |
uint32_t | refBuffDepth |
uint32_t | currBuffDepth |
uint32_t | fvBuffDepth |
uint32_t | topSR |
uint32_t | botSR |
uint32_t Vhwa_M2mDofSl2AllocPrms::maxImgWidth |
These parameters are used by the driver to allocater SL2 memory, used all driver handles. Ensure to allocate max of all handles requirement.Maximun image width
uint32_t Vhwa_M2mDofSl2AllocPrms::inCcsf |
CCSF for input image
uint32_t Vhwa_M2mDofSl2AllocPrms::refBuffDepth |
Input buffer depth in SL2 for reference image, final depth will be calculated based on tob and bottom searc range. Minumum configurable depth is 2
uint32_t Vhwa_M2mDofSl2AllocPrms::currBuffDepth |
Input buffer depth in SL2 for Current image Minumum configurable depth is 2
uint32_t Vhwa_M2mDofSl2AllocPrms::fvBuffDepth |
Flow vector buffer depth in Sl2
uint32_t Vhwa_M2mDofSl2AllocPrms::topSR |
Top search range
uint32_t Vhwa_M2mDofSl2AllocPrms::botSR |
Bottom search range