3. SDK Components¶
The following table lists all the top-level folders in the SDK package and the component it represents.
Folder |
Component |
|---|---|
app_utils |
|
c7x-mma-tidl |
|
cg_xml_* |
|
dsplib* |
|
edgeai-tiovx-apps |
|
ethfw |
|
fftlib_* |
|
imaging |
|
VHWA |
|
ivision |
|
mathlib_* |
|
mcusw |
|
mmalib_* |
|
pdk_j784s4_* |
|
psdk_rtos |
SDK Scripts and Documentation |
sdk_builder |
|
sdl |
|
tiadalg |
|
ti-perception-toolkit |
|
tiovx |
|
video_io |
|
vision_apps |
|
vxlib |
|
vxlib_* |
The following table lists all the packages that needs to downloaded separately or the script setup_psdk_rtos.sh will download these packages under /home/$USER/ti. Refer vision apps user guide [LINK].
Folder |
Component |
|---|---|
ti-cgt-arm_* |
|
ti-cgt-c7000_* |
3.1. HLOS Support (A72)¶
The vision apps demos assume and support either Linux or QNX running on the A72.
3.1.1. Processor SDK Linux J784S4¶
This package contains Linux kernel, uboot, filesystem and other linux tools.
Important
This package is NOT included in PSDK RTOS installer and needs to be downloaded separately
Either this package or QNX package MUST be downloaded to run vision apps, TI OpenVX demos.
Version |
11_01_00_03 |
Release notes |
${PSDK_LINUX_PATH}/docs/linux/index.html |
User guide |
${PSDK_LINUX_PATH}/docs/linux/index.html |
3.1.2. Processor SDK QNX J784S4¶
This package contains the QNX SDK components that include:
QNX resource manager for sci-client, udma, ipc and sharedmemory allocator
DEVNP driver for CPSW2G and CPSW5G
Test examples and sample applications
Important
This package is NOT included in PSDK RTOS installer and needs to be downloaded separately
Either this package or Linux package MUST be downloaded to run vision apps, TI OpenVX demos.
Version |
11_01_00 |
Release notes |
${PSDK_QNX_PATH}/docs/qnx/index.html |
User guide |
${PSDK_QNX_PATH}/docs/qnx/index.html |
3.2. SDK Builder¶
This package contains support for building different components.
Version |
11_01_00 |
Release notes |
|
User guide |
3.3. Vision Apps¶
This package contains Camera, ADAS, vision, perception, OpenVX demos.
Version |
11_01_00 |
Release notes |
|
User guide |
3.4. Edge AI TIOVX Apps¶
This package contains OpenVx based Edge AI applications
Version |
11_01_00 |
User guide |
3.5. Application Utilities (app_utils)¶
This package contains TI’s common abstraction layers for IPC and shared memory management that are used by TIOVX and Vision Apps. Below are the modules present in this package
console_io/file_io: Logging mechanism for remote cores Vto HLOS. Chunk of memory is reserved in DDR to send the logs from remote cores to HLOS.
ipc: Implements an abstraction layer between IPC stack for RTOS and HLOS(linux/QNX)
mem: Abstraction for shared memory heap management for RTOS and HLOS
perf_stats: APIs for HLOS to query performance data like remote core, HWA, DDR loading. Remote service framework is used to query data from remote cores
remote_service: A simple framework for remote cores to provide a user defined service to HLOS.
3.6. Platform Development Kit (PDK)¶
This package contains device drivers, bootloaders, CSL for baremetal/RTOS.
Version |
11_01_00 |
Release notes |
|
User guide |
3.7. MCU Software (MCU SW)¶
This package contains integrated MCU demos, MCAL for AutoSAR.
Version |
11_01_00 |
Release notes |
|
User guide |
3.8. Software Diagnostics Library (SDL)¶
This package provides interfaces to safety mechanisms and features for the development of software applications involving Functional Safety
Version |
11_01_00 |
Release notes |
|
User guide |
3.9. System firmware (SYSFW)¶
This package provides services for clock, power and resource management. These services are accessed via the “sciclient” interface in PDK.
Version |
11_01_08 |
Release notes |
|
User guide |
3.10. TI OpenVX (TIOVX)¶
This package contains TI’s implementation of OpenVX.
Version |
11_01_00 |
Release notes |
|
User guide |
3.11. Video Input/Output Kernels (video_io)¶
This package contains OpenVX kernels for CSI2RX, CSITX, and Display. These kernels used FVID2 interface to interact with low level drivers in PDK for Capture and Display.
3.12. TI Deep learning Product (TIDL)¶
This package contains TI’s Deep Learning inference solution with many industry wide open source run time (TFLite Runtime, ONNX Runtime and TVM based run time) on ARM MPU with an optimized TIDL runtime back-end on C7x and MMA. It also contains necessary tools for DNN compilation and provides many examples in both python and C to exercise tools and inference solution.
Version |
11_01_06_00 |
Release notes |
|
User guide |
3.13. MMALIB (C7x DSP)¶
This package contains MMA compute libraries
Version |
11_01_00_06 |
Release notes |
|
User guide |
3.14. Imaging¶
This package contains auto-exposure, auto-whilte balance algorithms for TI ISP. It also contains image sensor drivers, tuning parameters, as well as OpenVX kernels for VPAC and DMPAC.
Version |
11_01_01 |
Release notes |
|
User guide |
3.15. VHWA¶
The Vision Hardware Accelerator (VHWA) provides the logic to interface for MSC, NF, LDC, VISS, DOF and SDE accelerators. This is VHWA FVID2 driver documentation.
To build the user guide for VHWA run ‘make all’ from vhwa/docs/doxygen/
Version |
11_01_01 |
Release notes |
|
User guide |
3.16. Ethernet Switch Firmware (ETHFW)¶
This package contains Ethernet Switch Firmware for R5F.
Version |
11_01_00 |
Release notes |
|
User guide |
3.17. Perception Toolkit (PTK)¶
This package contains APIs and utilities for perception/fusion related functions and visualizations
Version |
11_01_00 |
Release notes |
|
User guide |
3.18. TI Autonomous Driving Algorithms (TIADALG)¶
This package contains sample pre-processing, post processing and other algorithms for autonomous driving.
Version |
11_01_00 |
Release notes |
|
User guide |
3.19. DSPLIB (C7x DSP)¶
This package implements common DSP functions for C7x
Version |
11_00_00_01 |
Release notes |
|
User guide |
3.20. FFTLIB (C7x DSP)¶
This package contains FFT compute libraries for C7x
Version |
11_00_00_01 |
Release notes |
|
User guide |
3.21. MATHLIB (C7x DSP)¶
This package implements common optimized math.h functions for C7x
Version |
11_00_00_01 |
Release notes |
|
User guide |
3.22. VXLIB¶
This package implements OpenVX v1.1 low level kernels cross compiled for C7x DSP
Version |
1_1_7_0 |
Release notes |
|
User guide |
3.23. VXLIB (C7x DSP)¶
This package implements common vision kernels for C7x
Version |
11_00_00_01 |
Release notes |
|
User guide |
3.24. CTools Library¶
CTools of Chip Tools contains a set of fundamental libraries to provide the debug facilities. CTools package is not included in PSDK RTOS installer and needs to be downloaded separately.
User Guide/Download Link |
https://software-dl.ti.com/emulation/esd/ctoolslib_k3/CToolsLib_K3.html |
3.25. RTOS¶
3.26. Code generation tools (CGT)¶
3.26.1. C7x code generation tools¶
This package contains C7x compiler, linker, host emulation mode libraries.
Version |
5.0.0.LTS |
Release notes |
|
User guide |
3.26.2. TI ARM R5F code generation tools¶
This package contains TI ARM R5F compiler, linker.
Version |
3.2.2.LTS |
Release notes |
|
User guide |
3.26.3. GCC ARM code generation tools¶
GCC tools are used to compile and link code on ARM A72. ARM CGT required for R5 Uboot and A72 Linux are packaged as part of SDK
CGT |
Download link |
|---|---|
ARM64 CGT for A72 RTOS |
Important
These packages are NOT included in PSDK RTOS installer and needs to be downloaded separately.
The script setup_psdk_rtos.sh downloads these packages. Refer vision apps user guide [LINK].