Vision Apps Release Notes

Version: 11.01.00

Contents

  1. Introduction
  2. Licensing
  3. Getting Started
  4. Documentation
  5. What's New
  6. Upgrade and Compatibility Information
  7. Device Support
  8. Validation Information
  9. Fixed Issues
  10. Open Defects
  11. Technical Support
  12. Package Versioning


Introduction

The Vision Apps package consists of ADAS, vision, deep learning, perception demos/applications for Jacinto 7 platform

To run the demos in vision apps, the companion Processor SDK Linux for Jacinto 7 also needs to be downloaded separately.


Licensing

Refer to Processor SDK RTOS manifest at top level [HTML]


Getting Started

The Vision Apps User Guide [HTML] provides the documentation and references necessary to begin development on TI's platforms using Vision Apps.


Documentation

Refer to following documentation for further details:

Vision Apps User Guide Build instructions, API Guide [HTML]
Surround View Manual Calibration Tool Instructions for Generating Calibration Binaries [PDF]
Release Notes Archive Previous release notes [FOLDER]


What's New

New features in this release are highlighted in bold


Upgrade and Compatibility Information


Device Support

Refer Processor SDK RTOS release notes [HTML]

Validation Information

The tools used to validate this package are listed in top level user guide [HTML]


Fixed Issues

ID Summary
ADASVISION-6386 QoS Settings cause artifacts in DSS M2M output
ADASVISION-6679 [QNX] GCC version of compiler is used in concerto instead of QCC
ADASVISION-6738 [QNX] vx_app_tidl app build broken for debug mode
ADASVISION-6647 MMALIB profile is hardcoded to "release" in linker paths

Open Defects

ID Summary
ADASVISION-4923 Single cam error on ports other than port 1 after running multi cam
ADASVISION-5555 SDE disparity artifacts on EVM
ADASVISION-6199 Race Conditions in c7x-mma-tidl and tiadalg builds
ADASVISION-6531 4k Display Flickers high C7x load
ADASVISION-6387 No option to set vpParams->scanFmt in the dss utility from vision_apps
ADASVISION-6451 mailbox queue overflowing while running vx_app_arm_ipc.out
ADASVISION-6452 SFM demo failing on J784S4 and J742S2
ADASVISION-6453 SRV + AVP demo not working
ADASVISION-6470 Dual Display with both DP ports is failing for J721S2 with LInux+RTOS
ADASVISION-6488 More than 1000% CPU Load for C7X & MCU
ADASVISION-6520 Apps killed with Cntrl^C do not do proper cleanup ... can't be run again
ADASVISION-6564 Vision app utils: qnx: All thread creation must use default stack instead of global stack


Technical Support

For technical support and additional assistance, contact local TI Field Application Engineer


Package Versioning

Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]. The table below provides a descriptive reference regarding package version numbering.

Digit Meaning Description
1 (M=Major) Major revision Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered.
2 (m=minor) Minor revision Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set.
3 (p=patch) Patch number Incremented for all other source code changes. This include any packaging support code.
4 (b=build) Build number Incremented for each release delivery to CM. Reset for any change to M, m or p

Copyright 2020, Texas Instruments Incorporated