TIOVX Release Notes

Version: 11.01.00


Contents

  1. Introduction
  2. Licensing
  3. Getting Started
  4. Documentation
  5. What's New
  6. Upgrade and Compatibility Information
  7. Device Support
  8. Validation Information
  9. Fixed Issues
  10. Known Issues
  11. Change Requests
  12. Documentation Change Log
  13. Technical Support
  14. Package Versioning


Introduction

The TIOVX package consists of the Texas Instruments OpenVX conformant implementation for Jacinto7 platform


Licensing

The licensing information of this library, as well as any third-party components included which are made available under a number of other open-source licenses are enumerated as part of the manifest. A complete manifest along with export control information is detailed here [HTML].


Getting Started

The TIOVX User Guide [HTML] provides the documentation and references necessary to begin development on TI's platforms using TIOVX.


Documentation

Refer to following documentation for further details:

TIOVX User Guide Build instructions, API Guide, tutorials, tool documentation, etc [HTML]
Test Reports Conformance test reports, TI platform test reports [XLSX]
Software Manifest Licenses, terms of use [HTML]
Static Analysis Report C and C++ Taxonomy Report [XLSX]
Bidirectional Traceability Report Traceability reports of MR to FR to Test [XLSX]
FMEA Failure modes and effects analysis of TIOVX framework, platform and utils layers Available upon request.


What's New

ID Summary
TIOVX-2256 Granular export of the usage of DDR_SHARED_MEM
TIOVX-2233 Support for RGB formats with Alpha value
TIOVX-2228 TIOVX shall support vxCreateTensorFromROI specification

Upgrade and Compatibility Information

File(s) Change description User application change required User application recompile required
utils/include/tivx_utils_graph_perf.h Added print API for application's node memory usage NO YES
utils/include/tivx_utils_ipc_ref_xfer.h Updated meta format internal structure to a union type NO YES
include/VX/vx_types.h Introduced VX_DF_IMAGE_RGBA image type NO YES
include/TI/soc/tivx_config_j784s4.h
include/TI/tivx_tensor.h
Added TIVX_IMAGE_MAX_SUBTENSORS and new API for creating a tensor object from a ROI NO YES


The tivxSetGraphPipelineDepth API will be deprecated in the 11.1 SDK. In place of this API, please use the vxSetGraphAttribute with the VX_GRAPH_PIPELINE_DEPTH attribute as is implemented in the Pipelining 2.0 extension.

Device Support

SoC Target (OS) Test Plaform
J784S4 x86_64 (Linux) x86_64 Linux with Ubuntu 22.04
J784S4 R5F, C7x running FreeRTOS or SafeRTOS
A72 running Linux Kernel v6.12 or QNX
J784S4 EVM

Validation Information

This release was built and validated using the following tools:

Build Tools (included in Processor SDK RTOS):

Dependencies (included in Processor SDK RTOS):

Dependencies (NOT included in Processor SDK RTOS):

Refer user guide [HTML] for instructions to install and setup above dependancies.

Fixed Issues

ID Summary
TIOVX-2338 Add documentation on the pipeline migration
TIOVX-2333 Mapping documentation is incomplete
TIOVX-2305 [OBJECT ARRAY] ownInitObjArrayFromObject in vx_objarray.c has a redundant loop
TIOVX-2279 Spinlock implementation for QNX do not need InterruptDisable/Enable
TIOVX-2235 Documentation: Several groups are missing from API docs

Known Issues

ID Summary
TIOVX-2142 [ J784S4 ] ./run_app_sfm.sh is not working in 10.01.00 SDK (Pink video issue)
TIOVX-1782 [LINUX] Array test case failing with migration to latest Linux GCC compiler
TIOVX-1453 Linux: APIs like vxSwapImageHandle, tivxReferenceImport and export handles does not consider dma_buf_fd
TIOVX-1309 Canny robustness test failing on PC emulation with full conformance test suite
TIOVX-1023 tivxGraphPipeline.MaxDataRef disabled due to failure caused by boundary condition
TIOVX-569 Bmp utils do not work for loading RGBX images

Change Requests

None


Documentation Change Log

Chapter Description
Graph Pipelining in TIOVX Detailed changes from migration to latest pipelining extension
TIOVX Public APIs Updated dangling APIs & organization
Data Object Mapping Included missing map APIs
Using TIVX_MEMORY_TYPE_DMA Clarified usage of TIVX_MEMORY_TYPE_DMA vs VX_MEMORY_TYPE_HOST

Technical Support

For technical support and additional assistance, contact local TI Field Application Engineer


Package Versioning

Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]. The table below provides a descriptive reference regarding package version numbering.

Digit Meaning Description
1 (M=Major) Major revision Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered.
2 (m=minor) Minor revision Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set.
3 (p=patch) Patch number Incremented for all other source code changes. This include any packaging support code.
4 (b=build) Build number Incremented for each release delivery to CM. Reset for any change to M, m or p

Copyright 2025, Texas Instruments Incorporated