TIOVX User Guide
tivx_objects.h
1 /*
2 *
3 * Copyright (c) 2017 Texas Instruments Incorporated
4 *
5 * All rights reserved not granted herein.
6 *
7 * Limited License.
8 *
9 * Texas Instruments Incorporated grants a world-wide, royalty-free, non-exclusive
10 * license under copyrights and patents it now or hereafter owns or controls to make,
11 * have made, use, import, offer to sell and sell ("Utilize") this software subject to the
12 * terms herein. With respect to the foregoing patent license, such license is granted
13 * solely to the extent that any such patent is necessary to Utilize the software alone.
14 * The patent license shall not apply to any combinations which include this software,
15 * other than combinations with devices manufactured by or for TI ("TI Devices").
16 * No hardware patent is licensed hereunder.
17 *
18 * Redistributions must preserve existing copyright notices and reproduce this license
19 * (including the above copyright notice and the disclaimer and (if applicable) source
20 * code license limitations below) in the documentation and/or other materials provided
21 * with the distribution
22 *
23 * Redistribution and use in binary form, without modification, are permitted provided
24 * that the following conditions are met:
25 *
26 * * No reverse engineering, decompilation, or disassembly of this software is
27 * permitted with respect to any software provided in binary form.
28 *
29 * * any redistribution and use are licensed by TI for use only with TI Devices.
30 *
31 * * Nothing shall obligate TI to provide you with source code for the software
32 * licensed and provided to you in object code.
33 *
34 * If software source code is provided to you, modification and redistribution of the
35 * source code are permitted provided that the following conditions are met:
36 *
37 * * any redistribution and use of the source code, including any resulting derivative
38 * works, are licensed by TI for use only with TI Devices.
39 *
40 * * any redistribution and use of any object code compiled from the source code
41 * and any resulting derivative works, are licensed by TI for use only with TI Devices.
42 *
43 * Neither the name of Texas Instruments Incorporated nor the names of its suppliers
44 *
45 * may be used to endorse or promote products derived from this software without
46 * specific prior written permission.
47 *
48 * DISCLAIMER.
49 *
50 * THIS SOFTWARE IS PROVIDED BY TI AND TI'S LICENSORS "AS IS" AND ANY EXPRESS
51 * OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES
52 * OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
53 * IN NO EVENT SHALL TI AND TI'S LICENSORS BE LIABLE FOR ANY DIRECT, INDIRECT,
54 * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
55 * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
56 * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY
57 * OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE
58 * OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED
59 * OF THE POSSIBILITY OF SUCH DAMAGE.
60 *
61 */
62 
63 
64 
65 
66 #ifndef TIVX_OBJECTS_H_
67 #define TIVX_OBJECTS_H_
68 
69 #include <vx_internal.h>
70 
71 #ifdef __cplusplus
72 extern "C" {
73 #endif
74 
80 typedef struct _tivx_object_t
81 {
200 } tivx_object_t;
201 
208 
215 
220 
225 
229 vx_status ownCheckUseFlag(vx_bool inUse[], uint32_t num_ele, uint32_t *error_index);
230 
234 void ownInitUseFlag(vx_bool inUse[], uint32_t num_ele);
235 
236 #ifdef __cplusplus
237 }
238 #endif
239 
240 #endif
vx_bool
Kernel object internal state.
Definition: vx_kernel.h:60
The top level context data for the entire OpenVX instance.
Definition: vx_context.h:75
Delay object internal state.
Definition: vx_delay.h:47
Image object internal state.
int32_t vx_enum
vx_status ownObjectDeInit(void)
De-Initialize object module.
#define TIVX_THRESHOLD_MAX_OBJECTS
Max number threshold objects supported.
Image object internal state.
Definition: vx_image.h:56
#define TIVX_SCALAR_MAX_OBJECTS
Max number scalar objects supported.
#define TIVX_PARAMETER_MAX_OBJECTS
Max number parameter objects supported.
vx_status ownObjectFree(vx_reference ref)
Free memory for a reference.
#define TIVX_RAW_IMAGE_MAX_OBJECTS
Max number raw image objects supported.
vx_enum vx_status
Distribution object internal state.
#define TIVX_CONVOLUTION_MAX_OBJECTS
Max number convolution objects supported.
Lut object internal state.
Definition: vx_lut.h:39
#define TIVX_SUPER_NODE_MAX_OBJECTS
Max number super node objects supported.
Definition: tivx.h:150
#define TIVX_DISTRIBUTION_MAX_OBJECTS
Max number distribution objects supported.
Image object internal state.
struct _vx_reference * vx_reference
#define TIVX_MATRIX_MAX_OBJECTS
Max number matrix objects supported.
vx_status ownCheckUseFlag(vx_bool inUse[], uint32_t num_ele, uint32_t *error_index)
Check flag for if the element is in use.
vx_reference ownObjectAlloc(vx_enum reftype)
Alloc memory for a reference of specified type.
Remap object internal state.
Definition: vx_remap.h:37
#define TIVX_GRAPH_MAX_OBJECTS
Max number graph objects supported.
Pyramid object internal state.
Definition: vx_pyramid.h:38
#define TIVX_NODE_MAX_OBJECTS
Max number node objects supported.
#define TIVX_PYRAMID_MAX_OBJECTS
Max number pyramid objects supported.
#define TIVX_USER_DATA_OBJECT_MAX_OBJECTS
Max number user data objects supported.
Structure to hold all framework objects.
Definition: tivx_objects.h:80
Convolution object internal state.
The top level data for graph object.
Definition: vx_graph.h:96
#define TIVX_ARRAY_MAX_OBJECTS
Max number array objects supported.
#define TIVX_TENSOR_MAX_OBJECTS
Max number tensor objects supported.
Scalar object internal state.
Definition: vx_scalar.h:39
object array internal state
Definition: vx_objarray.h:39
Parameter object internal state.
Definition: vx_parameter.h:39
User data object internal state.
Data Ref Queue internal state.
#define TIVX_KERNEL_MAX_OBJECTS
Max number kernel objects supported.
void ownInitUseFlag(vx_bool inUse[], uint32_t num_ele)
Initialize the array for flagging what is in use.
#define TIVX_CONTEXT_MAX_OBJECTS
Max number context objects supported.
Meta Format object internal state.
The internal representation of the error object.
Definition: vx_error.h:35
The internal representation of a node.
Definition: vx_node.h:45
Threshold object internal state.
Definition: vx_threshold.h:39
#define TIVX_META_FORMAT_MAX_OBJECTS
Max number meta format objects supported.
#define TIVX_DATA_REF_Q_MAX_OBJECTS
Max number data reference queue objects supported.
Matrix object internal state.
Definition: vx_matrix.h:39
The top level TI OpenVX implementation header.
Array object internal state.
Definition: vx_array.h:54
vx_status ownObjectInit(void)
Initialize object module.
#define TIVX_ERROR_MAX_OBJECTS
Max number error objects supported.
#define TIVX_IMAGE_MAX_OBJECTS
Max number image objects supported.
#define TIVX_LUT_MAX_OBJECTS
Max number LUT objects supported.
#define TIVX_REMAP_MAX_OBJECTS
Max number remap objects supported.
#define TIVX_OBJ_ARRAY_MAX_OBJECTS
Max number object arrays supported.
#define TIVX_DELAY_MAX_OBJECTS
Max number delay objects supported.
Tensor object internal state.
Definition: vx_tensor.h:101