![]() |
TIOVX User Guide
|
TI Extensions static configuration values.
Defines | |
| #define | TIVX_TARGET_MAX_JOB_QUEUE_DEPTH (96u) |
| Max depth of queue associated with target. More... | |
| #define | TIVX_DEFAULT_TILE_HEIGHT (48u) |
| Default tile height. | |
| #define | TIVX_DEFAULT_TILE_WIDTH (64u) |
| Default tile width. | |
| #define | TIVX_MAX_DSP_BAM_USER_PLUGINS (8u) |
| Max number of BAM user plugins on DSP (in addition to builtin vxlib plugins) | |
| #define | TIVX_SUPER_NODE_MAX_NODES (16u) |
| Max number of nodes per super node. | |
| #define | TIVX_SUPER_NODE_MAX_EDGES (16u) |
| Max number of edges per super node. | |
| #define | TIVX_SUPER_NODE_MAX_OBJECTS (16u) |
| Max number super node objects supported. | |
| #define | TIVX_MAX_CTRL_CMD_OBJECTS (4u) |
| Max size of control command objects. | |
| #define | TIVX_TARGET_MAX_TARGETS_IN_CPU (128u) |
| Max number of Target that can exist on a CPU. | |
| #define | TIVX_MAX_TARGETS_PER_KERNEL (32u) |
| Maximum targets a kernel can run on. | |
| #define | TIVX_TARGET_KERNEL_INSTANCE_MAX (64u) |
| Max target kernel instances that will be active on a CPU at the same time. | |
| #define | TIVX_TARGET_KERNEL_MAX (256u) |
| Max target kernel that will be active on a CPU at the same time. | |
| #define TIVX_TARGET_MAX_JOB_QUEUE_DEPTH (96u) |
Max depth of queue associated with target.
Definition at line 165 of file tivx_target.h.