138 #include "Std_Types.h" 140 #include <ti/drv/udma/udma.h> 141 #include "Spi/mcspi_hw/V0/mcspi.h" 159 #define SPI_SW_MAJOR_VERSION (2U) 161 #define SPI_SW_MINOR_VERSION (0U) 163 #define SPI_SW_PATCH_VERSION (0U) 173 #define SPI_AR_RELEASE_MAJOR_VERSION (4U) 175 #define SPI_AR_RELEASE_MINOR_VERSION (3U) 177 #define SPI_AR_RELEASE_REVISION_VERSION (1U) 185 #define SPI_VENDOR_ID ((uint16) 44U) 187 #define SPI_MODULE_ID ((uint16) 83U) 189 #define SPI_INSTANCE_ID ((uint8) 0U) 201 #define SPI_IB_EB (2U) 248 #ifndef SPI_E_PARAM_CHANNEL 250 #define SPI_E_PARAM_CHANNEL ((uint8) 0x0AU) 252 #ifndef SPI_E_PARAM_JOB 254 #define SPI_E_PARAM_JOB ((uint8) 0x0BU) 256 #ifndef SPI_E_PARAM_SEQ 258 #define SPI_E_PARAM_SEQ ((uint8) 0x0CU) 260 #ifndef SPI_E_PARAM_LENGTH 262 #define SPI_E_PARAM_LENGTH ((uint8) 0x0DU) 264 #ifndef SPI_E_PARAM_UNIT 266 #define SPI_E_PARAM_UNIT ((uint8) 0x0EU) 268 #ifndef SPI_E_PARAM_POINTER 270 #define SPI_E_PARAM_POINTER ((uint8) 0x10U) 274 #define SPI_E_UNINIT ((uint8) 0x1AU) 276 #ifndef SPI_E_SEQ_PENDING 278 #define SPI_E_SEQ_PENDING ((uint8) 0x2AU) 280 #ifndef SPI_E_SEQ_IN_PROCESS 282 #define SPI_E_SEQ_IN_PROCESS ((uint8) 0x3AU) 284 #ifndef SPI_E_ALREADY_INITIALIZED 289 #define SPI_E_ALREADY_INITIALIZED ((uint8) 0x4AU) 291 #ifndef SPI_E_SEQUENCE_NOT_OK 293 #define SPI_E_SEQUENCE_NOT_OK ((uint8) 0x5AU) 306 #define SPI_SID_INIT ((uint8) 0x00U) 308 #define SPI_SID_DEINIT ((uint8) 0x01U) 310 #define SPI_SID_WRITE_IB ((uint8) 0x02U) 312 #define SPI_SID_ASYNC_TRANSMIT ((uint8) 0x03U) 314 #define SPI_SID_READ_IB ((uint8) 0x04U) 316 #define SPI_SID_SETUP_EB ((uint8) 0x05U) 318 #define SPI_SID_GET_STATUS ((uint8) 0x06U) 320 #define SPI_SID_GET_JOB_RESULT ((uint8) 0x07U) 322 #define SPI_SID_GET_SEQ_RESULT ((uint8) 0x08U) 324 #define SPI_SID_GET_VERSION_INFO ((uint8) 0x09U) 326 #define SPI_SID_SYNC_TRANSMIT ((uint8) 0x0AU) 328 #define SPI_SID_GET_HW_UNIT_STATUS ((uint8) 0x0BU) 330 #define SPI_SID_CANCEL ((uint8) 0x0CU) 332 #define SPI_SID_SET_ASYNC_MODE ((uint8) 0x0DU) 334 #define SPI_SID_MAINFUNCTION_HANDLING ((uint8) 0x10U) 346 #define SPI_MCSPI_FCLK (48000000U) 356 #define SPI_CFG_ID_0 (0x01U) 359 #define SPI_CFG_ID_1 (0x02U) 361 #define SPI_CFG_ID_2 (0x04U) 363 #define SPI_CFG_ID_3 (0x08U) 365 #define SPI_CFG_ID_4 (0x10U) 367 #define SPI_CFG_ID_5 (0x20U) 369 #define SPI_CFG_ID_6 (0x40U) 799 typedef struct Spi_ConfigType_s
843 typedef struct Spi_ChannelConfigType_PC_s
855 typedef struct Spi_JobConfigType_PC_s
869 typedef struct Spi_SeqConfigType_PC_s
875 #if (STD_ON == SPI_REGISTER_READBACK_API) 956 FUNC(Std_ReturnType, SPI_CODE)
Spi_DeInit(
void);
1022 #if (STD_ON == SPI_VERSION_INFO_API) 1044 P2VAR(Std_VersionInfoType, AUTOMATIC, SPI_APPL_DATA) versioninfo);
1047 #if (STD_ON == SPI_HW_STATUS_API) 1072 #if ((SPI_CHANNELBUFFERS == SPI_IB) || (SPI_CHANNELBUFFERS == SPI_IB_EB)) 1135 #if ((SPI_CHANNELBUFFERS == SPI_EB) || (SPI_CHANNELBUFFERS == SPI_IB_EB)) 1168 FUNC(Std_ReturnType, SPI_CODE) Spi_SetupEB(
1176 #if ((SPI_SCALEABILITY == SPI_LEVEL_1) || (SPI_SCALEABILITY == \ 1202 #if (STD_ON == SPI_CANCEL_API) 1224 #if ((SPI_SCALEABILITY == SPI_LEVEL_0) || (SPI_SCALEABILITY == \ 1250 #if (SPI_SCALEABILITY == SPI_LEVEL_2) 1300 #if (STD_ON == SPI_REGISTER_READBACK_API) 1335 #if (STD_ON == SPI_SAFETY_API)
SPI Sequence configuration structure.
Definition: Spi.h:765
uint8 Spi_SequenceType
Specifies the identification (ID) for a sequence of jobs.
Definition: Spi.h:232
Std_ReturnType Spi_RegisterReadback(Spi_HWUnitType HWUnit, Spi_RegisterReadbackType *RegRbPtr)
This function reads the important registers of the hardware unit and returns the value in the structu...
Spi_SeqEndNotifyType Spi_SequenceEndNotification
Definition: Spi.h:769
Std_ReturnType Spi_SyncTransmit(Spi_SequenceType Sequence)
Service to transmit data on the SPI bus.
Spi_SeqResultType Spi_GetSequenceResult(Spi_SequenceType Sequence)
This service returns the last transmission result of the specified Sequence.
#define SPI_MAX_JOBS
Maximum jobs across all sequence/hwunit.
Definition: Spi_Cfg.h:182
void(* Spi_CacheInv)(uint8 *BufPtr, uint16 LenByte)
Cache invalidate function.
Definition: Spi.h:654
Spi_JobPriorityType jobPriority
Definition: Spi.h:746
Spi_AsyncModeType
Specifies the asynchronous mechanism mode for SPI busses handled asynchronously in LEVEL 2.
Definition: Spi.h:459
Spi_DataLineTransmitType transmissionLineEnable
Definition: Spi.h:724
#define SPI_MAX_CHANNELS_PER_JOB
Maximum channels allowed per job.
Definition: Spi_Cfg.h:173
Spi_StatusType Spi_GetHWUnitStatus(Spi_HWUnitType HWUnit)
This service returns the status of the specified SPI Hardware microcontroller peripheral.
Spi_NumberOfDataType maxBufLength
Definition: Spi.h:672
void(* Spi_CacheWb)(uint8 *BufPtr, uint16 LenByte)
Cache write-back function.
Definition: Spi.h:644
Std_ReturnType Spi_WriteIB(Spi_ChannelType Channel, const Spi_DataBufferType *DataBufferPtr)
Service for writing one or more data to an IB SPI Handler/Driver Channel specified by parameter.
uint8 externalDeviceCfgId
Definition: Spi.h:861
Spi_CacheWb cacheWb
Definition: Spi.h:824
void Spi_GetVersionInfo(Std_VersionInfoType *versioninfo)
This service returns the version information of this module.
Spi_JobResultType
This type defines a range of specific Jobs status for SPI Handler/Driver.
Definition: Spi.h:404
Spi_CsPinType
SPI Chip Select Pin.
Definition: Spi.h:495
Spi_TxRxMode
SPI TX/RX Mode.
Definition: Spi.h:535
uint8 Spi_HWUnitType
Specifies the identification (ID) for a SPI Hardware micro controller peripheral (unit)
Definition: Spi.h:240
#define SPI_MAX_HW_UNIT
Maximum HW unit - This should match the sum for the below units ISR which are ON.
Definition: Spi_Cfg.h:191
Mcspi_IrqStatusType
Irq status and std return type.
Definition: Spi.h:617
boolean enabledmaMode
Definition: Spi.h:785
Std_ReturnType Spi_dataOverflowUnderflowIntrDisable(Spi_HWUnitType HWUnit, uint32 intFlags)
This function Disable Under/Overflow Interupts of the hardware unit and returns the status.
Spi_DataDelayType
Spi_DataDelayType defines the number of interface clock cycles between CS toggling and first or last ...
Definition: Spi.h:576
Std_ReturnType Spi_SetAsyncMode(Spi_AsyncModeType Mode)
Service to set the asynchronous mechanism mode for SPI busses handled asynchronously.
Spi_HWUnitType hwUnitId
Definition: Spi.h:783
uint16 Spi_NumberOfDataType
Type for defining the number of data elements of the type Spi_DataBufferType to send and / or receive...
Definition: Spi.h:217
uint8 Spi_DataBufferType
Type of application data buffer elements.
Definition: Spi.h:209
SPI channel config structure parameters Pre-Compile only.
Definition: Spi.h:843
uint32 clkDivider
Definition: Spi.h:707
uint32 defaultTxData
Definition: Spi.h:670
#define SPI_MAX_JOBS_PER_SEQ
Maximum jobs allowed per sequence.
Definition: Spi_Cfg.h:176
uint32 udmaInstId
Definition: Spi.h:816
uint32 mcspiCh3config
Definition: Spi.h:904
Spi_CsModeType
SPI Chip Select Mode.
Definition: Spi.h:564
uint16 Spi_JobType
Specifies the identification (ID) for a Job.
Definition: Spi.h:227
Spi_SeqResultType
This type defines a range of specific Sequences status for SPI Handler/Driver.
Definition: Spi.h:425
Spi_HwUnitResultType
This type defines a range of specific HW unit status for SPI Handler/Driver.
Definition: Spi.h:442
#define SPI_MAX_CHANNELS
Maximum channels across all jobs/sequence/hwunit.
Definition: Spi_Cfg.h:179
SPI job config structure parameters Pre-Compile only.
Definition: Spi.h:855
SPI sequence config structure parameters Pre-Compile only.
Definition: Spi.h:869
Spi_TransferType transferType
Definition: Spi.h:682
uint32 mcspiRev
Definition: Spi.h:891
Mcspi_IrqStatusType Spi_dataOverflowUnderflowIntrGetStatus(Spi_HWUnitType HWUnit, uint32 intFlags)
This function status Under/Overflow Interupts of the hardware unit and returns the status.
uint16 startBitEnable
Definition: Spi.h:717
uint32 mcspiHlSysConfig
Definition: Spi.h:889
SPI Hardware unit configuration structure.
Definition: Spi.h:781
Spi_CacheWbInv cacheWbInv
Definition: Spi.h:822
uint8 dataWidth
Definition: Spi.h:667
Spi_ChannelType channelId
Definition: Spi.h:845
Spi_StatusType Spi_GetStatus(void)
Service returns the SPI Handler/Driver software module status.
Spi_CsModeType csMode
Definition: Spi.h:694
uint32 dmaTxChIntrNum
Definition: Spi.h:787
Std_ReturnType Spi_dataOverflowUnderflowIntrStatusClear(Spi_HWUnitType HWUnit, uint32 intFlags)
This function status clear Under/Overflow Interupts of the hardware unit and returns the status.
Spi_ClkMode clkMode
Definition: Spi.h:713
void(* Spi_CacheWbInv)(uint8 *BufPtr, uint16 LenByte)
Cache write-back invalidate function.
Definition: Spi.h:634
uint8 maxExtDevCfg
Definition: Spi.h:813
Spi_LevelType csPolarity
Definition: Spi.h:697
Spi_DataLineReceiveType receptionLineEnable
Definition: Spi.h:722
This file contains generated pre compile configuration file for SPI MCAL driver.
uint32 mcspiIrqenable
Definition: Spi.h:906
#define SPI_MAX_EXT_DEV
Maximum external device cfg.
Definition: Spi_Cfg.h:196
Spi_DataDelayType csIdleTime
Definition: Spi.h:699
Spi_McspiExternalDeviceConfigType mcspi
Definition: Spi.h:733
Std_ReturnType Spi_DeInit(void)
Service for SPI de-initialization.
void Spi_Init(const Spi_ConfigType *CfgPtr)
Service for SPI initialization.
uint8 maxSeq
Definition: Spi.h:807
Spi_LevelType startBitLevel
Definition: Spi.h:720
void Spi_Cancel(Spi_SequenceType Sequence)
Service cancels the specified on-going sequence transmission.
uint32 mcspiModulctrl
Definition: Spi.h:897
uint8 maxHwUnit
Definition: Spi.h:810
#define SPI_MAX_SEQ
Maximum sequence across all hwunit.
Definition: Spi_Cfg.h:185
Spi_CacheInv cacheInv
Definition: Spi.h:826
Spi_StatusType
This type defines a range of specific status for SPI Handler/Driver.
Definition: Spi.h:387
Std_ReturnType Spi_dataOverflowUnderflowIntrEnable(Spi_HWUnitType HWUnit, uint32 intFlags)
This function Enable Under/Overflow Interupts of the hardware unit and returns the status.
uint32 channelPerJob
Definition: Spi.h:752
uint32 mcspiCh0config
Definition: Spi.h:901
uint32 mcspiSysConfig
Definition: Spi.h:899
uint8 seqInterruptible
Definition: Spi.h:767
SPI register readback structure.
Definition: Spi.h:880
uint32 jobPerSeq
Definition: Spi.h:771
Spi_ClkMode
SPI Clock Mode - sets the clock polarity and phase. Note: These values are a direct register mapping....
Definition: Spi.h:511
uint32 mcspiHlRev
Definition: Spi.h:885
Spi_HWUnitType hwUnitId
Definition: Spi.h:748
uint32 mcspiSyst
Definition: Spi.h:895
Spi_TxRxMode txRxMode
Definition: Spi.h:715
SPI external device specific configuration structure .
Definition: Spi.h:731
uint32 dmaRxChIntrNum
Definition: Spi.h:789
uint8 maxChannels
Definition: Spi.h:801
SPI Job configuration structure specific to McSPI peripheral.
Definition: Spi.h:690
Std_ReturnType Spi_ReadIB(Spi_ChannelType Channel, Spi_DataBufferType *DataBufferPointer)
Service for reading synchronously one or more data from an IB SPI Handler/Driver Channel specified by...
Spi_JobType jobId
Definition: Spi.h:857
SPI Job configuration structure.
Definition: Spi.h:744
Spi_LevelType
Type for SPI Chip Select Polarity and Clock Idle Level.
Definition: Spi.h:484
Spi_JobEndNotifyType Spi_JobEndNotification
Definition: Spi.h:750
Spi_DataLineTransmitType
Spi_DataLineTransmitType defines the lines selected for transmission.
Definition: Spi.h:602
uint32 mcspiSysStatus
Definition: Spi.h:893
Spi_CsPinType csPin
Definition: Spi.h:859
uint32 mcspiHlHwInfo
Definition: Spi.h:887
Spi_JobPriorityType
SPI Job Priority.
Definition: Spi.h:549
Spi_DataLineReceiveType
Spi_DataLineReceiveType defines the lines selected for reception.
Definition: Spi.h:591
uint8 Spi_ChannelType
Specifies the identification (ID) for a Channel.
Definition: Spi.h:222
void Spi_MainFunction_Handling(void)
This function polls the SPI interrupts linked to HW Units allocated to the transmission of SPI sequen...
SPI Channel configuration structure.
Definition: Spi.h:663
Spi_SequenceType seqId
Definition: Spi.h:871
Std_ReturnType Spi_AsyncTransmit(Spi_SequenceType Sequence)
Service to transmit data on the SPI bus.
uint8 channelBufType
Definition: Spi.h:665
uint32 mcspiCh2config
Definition: Spi.h:903
uint16 csEnable
Definition: Spi.h:692
Spi_TransferType
Word transfer order - MSB first or LSB first.
Definition: Spi.h:473
Spi_JobResultType Spi_GetJobResult(Spi_JobType Job)
This service returns the last transmission result of the specified Job.
SPI config structure.
Definition: Spi.h:799
uint8 maxJobs
Definition: Spi.h:804
uint32 mcspiCh1config
Definition: Spi.h:902