Release notes version 08.01.00

New in this Release

  • Support for Sony’s IMX219 raw sensor with ISP offload using GStreamer element

  • Python and C++ apps integrated with newer GStreamer plugins, - tiovxmosaic - tiovxisp

  • Newer GST plugins available part of edgeai-gst-plugins repo - tiovxcolorblend - tiovxldc - tiovxmux - tiovxdemux

  • Support for hardware accelerated H.264 encoder

  • Support for hardware accelerated H.265 decoder

  • New easy to use ti-gpio python and C++ libraries

  • Multiple bug fixes to improve stability.

Fixed in this Release

  • ADASVISION-5115 - Edge AI Apps with RPi Camera as source hangs after running for around 45 min

  • ADASVISION-5103 - Random hang at vxWaitGraph for MCU2_0 based OpenVx nodes

  • ADASVISION-5102 - v4l2h265 decoder not working when followed by tee and tiovxmultiscalar

  • ADASVISION-5097 - Video file output is corrupt / not playable in docker

  • ADASVISION-5079 - Documentation errors for OV5640 CSI camera

  • ADASVISION-5059 - Edge AI SDK setup script fails to build edgeai-gst-plugins

  • ADASVISION-5048 - appDeInit not called when tiovx element is present in output pipeline (C++ apps only)

  • ADASVISION-5042 - setup_script fails to install dependency

  • ADASVISION-4991 - Decoder + kmssink elements generates pink and green frames blinking

  • ADASVISION-4981 - GStreamer-CRITICAL error observed in logs, however demos run fine

  • ADASVISION-4979 - Demo apps hang if RTSP server is down

  • ADASVISION-4960 - Edge AI C++ apps do not run when building in debug mode

  • ADASVISION-4959 - Edge AI Demos do not run more than 4-5 hours

  • ADASVISION-4872 - VX_ZONE-ERROR when application runs for more than 250 times

Known Issues

  • ADASVISION-5149 - Hostname incorrect in SK shows j7-evm instead of tda4vm-sk

  • ADASVISION-5117 - USB 3.0 device is recognized as USB 2.1 sometimes

  • ADASVISION-5113 - GST Pipeline error: Error pulling tensor from GST Pipeline

  • ADASVISION-5070 - Edge AI demo output not resizing properly on 4K monitor

  • ADASVISION-4997 - Multi-input multi-inference demo freezes after long duration run

  • ADASVISION-4953 - Video looping does not work with v4l2 HW decoder plugin

  • ADASVISION-4943 - IMX219 based Rpi camera cannot capture data correctly for 10 bit format

  • ADASVISION-4809 - Python and C++ apps cannot measure pre and post processing time accurately

  • ADASVISION-4794 - Application takes 10-15 seconds to come up in some cases

Note

Please also refer to edgeai-gst-plugins issues for more details on bugs filed on custom GStreamer plugins

Software components

List of software components used in this version

Componenet

Version

PSDKLA (filesystem, uboot)

08.01.00.07

PSDKRA (firmware)

08.01.00.13

Docker

19.03.8-ce

Ubuntu (Docker)

20.04.LTS

Python

3.8

OpenCV

4.5.1

GStreamer

1.16.2

Cmake

3.16.3

Ninja

1.10.0

Meson

0.57.2

Jupyterlab

3.0.14

NeoAI - DLR

1.8.0

Tensorflow

2.4

TFLite-runtime

2.5.0

ONNX-runtime

1.7.0

PyYAML

5.4.1

TI Model Zoo

8.1.0

edgeai-gst-plugins

0.5.3

edgeai-tiovx-modules

0.2.0