66 #ifndef TIVX_OBJECTS_H_ 67 #define TIVX_OBJECTS_H_ 80 typedef struct _tivx_object_t
Kernel object internal state.
The top level context data for the entire OpenVX instance.
Delay object internal state.
Image object internal state.
vx_status ownObjectDeInit(void)
De-Initialize object module.
#define TIVX_THRESHOLD_MAX_OBJECTS
Max number threshold objects supported.
Image object internal state.
#define TIVX_SCALAR_MAX_OBJECTS
Max number scalar objects supported.
#define TIVX_PARAMETER_MAX_OBJECTS
Max number parameter objects supported.
vx_status ownObjectFree(vx_reference ref)
Free memory for a reference.
#define TIVX_RAW_IMAGE_MAX_OBJECTS
Max number raw image objects supported.
Distribution object internal state.
#define TIVX_CONVOLUTION_MAX_OBJECTS
Max number convolution objects supported.
Lut object internal state.
#define TIVX_SUPER_NODE_MAX_OBJECTS
Max number super node objects supported.
#define TIVX_DISTRIBUTION_MAX_OBJECTS
Max number distribution objects supported.
Image object internal state.
struct _vx_reference * vx_reference
#define TIVX_MATRIX_MAX_OBJECTS
Max number matrix objects supported.
vx_status ownCheckUseFlag(vx_bool inUse[], uint32_t num_ele, uint32_t *error_index)
Check flag for if the element is in use.
vx_reference ownObjectAlloc(vx_enum reftype)
Alloc memory for a reference of specified type.
Remap object internal state.
#define TIVX_GRAPH_MAX_OBJECTS
Max number graph objects supported.
Pyramid object internal state.
#define TIVX_NODE_MAX_OBJECTS
Max number node objects supported.
#define TIVX_PYRAMID_MAX_OBJECTS
Max number pyramid objects supported.
#define TIVX_USER_DATA_OBJECT_MAX_OBJECTS
Max number user data objects supported.
Structure to hold all framework objects.
Convolution object internal state.
The top level data for graph object.
#define TIVX_ARRAY_MAX_OBJECTS
Max number array objects supported.
#define TIVX_TENSOR_MAX_OBJECTS
Max number tensor objects supported.
Scalar object internal state.
object array internal state
Parameter object internal state.
User data object internal state.
Data Ref Queue internal state.
#define TIVX_KERNEL_MAX_OBJECTS
Max number kernel objects supported.
void ownInitUseFlag(vx_bool inUse[], uint32_t num_ele)
Initialize the array for flagging what is in use.
#define TIVX_CONTEXT_MAX_OBJECTS
Max number context objects supported.
The internal representation of the error object.
The internal representation of a node.
Threshold object internal state.
#define TIVX_META_FORMAT_MAX_OBJECTS
Max number meta format objects supported.
#define TIVX_DATA_REF_Q_MAX_OBJECTS
Max number data reference queue objects supported.
Matrix object internal state.
The top level TI OpenVX implementation header.
Array object internal state.
vx_status ownObjectInit(void)
Initialize object module.
#define TIVX_ERROR_MAX_OBJECTS
Max number error objects supported.
#define TIVX_IMAGE_MAX_OBJECTS
Max number image objects supported.
#define TIVX_LUT_MAX_OBJECTS
Max number LUT objects supported.
#define TIVX_REMAP_MAX_OBJECTS
Max number remap objects supported.
#define TIVX_OBJ_ARRAY_MAX_OBJECTS
Max number object arrays supported.
#define TIVX_DELAY_MAX_OBJECTS
Max number delay objects supported.
Tensor object internal state.