TIOVX User Guide
vx_tensor.h
Go to the documentation of this file.
1 /*
2 *
3 * Copyright (c) 2018 Texas Instruments Incorporated
4 *
5 * All rights reserved not granted herein.
6 *
7 * Limited License.
8 *
9 * Texas Instruments Incorporated grants a world-wide, royalty-free, non-exclusive
10 * license under copyrights and patents it now or hereafter owns or controls to make,
11 * have made, use, import, offer to sell and sell ("Utilize") this software subject to the
12 * terms herein. With respect to the foregoing patent license, such license is granted
13 * solely to the extent that any such patent is necessary to Utilize the software alone.
14 * The patent license shall not apply to any combinations which include this software,
15 * other than combinations with devices manufactured by or for TI ("TI Devices").
16 * No hardware patent is licensed hereunder.
17 *
18 * Redistributions must preserve existing copyright notices and reproduce this license
19 * (including the above copyright notice and the disclaimer and (if applicable) source
20 * code license limitations below) in the documentation and/or other materials provided
21 * with the distribution
22 *
23 * Redistribution and use in binary form, without modification, are permitted provided
24 * that the following conditions are met:
25 *
26 * * No reverse engineering, decompilation, or disassembly of this software is
27 * permitted with respect to any software provided in binary form.
28 *
29 * * any redistribution and use are licensed by TI for use only with TI Devices.
30 *
31 * * Nothing shall obligate TI to provide you with source code for the software
32 * licensed and provided to you in object code.
33 *
34 * If software source code is provided to you, modification and redistribution of the
35 * source code are permitted provided that the following conditions are met:
36 *
37 * * any redistribution and use of the source code, including any resulting derivative
38 * works, are licensed by TI for use only with TI Devices.
39 *
40 * * any redistribution and use of any object code compiled from the source code
41 * and any resulting derivative works, are licensed by TI for use only with TI Devices.
42 *
43 * Neither the name of Texas Instruments Incorporated nor the names of its suppliers
44 *
45 * may be used to endorse or promote products derived from this software without
46 * specific prior written permission.
47 *
48 * DISCLAIMER.
49 *
50 * THIS SOFTWARE IS PROVIDED BY TI AND TI'S LICENSORS "AS IS" AND ANY EXPRESS
51 * OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES
52 * OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
53 * IN NO EVENT SHALL TI AND TI'S LICENSORS BE LIABLE FOR ANY DIRECT, INDIRECT,
54 * INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING,
55 * BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
56 * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY
57 * OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE
58 * OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED
59 * OF THE POSSIBILITY OF SUCH DAMAGE.
60 *
61 */
62 
63 
64 
65 #ifndef VX_TENSOR_H_
66 #define VX_TENSOR_H_
67 
68 
69 #ifdef __cplusplus
70 extern "C" {
71 #endif
72 
83 typedef struct _tivx_tensor_map_info_t
84 {
86  uint8_t *map_addr;
94 
95 
101 typedef struct _vx_tensor
102 {
107 
108 } tivx_tensor_t;
109 
110 
111 
112 
113 #ifdef __cplusplus
114 }
115 #endif
116 
117 #endif
size_t vx_size
vx_enum usage
Type of access being done by user, see vx_accessor_e.
Definition: vx_tensor.h:92
int32_t vx_enum
The most basic type in the OpenVX system. Any type that inherits from tivx_reference_t must have a vx...
Definition: vx_reference.h:73
uint8_t * map_addr
Address mapped via vxMapTensorPatch()
Definition: vx_tensor.h:86
#define TIVX_TENSOR_MAX_MAPS
Max possible mapping via vxMapTensorPatch supported.
tivx_reference_t base
reference object
Definition: vx_tensor.h:104
vx_enum mem_type
Type of memory mapped via vxMapTensorPatch(), see vx_memory_type_e and tivx_memory_type_e.
Definition: vx_tensor.h:90
vx_size map_size
Size of memory region mapped via vxMapTensorPatch()
Definition: vx_tensor.h:88
Information about a image mapping.
Definition: vx_tensor.h:83
Tensor object internal state.
Definition: vx_tensor.h:101