![]() |
TIOVX User Guide
|
Internal APIs for object operations.
Data Structures | |
| struct | tivx_object_t |
| Structure to hold all framework objects. More... | |
Functions | |
| vx_reference | ownObjectAlloc (vx_enum reftype) |
| Alloc memory for a reference of specified type. More... | |
| vx_status | ownObjectFree (vx_reference ref) |
| Free memory for a reference. More... | |
| vx_status | ownObjectInit (void) |
| Initialize object module. | |
| vx_status | ownObjectDeInit (void) |
| De-Initialize object module. | |
| vx_status | ownCheckUseFlag (vx_bool inUse[], uint32_t num_ele, uint32_t *error_index) |
| Check flag for if the element is in use. | |
| void | ownInitUseFlag (vx_bool inUse[], uint32_t num_ele) |
| Initialize the array for flagging what is in use. | |
| vx_reference ownObjectAlloc | ( | vx_enum | reftype | ) |
Alloc memory for a reference of specified type.
| [in] | reftype | The reference type. See tivx_reftype_e |
| vx_status ownObjectFree | ( | vx_reference | ref | ) |
Free memory for a reference.
| [in] | ref | The reference. |