TIOVX User Guide
vx_objarray.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2012-2016 The Khronos Group Inc.
3  *
4  * Licensed under the Apache License, Version 2.0 (the "License");
5  * you may not use this file except in compliance with the License.
6  * You may obtain a copy of the License at
7  *
8  * http://www.apache.org/licenses/LICENSE-2.0
9  *
10  * Unless required by applicable law or agreed to in writing, software
11  * distributed under the License is distributed on an "AS IS" BASIS,
12  * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13  * See the License for the specific language governing permissions and
14  * limitations under the License.
15  */
16 
17 
18 
19 #ifndef VX_OBJARRAY_H_
20 #define VX_OBJARRAY_H_
21 
22 
23 #ifdef __cplusplus
24 extern "C" {
25 #endif
26 
39 typedef struct _vx_object_array
40 {
43 
47 
48 
49 
50 
51 #ifdef __cplusplus
52 }
53 #endif
54 
55 #endif
#define TIVX_OBJECT_ARRAY_MAX_ITEMS
Maximum number of objects supported in object array.
The most basic type in the OpenVX system. Any type that inherits from tivx_reference_t must have a vx...
Definition: vx_reference.h:73
struct _vx_reference * vx_reference
object array internal state
Definition: vx_objarray.h:39
tivx_reference_t base
reference object
Definition: vx_objarray.h:42