![]() |
![]() |
|
TI-RTOS Drivers
tidrivers_full_2_20_00_08
|
| CADC_Config | ADC Global configuration |
| CADC_FxnTable | The definition of a ADC function table that contains the required set of functions to control a specific ADC driver implementation |
| CADC_Params | ADC Parameters |
| CADCBuf_Config | ADCBuf Global configuration |
| CADCBuf_Conversion | An ADCBuf_Conversion data structure is used with ADCBuf_convert(). It indicates which channel to perform the ADC conversion on, how many conversions to make, and where to put them. The arg variable is an user-definable argument which gets passed to the ADCBuf_Callback when the ADC driver is in ADCBuf_RETURN_MODE_CALLBACK |
| CADCBuf_FxnTable | The definition of an ADCBuf function table that contains the required set of functions to control a specific ADC driver implementation |
| CADCBuf_Params | ADC Parameters |
| CADCBufCC26XX_AdcChannelLutEntry | Table entry that maps a virtual adc channel to a dio and its corresponding internal analogue signal |
| CADCBufCC26XX_HWAttrs | ADCBufCC26XX Hardware Attributes |
| CADCBufCC26XX_Object | ADCBufCC26XX Object |
| CADCBufCC26XX_ParamsExtension | CC26XX specfic extension to ADCBuf_Params |
| CADCCC26XX_HWAttrs | ADCCC26XX Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions |
| CADCCC26XX_Object | ADCCC26XX Object |
| CADCMSP432_HWAttrs | ADCMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSPWare these definitions are found in: |
| CADCMSP432_Object | ADCMSP432 Object |
| CCamera_Config | Camera Global configuration |
| CCamera_FxnTable | The definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation |
| CCamera_Params | Camera Parameters |
| CCameraCC3200DMA_HWAttrs | CameraCC3200DMA Hardware attributes |
| CCameraCC3200DMA_Object | CameraCC3200DMA Object |
| CClockP_FreqHz | Frequency-in-hertz struct |
| CClockP_Params | Basic ClockP Parameters |
| CCryptoCC26XX_AESCBC_Transaction | CryptoCC26XX AES-CBC Transaction |
| CCryptoCC26XX_AESCCM_Transaction | CryptoCC26XX AES-CCM Transaction |
| CCryptoCC26XX_AESECB_Transaction | CryptoCC26XX AES-ECB Transaction |
| CCryptoCC26XX_Config | CryptoCC26XX Global Configuration |
| CCryptoCC26XX_HWAttrs | CryptoCC26XX Hardware Attributes |
| CCryptoCC26XX_Object | CryptoCC26XX Object |
| CCryptoCC26XX_Params | CryptoCC26XX Parameters |
| CCryptoCC26XX_Transaction | CryptoCC26XX Transaction |
| CDIR | |
| Cdiskio_fxns | |
| CDisplay_Config | Display Global configuration |
| CDisplay_FxnTable | The definition of a Display function table that contains the required set of functions to control a specific Display driver implementation |
| CDisplay_Params | Display Parameters |
| CDisplayDogm1286_HWAttrs | |
| CDisplayDogm1286_Object | |
| CDisplayGrLib_Object | |
| CDisplayLog_Object | |
| CDisplaySharp_HWAttrs | |
| CDisplaySharp_Object | |
| CDisplaySharpColor_t | Foreground and background color struct, compatible with GrLib |
| CDisplayUart_HWAttrs | |
| CDisplayUart_Object | |
| CEMAC_Config | EMAC Global configuration |
| CEMAC_FxnTable | EMAC Function table structure |
| CEMACSnow_HWAttrs | EMACSnow Hardware attributes |
| CEMACSnow_Object | EMACSnow Object |
| CEMACTiva_HWAttrs | EMACTiva Hardware attributes |
| CEMACTiva_Object | EMACTiva Object |
| CExtFlashInfo_t | |
| CFATFS | |
| CFIL | |
| CFILINFO | |
| CGPIOCC26XX_Config | GPIO device specific driver configuration structure |
| CGPIOCC3200_Config | GPIO device specific driver configuration structure |
| CGPIOMSP430_Config | GPIO device specific driver configuration structure |
| CGPIOMSP432_Config | GPIO device specific driver configuration structure |
| CGPIOTiva_Config | GPIO device specific driver configuration structure |
| CGPTimerCC26XX_Config | GPTimer Global configuration |
| CGPTimerCC26XX_HWAttrs | GPTimer26XX Hardware attributes |
| CGPTimerCC26XX_Object | GPTimer26XX Object |
| CGPTimerCC26XX_Params | GPTimerCC26XX Parameters |
| CHwiP_Params | Basic HwiP Parameters |
| CI2C_Config | I2C global configuration |
| CI2C_FxnTable | The definition of an I2C function table that contains the required set of functions to control a specific I2C driver implementation |
| CI2C_Params | I2C Parameters |
| CI2C_Transaction | I2C transaction |
| CI2CCC26XX_HWAttrsV1 | I2CCC26XX Hardware attributes |
| CI2CCC26XX_I2CPinCfg | I2CCC26XX Pin Configuration |
| CI2CCC26XX_Object | I2CCC26XX Object |
| CI2CCC3200_HWAttrs | I2CCC3200 Hardware attributes |
| CI2CCC3200_Object | I2CCC3200 Object |
| CI2CEUSCIB_HWAttrs | I2CEUSCIB Hardware attributes |
| CI2CEUSCIB_Object | I2CEUSCIB Object |
| CI2CMSP432_HWAttrs | I2CMSP432 Hardware attributes These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: |
| CI2CMSP432_Object | I2CMSP432 Object |
| CI2CSlave_Config | I2CSlave Global configuration |
| CI2CSlave_FxnTable | The definition of a I2CSlave function table that contains the required set of functions to control a specific I2CSlave driver implementation |
| CI2CSlave_Params | I2CSlave Parameters |
| CI2CSlaveMSP432_HWAttrs | I2CSlaveMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: |
| CI2CSlaveMSP432_Object | I2CSlaveMSP432 Object |
| CI2CTiva_HWAttrs | I2CTiva Hardware attributes |
| CI2CTiva_Object | I2CTiva Object |
| CI2CUSCIB_HWAttrs | I2CUSCIB Hardware attributes |
| CI2CUSCIB_Object | I2CUSCIB Object |
| CI2S_BufDesc | I2S buffer descriptor for issue/reclaim mode |
| CI2S_Config | I2S Global configuration |
| CI2S_FxnTable | The definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation |
| CI2S_Params | Basic I2S Parameters |
| CI2SCC3200DMA_HWAttrs | I2SCC3200DMA Hardware attributes |
| CI2SCC3200DMA_Object | I2SCC3200DMA Object |
| CI2SCC3200DMA_SerialPinConfig | CC3200 Serial Pin Configuration |
| CI2SCC3200DMA_SerialPinParams | CC3200 specific I2S Parameters |
| CI2SCC3200DMA_SerialPinVars | I2SCC3200DMA Serial pin variables |
| CLCD_Buffer | LCD_Buffer used to store data to be printed on the LCD display |
| CLCD_Command | Format of LCD commands used by the LCD controller |
| CLCD_Config | The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementation |
| CLCD_HWAttrs | LCD Hardware attributes |
| CLCD_Object | LCD Object |
| CLCD_Params | LCD Parameters are used to with the LCD_open() call. Default values for these parameters are set using LCD_Params_init() |
| CList_Elem | |
| CList_List | |
| CMutexP_Params | Basic MutexP Parameters |
| CNVS_Attrs | NVS attributes |
| CNVS_Config | NVS Global configuration |
| CNVS_FxnTable | The definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation |
| CNVS_Params | NVS Parameters |
| CNVSCC26XX_CmdSetCopyBlockArgs | NVSCC26XX command structure for setting copy block |
| CNVSCC26XX_HWAttrs | NVSCC26XX attributes |
| CNVSCC26XX_Object | |
| CNVSCC3200_CmdSetCopyBlockArgs | NVSCC3200 command structure for setting copy block |
| CNVSCC3200_HWAttrs | NVSCC3200 attributes |
| CNVSCC3200_Object | |
| CNVSMSP432_CmdSetCopyBlockArgs | NVSMSP432 command structure for setting copy block |
| CNVSMSP432_HWAttrs | NVSMSP432 attributes |
| CNVSMSP432_Object | |
| CNVSTiva_CmdSetCopyBlockArgs | NVSTiva command structure for setting copy block |
| CNVSTiva_HWAttrs | NVSTiva attributes |
| CNVSTiva_Object | |
| CPDMCC26XX_BufferRequest | A PDMCC26XX_BufferRequest data structure is used with PDMCC26XX_requestBuffer() |
| CPDMCC26XX_Config | The PDMCC26XX_Config structure contains a set of pointers used to characterize the PDMCC26XX driver implementation |
| CPDMCC26XX_HWAttrs | PDMCC26XX Hardware attributes |
| CPDMCC26XX_I2S_AudioClockConfig | PDMCC26XX_I2S Audio Clock configuration |
| CPDMCC26XX_I2S_AudioFormatConfig | PDMCC26XX_I2S Hardware configuration |
| CPDMCC26XX_I2S_AudioPinConfig | PDMCC26XX_I2S Audio Pin configuration |
| CPDMCC26XX_I2S_BufferRelease | A PDMCC26XX_I2S_BufferRelease data structure is used with PDMCC26XX_I2S_releaseBuffer() |
| CPDMCC26XX_I2S_BufferRequest | A PDMCC26XX_I2S_BufferRequest data structure is used with PDMCC26XX_I2S_requestBuffer() |
| CPDMCC26XX_I2S_Config | The PDMCC26XX_I2S_Config structure contains a set of pointers used to characterize the PDMCC26XX_I2S driver implementation |
| CPDMCC26XX_I2S_HWAttrs | PDMCC26XX_I2S Hardware attributes |
| CPDMCC26XX_I2S_Object | PDMCC26XX_I2S Object |
| CPDMCC26XX_I2S_Params | PDMCC26XX I2S Parameters are used when calling PDMCC26XX_I2S_open() |
| CPDMCC26XX_I2S_StreamNotification | A PDMCC26XX_I2S_StreamNotification data structure is used with PDMCC26XX_I2S_CallbackFxn(). Provides notification about available buffers and potential errors |
| CPDMCC26XX_metaData | Metadata associated with an array of PCM data |
| CPDMCC26XX_Object | PDMCC26XX Object |
| CPDMCC26XX_Params | PDMCC26XX Parameters are used to with the PDMCC26XX_open() call. Default values for these parameters are set using PDMCC26XX_Params_init() |
| CPDMCC26XX_pcmBuffer | PCM buffer pointed to in a PDMCC26XX_BufferRequest |
| CPDMCC26XX_StreamNotification | A PDMCC26XX_StreamNotification data structure is used with PDMCC26XX_CallbackFxn(). Provides notification about available buffers and potential errors |
| CPIN_State_s | Underlying data structure for type PIN_State |
| CPINCC26XX_HWAttrs | PINCC26XX Hardware attributes |
| CPower_NotifyObj | Power notify object structure |
| CPowerCC26XX_Config | Global configuration structure |
| CPowerCC26XX_ModuleState | Internal module state |
| CPowerCC26XX_ResourceRecord | Power resource database record format |
| CPowerCC3200_ConfigV1 | Power global configuration |
| CPowerCC3200_MCURegisters | MCU core registers that need to be save on entering LPDS |
| CPowerCC3200_ModuleState | Internal module state |
| CPowerCC3200_NVICRegisters | NVIC registers that need to be save on entering LPDS |
| CPowerCC3200_ParkInfo | Used to specify parking of a pin during LPDS |
| CPowerCC3200_SaveRegisters | Struct of context registers to save on entering LPDS |
| CPowerCC3200_Wakeup | For wakeup from LPDS or shutdown configuration |
| CPowerMSP432_ConfigV1 | Power global configuration (MSP432-specific) |
| CPowerMSP432_Freqs | Structure holding device frequencies (in Hz) |
| CPWM_Config | PWM Global configuration |
| CPWM_FxnTable | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
| CPWM_Params | PWM Parameters |
| CPWMTimerCC26XX_HwAttrs | PWMTimer26XX Hardware attributes |
| CPWMTimerCC26XX_Object | PWMTimer26XX Object |
| CPWMTimerCC3200_HWAttrsV1 | PWMTimerCC3200 Hardware attributes |
| CPWMTimerCC3200_Object | PWMTimerCC3200 Object |
| CPWMTimerMSP432_HWAttrsV1 | PWMTimerMSP432 Hardware attributes |
| CPWMTimerMSP432_Object | PWMTimerMSP432 Object |
| CPWMTimerMSP432_Status | PWMTimerMSP432_Status |
| CPWMTimerTiva_HWAttrsV1 | PWMTimerTiva Hardware attributes |
| CPWMTimerTiva_Object | PWMTimerTiva Object |
| CPWMTiva_HWAttrsV1 | PWMTiva Hardware attributes |
| CPWMTiva_Object | PWMTiva Object |
| CPWMTiva_Status | PWMTiva_Status |
| CRF_AccessParams | RF request access parameter struct RF request access command parameters are used with the RF_requestAccess() call |
| CRF_InfoVal | RF_getParamsVal used to input and return RF driver paramters with RF_getParams() |
| CRF_Mode | Struct defining operating mode of RF driver |
| CRF_Object | Struct used to store RF client state and configuration Pointer to an RF_Object is used as handles (RF_Handle) in interactions with the RF driver |
| CRF_Params | RF parameter struct RF parameters are used with the RF_open() and RF_Params_init() call |
| CRF_RadioSetup | Union of the different flavors of RADIO_SETUP commands |
| CRF_ScheduleCmdParams | RF schedule command parameter struct RF schedule command parameters are used with the RF_scheduleCmd() call |
| CRFCC26XX_HWAttrs | RF Hardware attributes |
| CRingBuf_Object | |
| CSDHostCC3200_Config | SDHost Global configuration |
| CSDHostCC3200_HWAttrs | SDHostCC3200 Hardware attributes |
| CSDHostCC3200_Object | SDHostCC3200 Object |
| CSDHostCC3200_Params | SDHostParameters |
| CSDSPI_Config | SDSPI Global configuration |
| CSDSPI_FxnTable | The definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation |
| CSDSPI_Params | SDSPI Parameters |
| CSDSPICC3200_HWAttrs | SDSPICC3200 Hardware attributes |
| CSDSPICC3200_Object | SDSPICC3200 Object |
| CSDSPIEUSCIA_HWAttrsV1 | SDSPIEUSCIA Hardware attributes |
| CSDSPIEUSCIA_Object | SDSPIEUSCIA Object |
| CSDSPIEUSCIB_HWAttrsV1 | SDSPIEUSCIB Hardware attributes |
| CSDSPIEUSCIB_Object | SDSPIEUSCIB Object |
| CSDSPIMSP432_HWAttrs | SDSPIMSP432 Hardware attributes |
| CSDSPIMSP432_Object | SDSPIMSP432 Object |
| CSDSPITiva_HWAttrs | SDSPITiva Hardware attributes |
| CSDSPITiva_Object | SDSPITiva Object |
| CSDSPIUSCIA_HWAttrs | SDSPIUSCIA Hardware attributes |
| CSDSPIUSCIA_Object | SDSPIUSCIA Object |
| CSDSPIUSCIB_HWAttrs | SDSPIUSCIB Hardware attributes |
| CSDSPIUSCIB_Object | SDSPIUSCIB Object |
| CSemaphoreP_Params | Basic SemaphoreP Parameters |
| CSPI_Config | SPI Global configuration |
| CSPI_FxnTable | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
| CSPI_Params | SPI Parameters |
| CSPI_Transaction | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
| CSPICC26XXDMA_HWAttrsV1 | SPICC26XXDMA Hardware attributes |
| CSPICC26XXDMA_Object | SPICC26XXDMA Object |
| CSPICC3200DMA_HWAttrs | SPICC3200DMA Hardware attributes |
| CSPICC3200DMA_Object | SPICC3200DMA Object |
| CSPIEUSCIADMA_HWAttrs | SPIEUSCIADMA Hardware attributes |
| CSPIEUSCIADMA_Object | SPIEUSCIADMA Object |
| CSPIEUSCIBDMA_HWAttrs | SPIEUSCIBDMA Hardware attributes |
| CSPIEUSCIBDMA_Object | SPIEUSCIBDMA Object |
| CSPIMSP432DMA_HWAttrs | SPIMSP432DMA Hardware attributes These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP430Ware these definitions are found in: |
| CSPIMSP432DMA_Object | SPIMSP432DMA Object |
| CSPITivaDMA_HWAttrs | SPITivaDMA Hardware attributes |
| CSPITivaDMA_Object | SPITivaDMA Object |
| CSPIUSCIADMA_HWAttrs | SPIUSCIADMA Hardware attributes |
| CSPIUSCIADMA_Object | SPIUSCIADMA Object |
| CSPIUSCIBDMA_HWAttrs | SPIUSCIBDMA Hardware attributes |
| CSPIUSCIBDMA_Object | SPIUSCIBDMA Object |
| CtContext | |
| CtDisplay | This structure defines the characteristics of a display driver |
| CtDisplayFxns | This structure defines the implementation of a display driver |
| CtFont | This structure describes a font used for drawing text onto the screen |
| CtFontEx | |
| CtImage | This structure defines the characteristics of a Bitmap Image |
| CtRectangle | |
| CUART_Config | UART Global configuration |
| CUART_FxnTable | The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation |
| CUART_Params | UART Parameters |
| CUARTCC26XX_HWAttrsV1 | UARTCC26XX Hardware attributes |
| CUARTCC26XX_Object | UARTCC26XX Object |
| CUARTCC3200_FxnSet | Complement set of read functions to be used by the UART ISR and UARTCC3200_read(). Internal use only |
| CUARTCC3200_HWAttrs | UARTCC3200 Hardware attributes |
| CUARTCC3200_Object | UARTCC3200 Object |
| CUARTCC3200DMA_HWAttrs | UARTCC3200DMA Hardware attributes |
| CUARTCC3200DMA_Object | UARTCC3200DMA Object |
| CUARTEUSCIA_BaudrateConfig | UARTEUSCIA Baudrate configuration |
| CUARTEUSCIA_HWAttrs | UARTEUSCIA Hardware attributes |
| CUARTEUSCIA_Object | UARTEUSCIA Object |
| CUARTMSP432_BaudrateConfig | UARTMSP432 Baudrate configuration |
| CUARTMSP432_FxnSet | Complement set of read functions to be used by the UART ISR and UARTMSP432_read(). Internal use only |
| CUARTMSP432_HWAttrs | UARTMSP432 Hardware attributes |
| CUARTMSP432_Object | UARTMSP432 Object |
| CUARTTiva_FxnSet | Complement set of read functions to be used by the UART ISR and UARTTiva_read(). Internal use only |
| CUARTTiva_HWAttrs | UARTTiva Hardware attributes |
| CUARTTiva_Object | UARTTiva Object |
| CUARTTivaDMA_HWAttrs | UARTTivaDMA Hardware attributes |
| CUARTTivaDMA_Object | UARTTivaDMA Object |
| CUARTUSCIA_BaudrateConfig | UARTUSCIA Baudrate configuration |
| CUARTUSCIA_HWAttrs | UARTUSCIA Hardware attributes |
| CUARTUSCIA_Object | UARTUSCIA Object |
| CUDMACC26XX_Config | UDMACC26XX Global configuration |
| CUDMACC26XX_HWAttrs | UDMACC26XX hardware attributes |
| CUDMACC26XX_Object | UDMACC26XX object |
| CUDMACC3200_Config | UDMACC3200 Global configuration |
| CUDMACC3200_HWAttrs | UDMACC3200 Hardware attributes |
| CUDMACC3200_Object | UDMACC3200 object |
| CUDMAMSP432_Config | UDMAMSP432 Global configuration |
| CUDMAMSP432_HWAttrs | UDMAMSP432 Hardware attributes |
| CUDMAMSP432_Object | UDMAMSP432 object |
| CUSBMSCHFatFs_Config | USBMSCHFatFs Global configuration |
| CUSBMSCHFatFs_FxnTable | The definition of a USBMSCHFatFs function table that contains the required set of functions to control a specific USBMSCHFatFs driver implementation |
| CUSBMSCHFatFs_Params | USBMSCHFatFs Parameters |
| CUSBMSCHFatFsTiva_HWAttrs | USBMSCHFatFsTiva Hardware attributes |
| CUSBMSCHFatFsTiva_Object | USBMSCHFatFsTiva Object |
| CWatchdog_Config | Watchdog Global configuration |
| CWatchdog_FxnTable | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
| CWatchdog_Params | Watchdog Parameters |
| CWatchdogCC26XX_HWAttrs | Watchdog hardware attributes for CC26XX |
| CWatchdogCC26XX_Object | Watchdog Object for CC26XX |
| CWatchdogCC3200_HWAttrs | Watchdog hardware attributes for CC3200 |
| CWatchdogCC3200_Object | Watchdog Object for CC3200 |
| CWatchdogMSP430_HWAttrs | Watchdog hardware attributes for MSP430 |
| CWatchdogMSP430_Object | Watchdog Object for MSP430 |
| CWatchdogMSP432_HWAttrs | Watchdog hardware attributes for MSP432 These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432Ware these definitions are found in: |
| CWatchdogMSP432_Object | Watchdog Object for MSP432 |
| CWatchdogTiva_HWAttrs | Watchdog hardware attributes for Tiva |
| CWatchdogTiva_Object | Watchdog Object for Tiva |
| CWiFi_Config | WiFi Global configuration |
| CWiFi_FxnTable | The definition of a WiFi function table that contains the required set of functions to control a specific WiFi driver implementation |
| CWiFi_Params | WiFi Parameters |
| CWiFiCC3100_HWAttrs | WiFiCC3100 Hardware attributes |
| CWiFiCC3100_Object | WiFiCC3100 Object |
| CWiFiCC3200_HWAttrs | WiFiCC3200 Hardware attributes |
| CWiFiCC3200_Object | WiFiCC3200 Object |