39 #ifndef __COMMON_CMD_H
40 #define __COMMON_CMD_H
44 #define __RFC_STRUCT __attribute__ ((aligned (4)))
121 uint8_t triggerType:4;
138 #define CMD_NOP 0x0801
147 uint8_t triggerType:4;
164 #define CMD_RADIO_SETUP 0x0802
173 uint8_t triggerType:4;
196 uint16_t frontEndMode:3;
203 uint16_t analogCfgMode:6;
205 uint16_t bNoFsPowerUp:1;
223 #define CMD_FS 0x0803
232 uint8_t triggerType:4;
261 #define CMD_FS_OFF 0x0804
270 uint8_t triggerType:4;
287 #define CMD_RX 0x0805
296 uint8_t triggerType:4;
308 uint16_t endianness:1;
309 uint16_t numHdrBits:6;
314 uint16_t bCrcIncSw:1;
316 uint16_t bCrcIncHdr:1;
318 uint16_t bReportCrc:1;
329 uint16_t numLenBits:4;
330 uint16_t lenFieldPos:5;
331 uint16_t lenOffset:7;
337 uint8_t triggerType:4;
359 #define CMD_TX 0x0806
368 uint8_t triggerType:4;
380 uint16_t endianness:1;
381 uint16_t numHdrBits:6;
386 uint16_t bCrcIncSw:1;
388 uint16_t bCrcIncHdr:1;
401 #define CMD_RX_TEST 0x0807
410 uint8_t triggerType:4;
430 uint8_t triggerType:4;
445 #define CMD_TX_TEST 0x0808
454 uint8_t triggerType:4;
469 uint8_t whitenMode:2;
479 uint8_t triggerType:4;
494 #define CMD_SYNC_STOP_RAT 0x0809
503 uint8_t triggerType:4;
523 #define CMD_SYNC_START_RAT 0x080A
532 uint8_t triggerType:4;
552 #define CMD_COUNT 0x080B
561 uint8_t triggerType:4;
580 #define CMD_FS_POWERUP 0x080C
589 uint8_t triggerType:4;
608 #define CMD_FS_POWERDOWN 0x080D
617 uint8_t triggerType:4;
634 #define CMD_SCH_IMM 0x0810
643 uint8_t triggerType:4;
663 #define CMD_COUNT_BRANCH 0x0812
672 uint8_t triggerType:4;
692 #define CMD_PATTERN_CHECK 0x0813
701 uint8_t triggerType:4;
713 uint16_t operation:2;
721 uint16_t signExtend:5;
738 #define CMD_ABORT 0x0401
747 #define CMD_STOP 0x0402
756 #define CMD_GET_RSSI 0x0403
765 #define CMD_UPDATE_RADIO_SETUP 0x0001
776 #define CMD_TRIGGER 0x0404
786 #define CMD_GET_FW_INFO 0x0002
799 #define CMD_START_RAT 0x0405
808 #define CMD_PING 0x0406
817 #define CMD_READ_RFREG 0x0601
828 #define CMD_ADD_DATA_ENTRY 0x0005
840 #define CMD_REMOVE_DATA_ENTRY 0x0006
852 #define CMD_FLUSH_QUEUE 0x0007
864 #define CMD_CLEAR_RX 0x0008
875 #define CMD_REMOVE_PENDING_ENTRIES 0x0009
887 #define CMD_SET_RAT_CMP 0x000A
899 #define CMD_SET_RAT_CPT 0x0603
906 uint16_t bRepeated:1;
907 uint16_t inputMode:2;
920 #define CMD_DISABLE_RAT_CH 0x0408
930 #define CMD_SET_RAT_OUTPUT 0x0604
935 uint16_t outputSel:3;
936 uint16_t outputMode:3;
951 #define CMD_ARM_RAT_CH 0x0409
961 #define CMD_DISARM_RAT_CH 0x040A
971 #define CMD_SET_TX_POWER 0x0010
978 uint16_t tempCoeff:7;
986 #define CMD_UPDATE_FS 0x0011
1001 #define CMD_BUS_REQUEST 0x040E
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint16_t commandNo
The command ID number 0x0408.
uint16_t startOffset
The start of free RAM.
uint16_t commandNo
The command ID number 0x0007.
uint16_t counter
Counter. On start, the radio CPU decrements the value, and the end status of the operation differs if...
struct __RFC_STRUCT rfc_CMD_TRIGGER_s rfc_CMD_TRIGGER_t
struct __RFC_STRUCT rfc_CMD_STOP_s rfc_CMD_STOP_t
uint8_t ratCh
The radio timer channel number.
uint16_t commandNo
The command ID number 0x0803.
struct __RFC_STRUCT rfc_CMD_ARM_RAT_CH_s rfc_CMD_ARM_RAT_CH_t
uint16_t counter
Counter. On start, the radio CPU decrements the value, and the end status of the operation differs if...
struct __RFC_STRUCT rfc_CMD_SYNC_STOP_RAT_s rfc_CMD_SYNC_STOP_RAT_t
uint8_t mode
The main mode to use 0x00: BLE 0x01: IEEE 802.15.4 0x02: 2 Mbps GFSK 0x05: 5 Mbps coded 8-FSK 0x...
struct __RFC_STRUCT rfc_CMD_UPDATE_FS_s rfc_CMD_UPDATE_FS_t
uint16_t commandNo
The command ID number 0x0806.
ratmr_t endTime
Time to end the operation.
uint16_t commandNo
The command ID number 0x0801.
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
struct __RFC_STRUCT rfc_CMD_SET_RAT_CMP_s rfc_CMD_SET_RAT_CMP_t
struct __RFC_STRUCT rfc_CMD_RX_TEST_s rfc_CMD_RX_TEST_t
ratmr_t endTime
Time to end the operation.
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint8_t * pFirstEntry
Pointer to the first entry that was removed.
uint16_t txPower
Transmit power.
ratmr_t rat0
The desired RAT timer value corresponding to the value the RAT would have had when the RTC was zero...
struct __RFC_STRUCT rfc_CMD_CLEAR_RX_s rfc_CMD_CLEAR_RX_t
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint8_t midPrecal
Mid pre-calibration value to use when bOverrideCalib and bSkipCoarseCalib are both 1...
struct __RFC_STRUCT rfc_CMD_START_RAT_s rfc_CMD_START_RAT_t
uint16_t commandNo
The command ID number 0x0002.
uint16_t commandNo
The command ID number 0x0409.
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint16_t commandNo
The command ID number 0x0808.
uint16_t freeRamSz
The size of free RAM.
uint16_t commandNo
The command ID number 0x0008.
dataQueue_t * pQueue
Pointer to the queue structure to be flushed.
dataQueue_t * pQueue
Pointer to the queue structure to which the entry will be added.
uint16_t commandNo
The command ID number 0x0603.
uint16_t commandNo
The command ID number 0x0001.
dataQueue_t * pQueue
Pointer to the queue structure from which the entry will be removed.
uint8_t * pEntry
Pointer to the entry.
struct __RFC_STRUCT rfc_CMD_FS_POWERDOWN_s rfc_CMD_FS_POWERDOWN_t
struct __RFC_STRUCT rfc_CMD_RADIO_SETUP_s rfc_CMD_RADIO_SETUP_t
dataQueue_t * pQueue
Pointer to the queue structure to be cleared.
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
uint16_t fractFreq
Fractional part of the frequency to tune to.
struct __RFC_STRUCT rfc_CMD_COUNT_BRANCH_s rfc_CMD_COUNT_BRANCH_t
uint16_t tdcPrecal
TDC pre-calibration value to use when bOverrideCalib and bSkipCoarseCalib are both 1...
uint16_t maxLen
Maximum number of bytes in the received packet (including header, excluding CRC)
uint16_t versionNo
Firmware version number.
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
uint32_t mask
Bit mask to apply before comparison.
uint32_t cmdstaVal
Value as would be returned in CMDSTA.
uint32_t syncWord
Sync word to transmit.
uint16_t commandNo
The command ID number 0x040A.
struct __RFC_STRUCT rfc_radioOp_s rfc_radioOp_t
struct __RFC_STRUCT rfc_CMD_REMOVE_DATA_ENTRY_s rfc_CMD_REMOVE_DATA_ENTRY_t
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint16_t commandNo
The command ID number.
uint16_t commandNo
The command ID number 0x080B.
uint16_t commandNo
The command ID number 0x0006.
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint16_t nRxNok
Counter of number of received packets with CRC error and first sync word.
uint32_t compareVal
Value to compare to.
uint16_t commandNo
The command ID number 0x0402.
struct __RFC_STRUCT rfc_CMD_FS_s rfc_CMD_FS_t
struct __RFC_STRUCT rfc_CMD_SYNC_START_RAT_s rfc_CMD_SYNC_START_RAT_t
int8_t rssi
RSSI of received packet.
struct __RFC_STRUCT rfc_CMD_SCH_IMM_s rfc_CMD_SCH_IMM_t
dataQueue_t * pQueue
Pointer to the queue structure to be flushed.
uint16_t commandNo
The command ID number 0x0401.
ratmr_t endTime
Time to end the operation.
uint16_t address
The offset from the start of the RF core HW register bank (0x40040000)
uint16_t commandNo
The command ID number 0x040E.
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
uint16_t commandNo
The command ID number 0x000A.
uint8_t bSysBusNeeded
0: System bus may sleep 1: System bus access needed
struct __RFC_STRUCT rfc_CMD_BUS_REQUEST_s rfc_CMD_BUS_REQUEST_t
uint8_t * pTxPkt
Pointer to buffer for transmitted packet.
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
rfc_radioOp_t * pNextOpIfOk
Pointer to next operation if comparison result was true.
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
struct __RFC_STRUCT rfc_CMD_REMOVE_PENDING_ENTRIES_s rfc_CMD_REMOVE_PENDING_ENTRIES_t
struct __RFC_STRUCT rfc_CMD_READ_RFREG_s rfc_CMD_READ_RFREG_t
struct __RFC_STRUCT rfc_CMD_PATTERN_CHECK_s rfc_CMD_PATTERN_CHECK_t
uint16_t availRatCh
Bitmap of available RAT channels.
uint8_t * pFirstEntry
Pointer to the first entry that was removed.
struct __RFC_STRUCT rfc_CMD_FS_OFF_s rfc_CMD_FS_OFF_t
uint16_t commandNo
The command ID number 0x0805.
uint16_t nRx2Ok
Counter of number of received packets with CRC OK and second sync word; may safely be omitted if pktC...
struct __RFC_STRUCT rfc_CMD_TX_TEST_s rfc_CMD_TX_TEST_t
uint16_t frequency
The frequency in MHz to tune to, compensated for LO divider setting.
uint16_t commandNo
The command ID number 0x0809.
struct __RFC_STRUCT rfc_CMD_NOP_s rfc_CMD_NOP_t
uint32_t value
Returned value of the register.
struct __RFC_STRUCT rfc_command_s rfc_command_t
uint16_t pktLen
Number of bytes in the transmitted packet.
uint16_t commandNo
The command ID number 0x0813.
uint16_t commandNo
The command ID number 0x080C.
uint16_t commandNo
The command ID number 0x0601.
struct __RFC_STRUCT rfc_CMD_SET_RAT_CPT_s rfc_CMD_SET_RAT_CPT_t
uint32_t ratmr_t
Type definition for RAT.
uint16_t commandNo
The command ID number 0x0005.
ratmr_t rat0
The returned RAT timer value corresponding to the value the RAT would have had when the RTC was zero...
uint16_t commandNo
The command ID number.
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint32_t * pRegOverride
Pointer to a list of hardware and configuration registers to override. If NULL, no override is used...
uint32_t syncWord2
Secondary sync word to receive if pktConfig.bDualSw = 1.
uint16_t commandNo
The command ID number 0x0405.
struct __RFC_STRUCT rfc_CMD_SET_TX_POWER_s rfc_CMD_SET_TX_POWER_t
uint8_t ktPrecal
KT pre-calibration value to use when bOverrideCalib and bSkipCoarseCalib are both 1...
struct __RFC_STRUCT rfc_CMD_DISABLE_RAT_CH_s rfc_CMD_DISABLE_RAT_CH_t
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint16_t recLen
Number of bytes written to receive buffer.
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint8_t ratCh
The radio timer channel number.
uint16_t commandNo
The command ID number 0x0802.
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
struct __RFC_STRUCT rfc_CMD_ABORT_s rfc_CMD_ABORT_t
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
ratmr_t compareTime
The time at which the compare occurs.
struct __RFC_STRUCT rfc_CMD_UPDATE_RADIO_SETUP_s rfc_CMD_UPDATE_RADIO_SETUP_t
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint16_t commandNo
The command ID number 0x0010.
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint16_t commandNo
The command ID number 0x0804.
uint8_t triggerNo
Command trigger number.
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint32_t syncWord
Sync word to receive.
uint16_t commandNo
The command ID number 0x0011.
uint16_t fractFreq
Fractional part of the frequency to tune to.
uint8_t ratCh
The radio timer channel number.
uint32_t syncWord
Sync word to use for receiver.
struct __RFC_STRUCT rfc_CMD_PING_s rfc_CMD_PING_t
uint8_t * pEntry
Pointer to the entry that was removed.
uint16_t commandNo
The command ID number 0x0403.
uint32_t * pRegOverride
Pointer to a list of hardware and configuration registers to override.
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
Type definition for a data queue.
struct __RFC_STRUCT rfc_CMD_FLUSH_QUEUE_s rfc_CMD_FLUSH_QUEUE_t
struct __RFC_STRUCT rfc_CMD_RX_s rfc_CMD_RX_t
struct __RFC_STRUCT rfc_CMD_TX_s rfc_CMD_TX_t
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
struct __RFC_STRUCT rfc_CMD_GET_FW_INFO_s rfc_CMD_GET_FW_INFO_t
uint16_t frequency
The frequency in MHz to tune to.
uint16_t commandNo
The command ID number 0x0807.
uint8_t ratCh
The radio timer channel number.
uint32_t syncWord
Sync word to use for transmitter.
uint8_t * pValue
Pointer to read from, or offset from last Rx entry if patternOpt.bRxVal == 1.
struct __RFC_STRUCT rfc_CMD_DISARM_RAT_CH_s rfc_CMD_DISARM_RAT_CH_t
uint16_t commandNo
The command ID number 0x0810.
struct __RFC_STRUCT rfc_CMD_FS_POWERUP_s rfc_CMD_FS_POWERUP_t
uint16_t commandNo
The command ID number 0x080D.
uint32_t * pRegOverride
Pointer to a list of hardware and configuration registers to override. If NULL, no override is used...
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint32_t cmdrVal
Value as would be written to CMDR.
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
struct __RFC_STRUCT rfc_CMD_GET_RSSI_s rfc_CMD_GET_RSSI_t
uint16_t nRxOk
Counter of number of received packets with CRC OK and first sync word.
uint16_t commandNo
The command ID number 0x0406.
struct __RFC_STRUCT rfc_CMD_COUNT_s rfc_CMD_COUNT_t
uint16_t txWord
Value to send to the modem before whitening.
struct __RFC_STRUCT rfc_CMD_ADD_DATA_ENTRY_s rfc_CMD_ADD_DATA_ENTRY_t
uint16_t commandNo
The command ID number 0x0812.
ratmr_t timeStamp
Time stamp of received packet.
uint16_t status
An integer telling the status of the command. This value is updated by the radio CPU during operation...
uint16_t commandNo
The command ID number 0x0009.
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
struct __RFC_STRUCT rfc_CMD_SET_RAT_OUTPUT_s rfc_CMD_SET_RAT_OUTPUT_t
uint16_t commandNo
The command ID number 0x0404.
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
uint8_t * pRecPkt
Pointer to buffer for received packet. NULL: Do not store the contents.
uint16_t commandNo
The command ID number 0x080A.
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
uint16_t commandNo
The command ID number 0x0604.
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)
ratmr_t startTime
Absolute or relative start time (depending on the value of startTrigger)