CC13xx Driver Library
rfc_CMD_NOP_s Struct Reference

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0801. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips if the rule involves skipping. More...
 
condition
 

Detailed Description

Definition at line 139 of file rf_common_cmd.h.

Field Documentation

uint8_t rfc_CMD_NOP_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

Definition at line 148 of file rf_common_cmd.h.

uint16_t rfc_CMD_NOP_s::commandNo

The command ID number 0x0801.

Definition at line 140 of file rf_common_cmd.h.

struct { ... } rfc_CMD_NOP_s::condition
uint8_t rfc_CMD_NOP_s::nSkip

Number of skips if the rule involves skipping.

Definition at line 156 of file rf_common_cmd.h.

uint8_t rfc_CMD_NOP_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

Definition at line 151 of file rf_common_cmd.h.

rfc_radioOp_t* rfc_CMD_NOP_s::pNextOp

Pointer to the next operation to run after this operation is done.

Definition at line 144 of file rf_common_cmd.h.

uint8_t rfc_CMD_NOP_s::rule

Condition for running next command: Rule for how to proceed.

Definition at line 155 of file rf_common_cmd.h.

ratmr_t rfc_CMD_NOP_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

Definition at line 145 of file rf_common_cmd.h.

struct { ... } rfc_CMD_NOP_s::startTrigger

Identification of the trigger that starts the operation.

uint16_t rfc_CMD_NOP_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

Definition at line 141 of file rf_common_cmd.h.

uint8_t rfc_CMD_NOP_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

Definition at line 150 of file rf_common_cmd.h.

uint8_t rfc_CMD_NOP_s::triggerType

The type of trigger.

Definition at line 147 of file rf_common_cmd.h.