#include <rf_common_cmd.h>
Data Fields | |
uint16_t | commandNo |
The command ID number 0x0803. More... | |
uint16_t | status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More... | |
rfc_radioOp_t * | pNextOp |
Pointer to the next operation to run after this operation is done. More... | |
ratmr_t | startTime |
Absolute or relative start time (depending on the value of startTrigger ) More... | |
struct { | |
uint8_t triggerType:4 | |
The type of trigger. More... | |
uint8_t bEnaCmd:1 | |
0: No alternative trigger command 1: CMD_TRIGGER can be used as an alternative trigger More... | |
uint8_t triggerNo:2 | |
The trigger number of the CMD_TRIGGER command that triggers this action. More... | |
uint8_t pastTrig:1 | |
0: A trigger in the past is never triggered, or for start of commands, give an error 1: A trigger in the past is triggered as soon as possible More... | |
} | startTrigger |
Identification of the trigger that starts the operation. More... | |
struct { | |
uint8_t rule:4 | |
Condition for running next command: Rule for how to proceed. More... | |
uint8_t nSkip:4 | |
Number of skips if the rule involves skipping. More... | |
} | condition |
uint16_t | frequency |
The frequency in MHz to tune to. More... | |
uint16_t | fractFreq |
Fractional part of the frequency to tune to. More... | |
struct { | |
uint8_t bTxMode:1 | |
0: Start synth in Rx mode 1: Start synth in Tx mode More... | |
uint8_t refFreq:6 | |
0: Use default reference frequency Others: Use reference frequency 24 MHz/ refFreq More... | |
} | synthConf |
uint8_t | __dummy0 |
uint8_t | midPrecal |
Mid pre-calibration value to use when bOverrideCalib and bSkipCoarseCalib are both 1. More... | |
uint8_t | ktPrecal |
KT pre-calibration value to use when bOverrideCalib and bSkipCoarseCalib are both 1. More... | |
uint16_t | tdcPrecal |
TDC pre-calibration value to use when bOverrideCalib and bSkipCoarseCalib are both 1. More... | |
Definition at line 224 of file rf_common_cmd.h.
uint8_t rfc_CMD_FS_s::__dummy0 |
Definition at line 251 of file rf_common_cmd.h.
uint8_t rfc_CMD_FS_s::bEnaCmd |
0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger
Definition at line 233 of file rf_common_cmd.h.
uint8_t rfc_CMD_FS_s::bTxMode |
0: Start synth in Rx mode
1: Start synth in Tx mode
Definition at line 246 of file rf_common_cmd.h.
uint16_t rfc_CMD_FS_s::commandNo |
The command ID number 0x0803.
Definition at line 225 of file rf_common_cmd.h.
struct { ... } rfc_CMD_FS_s::condition |
uint16_t rfc_CMD_FS_s::fractFreq |
Fractional part of the frequency to tune to.
Definition at line 244 of file rf_common_cmd.h.
uint16_t rfc_CMD_FS_s::frequency |
The frequency in MHz to tune to.
Definition at line 243 of file rf_common_cmd.h.
uint8_t rfc_CMD_FS_s::ktPrecal |
KT pre-calibration value to use when bOverrideCalib
and bSkipCoarseCalib
are both 1.
Definition at line 253 of file rf_common_cmd.h.
uint8_t rfc_CMD_FS_s::midPrecal |
Mid pre-calibration value to use when bOverrideCalib
and bSkipCoarseCalib
are both 1.
Definition at line 252 of file rf_common_cmd.h.
uint8_t rfc_CMD_FS_s::nSkip |
Number of skips if the rule involves skipping.
Definition at line 241 of file rf_common_cmd.h.
uint8_t rfc_CMD_FS_s::pastTrig |
0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible
Definition at line 236 of file rf_common_cmd.h.
rfc_radioOp_t* rfc_CMD_FS_s::pNextOp |
Pointer to the next operation to run after this operation is done.
Definition at line 229 of file rf_common_cmd.h.
uint8_t rfc_CMD_FS_s::refFreq |
0: Use default reference frequency
Others: Use reference frequency 24 MHz/refFreq
Definition at line 248 of file rf_common_cmd.h.
uint8_t rfc_CMD_FS_s::rule |
Condition for running next command: Rule for how to proceed.
Definition at line 240 of file rf_common_cmd.h.
ratmr_t rfc_CMD_FS_s::startTime |
Absolute or relative start time (depending on the value of startTrigger
)
Definition at line 230 of file rf_common_cmd.h.
struct { ... } rfc_CMD_FS_s::startTrigger |
Identification of the trigger that starts the operation.
uint16_t rfc_CMD_FS_s::status |
An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.
Definition at line 226 of file rf_common_cmd.h.
struct { ... } rfc_CMD_FS_s::synthConf |
uint16_t rfc_CMD_FS_s::tdcPrecal |
TDC pre-calibration value to use when bOverrideCalib
and bSkipCoarseCalib
are both 1.
Definition at line 254 of file rf_common_cmd.h.
uint8_t rfc_CMD_FS_s::triggerNo |
The trigger number of the CMD_TRIGGER command that triggers this action.
Definition at line 235 of file rf_common_cmd.h.
uint8_t rfc_CMD_FS_s::triggerType |
The type of trigger.
Definition at line 232 of file rf_common_cmd.h.