CC13xx Driver Library
rfc_CMD_REMOVE_DATA_ENTRY_s Struct Reference

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0006. More...
 
uint16_t __dummy0
 
dataQueue_tpQueue
 Pointer to the queue structure from which the entry will be removed. More...
 
uint8_t * pEntry
 Pointer to the entry that was removed. More...
 

Detailed Description

Definition at line 841 of file rf_common_cmd.h.

Field Documentation

uint16_t rfc_CMD_REMOVE_DATA_ENTRY_s::__dummy0

Definition at line 843 of file rf_common_cmd.h.

uint16_t rfc_CMD_REMOVE_DATA_ENTRY_s::commandNo

The command ID number 0x0006.

Definition at line 842 of file rf_common_cmd.h.

uint8_t* rfc_CMD_REMOVE_DATA_ENTRY_s::pEntry

Pointer to the entry that was removed.

Definition at line 845 of file rf_common_cmd.h.

dataQueue_t* rfc_CMD_REMOVE_DATA_ENTRY_s::pQueue

Pointer to the queue structure from which the entry will be removed.

Definition at line 844 of file rf_common_cmd.h.