![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
Defines instance status parameters (read-only). More...
#include <iaudenc1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
Extended error information. | |
XDM1_SingleBufDesc | data |
XDM_AlgBufInfo | bufInfo |
XDAS_Int32 | validFlag |
XDAS_Int32 | lfeFlag |
XDAS_Int32 | bitRate |
XDAS_Int32 | sampleRate |
XDAS_Int32 | channelMode |
XDAS_Int32 | encMode |
Defines instance status parameters (read-only).
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IAUDENC1_Fxns::control()
XDAS_Int32 IAUDENC1_Status::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IAUDENC1_Status::extendedError |
Extended error information.
XDM1_SingleBufDesc IAUDENC1_Status::data |
Buffer descriptor for data passing.
@remarks This buffer can be used as either input or output, depending on the command. @remarks The buffer will be provided by the application, and returned to the application upon return of the control() call. The algorithm must not retain a pointer to this data. @sa #XDM_GETVERSION
XDM_AlgBufInfo IAUDENC1_Status::bufInfo |
Input and output buffer information.
@sa XDM_AlgBufInfo
XDAS_Int32 IAUDENC1_Status::validFlag |
Flag indicating the validity of the status struct.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
XDAS_Int32 IAUDENC1_Status::lfeFlag |
Flag indicating whether LFE channel data is present or not in the input.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
XDAS_Int32 IAUDENC1_Status::bitRate |
Average bit rate, in bits per second.
@sa IAUDENC1_Params.bitRate @sa IAUDENC1_DynamicParams.bitRate
XDAS_Int32 IAUDENC1_Status::sampleRate |
Sampling frequency in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.
XDAS_Int32 IAUDENC1_Status::channelMode |
Input Channel Mode.
@sa IAUDIO_ChannelMode for valid values. @sa IAUDENC1_Params.channelMode @sa IAUDENC1_DynamicParams.channelMode
XDAS_Int32 IAUDENC1_Status::encMode |
Encoding mode.
@sa IAUDIO_EncMode @sa IAUDENC1_Params.encMode