Codec Engine Application Programming Interface (API)
ce-w08
|
Data Structures | |
struct | IAUDENC1_Obj |
This must be the first field of all IAUDENC1 instance objects. More... | |
struct | IAUDENC1_Params |
Defines the creation time parameters for all IAUDENC1 instance objects. More... | |
struct | IAUDENC1_DynamicParams |
This structure defines the algorithm parameters that can be modified after creation via control() calls. More... | |
struct | IAUDENC1_InArgs |
Defines the input arguments for all IAUDENC1 instance process function. More... | |
struct | IAUDENC1_Status |
Defines instance status parameters (read-only). More... | |
struct | IAUDENC1_OutArgs |
Defines the run time output arguments for all IAUDENC1 instance objects. More... | |
struct | IAUDENC1_Fxns |
Defines all of the operations on IAUDENC1 objects. More... |
Macros | |
#define | IAUDENC1_EOK XDM_EOK |
| |
#define | IAUDENC1_EFAIL XDM_EFAIL |
| |
#define | IAUDENC1_EUNSUPPORTED XDM_EUNSUPPORTED |
|
Typedefs | |
typedef struct IAUDENC1_Obj | IAUDENC1_Obj |
This must be the first field of all IAUDENC1 instance objects. | |
typedef struct IAUDENC1_Obj * | IAUDENC1_Handle |
Opaque handle to an IAUDENC1 objects. | |
typedef struct IAUDENC1_Params | IAUDENC1_Params |
Defines the creation time parameters for all IAUDENC1 instance objects. | |
typedef struct IAUDENC1_DynamicParams | IAUDENC1_DynamicParams |
This structure defines the algorithm parameters that can be modified after creation via control() calls. | |
typedef struct IAUDENC1_InArgs | IAUDENC1_InArgs |
Defines the input arguments for all IAUDENC1 instance process function. | |
typedef struct IAUDENC1_Status | IAUDENC1_Status |
Defines instance status parameters (read-only). | |
typedef struct IAUDENC1_OutArgs | IAUDENC1_OutArgs |
Defines the run time output arguments for all IAUDENC1 instance objects. | |
typedef IALG_Cmd | IAUDENC1_Cmd |
Defines the control commands for the IAUDENC1 module. | |
typedef struct IAUDENC1_Fxns | IAUDENC1_Fxns |
Defines all of the operations on IAUDENC1 objects. |
This is the XDM IAUDENC1 Audio Encoder Interface.
#define IAUDENC1_EOK XDM_EOK |
Success.
#define IAUDENC1_EFAIL XDM_EFAIL |
General failure.
#define IAUDENC1_EUNSUPPORTED XDM_EUNSUPPORTED |
Request is unsupported.
typedef struct IAUDENC1_Obj IAUDENC1_Obj |
This must be the first field of all IAUDENC1 instance objects.
typedef struct IAUDENC1_Obj* IAUDENC1_Handle |
Opaque handle to an IAUDENC1 objects.
typedef struct IAUDENC1_Params IAUDENC1_Params |
Defines the creation time parameters for all IAUDENC1 instance objects.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. typedef struct IAUDENC1_DynamicParams IAUDENC1_DynamicParams |
This structure defines the algorithm parameters that can be modified after creation via control() calls.
@remarks It is not necessary that given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error. @remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IAUDENC1_Fxns::control()
typedef struct IAUDENC1_InArgs IAUDENC1_InArgs |
Defines the input arguments for all IAUDENC1 instance process function.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IAUDENC1_Fxns::process()
typedef struct IAUDENC1_Status IAUDENC1_Status |
Defines instance status parameters (read-only).
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IAUDENC1_Fxns::control()
typedef struct IAUDENC1_OutArgs IAUDENC1_OutArgs |
Defines the run time output arguments for all IAUDENC1 instance objects.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IAUDENC1_Fxns::process()
typedef IALG_Cmd IAUDENC1_Cmd |
Defines the control commands for the IAUDENC1 module.
typedef struct IAUDENC1_Fxns IAUDENC1_Fxns |
Defines all of the operations on IAUDENC1 objects.