![]() |
![]() |
Codec Engine Application Programming Interface (API)
ce-w08
|
This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
#include <iaudenc1.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | bitRate |
XDAS_Int32 | sampleRate |
XDAS_Int32 | channelMode |
XDAS_Int32 | lfeFlag |
XDAS_Int32 | dualMonoMode |
XDAS_Int32 | inputBitsPerSample |
This structure defines the algorithm parameters that can be modified after creation via control() calls.
@remarks It is not necessary that given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error. @remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. @sa IAUDENC1_Fxns::control()
XDAS_Int32 IAUDENC1_DynamicParams::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IAUDENC1_DynamicParams::bitRate |
Average bit rate, in bits per second.
@sa IAUDENC1_Params.bitRate @sa IAUDENC1_Status.bitRate
XDAS_Int32 IAUDENC1_DynamicParams::sampleRate |
Sampling frequency in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.
XDAS_Int32 IAUDENC1_DynamicParams::channelMode |
Input Channel Mode.
@sa IAUDIO_ChannelMode @sa IAUDENC1_Params.channelMode
XDAS_Int32 IAUDENC1_DynamicParams::lfeFlag |
Flag indicating whether LFE channel data is present or not in the input.
Valid values for this field are XDAS_TRUE and XDAS_FALSE.
XDAS_Int32 IAUDENC1_DynamicParams::dualMonoMode |
Mode to indicate type of Dual Mono. Applicable only if channelMode is dualMono
XDAS_Int32 IAUDENC1_DynamicParams::inputBitsPerSample |
Number of input bits per output sample. For example, if there are 16 bits per PCM input sample, this should be set to 16.