Functions |
VIDDEC2_Handle | VIDDEC2_create (Engine_Handle e, String name, VIDDEC2_Params *params) |
| Create an instance of a video decoder algorithm.
|
Int32 | VIDDEC2_process (VIDDEC2_Handle handle, XDM1_BufDesc *inBufs, XDM_BufDesc *outBufs, VIDDEC2_InArgs *inArgs, VIDDEC2_OutArgs *outArgs) |
| Execute the process() method in this instance of a video decoder algorithm.
|
Int32 | VIDDEC2_control (VIDDEC2_Handle handle, VIDDEC2_Cmd id, VIDDEC2_DynamicParams *params, VIDDEC2_Status *status) |
| Execute the control() method in this instance of a video decoder algorithm.
|
Void | VIDDEC2_delete (VIDDEC2_Handle handle) |
| Delete the instance of a video decoder algorithm.
|
XDAS_Int32 | VIDDEC2_processAsync (VIDDEC2_Handle handle, XDM1_BufDesc *inBufs, XDM_BufDesc *outBufs, VIDDEC2_InArgs *inArgs, VIDDEC2_OutArgs *outArgs) |
| Perform asynchronous submission to this instance of a video decoder algorithm.
|
XDAS_Int32 | VIDDEC2_processWait (VIDDEC2_Handle handle, XDM1_BufDesc *inBufs, XDM_BufDesc *outBufs, VIDDEC2_InArgs *inArgs, VIDDEC2_OutArgs *outArgs, UInt timeout) |
| Wait for a return message from a previous invocation of VIDDEC2_processAsync() in this instance of an video decoder algorithm.
|
Detailed Description
This is the VIDDEC2 video decoder interface. Several of the data types in this API are specified by the XDM interface; please see the XDM documentation for those details.
Macro Definition Documentation
General failure. Request is unsupported.
Special value for timeout parameter indicating never timeout.
#define VIDDEC2_VISATYPE "ti.sdo.ce.video2.IVIDDEC2" |
#define VIDDEC2_STUBSNAME "VIDDEC2_STUBS" |
Name of stub functions. Use this name when registering the VIDDEC2_STUBS functions with Engine_addStubFxns.
- See also:
- Engine_addStubFxns
Typedef Documentation
Defines instance status parameters.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
Opaque handle to a VIDDEC2 codec.
This structure defines the parameters necessary to create an instance of a video decoder object.
Defines the input arguments for all IVIDDEC2 instance process function.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
Defines the run time output arguments for all IVIDDEC2 instance objects.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
This structure defines the codec parameters that can be modified after creation via control() calls.
@remarks It is not necessary that a given implementation support all
dynamic parameters to be configurable at run time. If a
particular algorithm does not support run-time updates to
a parameter that the application is attempting to change
at runtime, it may indicate this as an error.
@remarks This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the @c size parameter.
Function Documentation
Create an instance of a video decoder algorithm.
Instance handles must not be concurrently accessed by multiple threads;
each thread must either obtain its own handle (via VIDDEC2_create()) or
explicitly serialize access to a shared handle.
@param[in] e Handle to an opened engine.
@param[in] name String identifier of the type of video decoder
to create.
@param[in] params Creation parameters.
@retval NULL An error has occurred.
@retval non-NULL The handle to the newly created video decoder
instance.
@remarks @c params is optional. If it's not supplied, codec-specific
default params will be used.
@remark Depending on the configuration of the engine opened, this
call may create a local or remote instance of the video
decoder.
@remarks In general, @c name is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated, to be overridden. This optional argument string is of the form <b>":priority"</b>, <b>":priority:flag"</b>, or <b>"::flag"</b>.
Execute the process() method in this instance of a video decoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created video decoder instance. |
[in] | inBufs | A buffer descriptor containing input buffers. |
[out] | outBufs | A buffer descriptor containing output buffers. |
[in] | inArgs | Input Arguments. |
[out] | outArgs | Output Arguments. |
- Precondition:
handle
is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
- Return values:
-
- See also:
- VIDDEC2_create()
-
VIDDEC2_delete()
-
VIDDEC2_control()
-
VIDDEC2_processAsync()
-
VIDDEC2_processWait()
-
IVIDDEC2_Fxns::process() - the reflected algorithm interface, which may contain further usage details.
Execute the control() method in this instance of a video decoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created video decoder instance. |
[in] | id | Command id for xDM control operation. |
[in] | params | Runtime control parameters used for decoding. |
[out] | status | Status info upon completion of decode operation. |
- Precondition:
handle
is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
- Return values:
-
- See also:
- VIDDEC2_create()
-
VIDDEC2_delete()
-
IVIDDEC2_Fxns::process()
Delete the instance of a video decoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created video decoder instance. |
- Precondition:
handle
is a valid (non-NULL) handle which is in the created state.
- Postcondition:
- All resources allocated as part of the VIDDEC2_create() operation (memory, DMA channels, etc.) are freed.
- See also:
- VIDDEC2_create()
Perform asynchronous submission to this instance of a video decoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created video decoder instance. |
[in] | inBufs | A buffer descriptor containing input buffers. |
[out] | outBufs | A buffer descriptor containing output buffers. |
[in] | inArgs | Input Arguments. |
[out] | outArgs | Output Arguments. |
- Precondition:
handle
is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
- Return values:
-
- See also:
- VIDDEC2_create()
-
VIDDEC2_delete()
-
VIDDEC2_control()
-
VIDDEC2_process()
-
VIDDEC2_processWait()
-
IVIDDEC2_Fxns::process()
Wait for a return message from a previous invocation of VIDDEC2_processAsync() in this instance of an video decoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created video decoder instance. |
[in] | inBufs | A buffer descriptor containing input buffers. |
[out] | outBufs | A buffer descriptor containing output buffers. |
[in] | inArgs | Input Arguments. |
[out] | outArgs | Output Arguments. |
[in] | timeout | Amount of "time" to wait (from 0 -> VIDDEC2_FOREVER) |
- Precondition:
handle
is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
- Return values:
-
- See also:
- VIDDEC2_create()
-
VIDDEC2_delete()
-
VIDDEC2_control()
-
VIDDEC2_process()
-
VIDDEC2_processAsync()