DSP/BIOSTM LINK
VERSION
1.65.02.09
OMAP3530 Processor
OMAP2530 Processor
DM6446 Media Processor
DM357 Media Processor
DM6467 Processor
DM6437 Processor
DA8XX Media Processor
OMAPL1xx Media processor
DA850 Media processor
OMAPL138 Media processor
DM648 Processor
TNETV107X
Processor
The documents included with DSP/BIOSTM LINK are listed here under
categories based on their intended usage.
GETTING
STARTED
[UserGuide.pdf]
This document provides information to get started
with using DSP/BIOSTM LINK.
[ProgrammersGuide.pdf]
This document provides information
enabling users to write applications using DSP/BIOSTM LINK.
INSTALLATION
GUIDE FOR OMAP3530 EVM
[InstallGuide_Linux_OMAP3530.pdf]
This document provides information to install DSP/BIOSTM LINK on the development host and
setup the development platform.
INSTALLATION GUIDE FOR
OMAP2530 EVM
[InstallGuide_Linux_OMAP2530.pdf]
This document provides information to install DSP/BIOSTM LINK on the development host and
setup the development platform.
INSTALLATION
GUIDE FOR DM6446, DM6467 AND DM6467 MEDIA PROCESSOR
[InstallGuide_Linux_DM6446_DM6467_DM6467T.pdf]
This document provides information to install DSP/BIOSTM LINK on the development host and
setup the development platform.
INSTALLATION GUIDE FOR DM357
MEDIA PROCESSOR
[InstallGuide_Linux_DM357.pdf]
This document provides information to install
DSP/BIOSTM
LINK on the development host and setup the development platform.
[InstallGuide_Linux_PCI.pdf]
This document provides information to install
DSP/BIOSTM
LINK on the development host and setup the development platform.
[InstallGuide_Linux_PCI.pdf]
This document provides information
to install DSP/BIOSTM LINK on the development host and setup the development platform.
INSTALLATION GUIDE FOR DA8XX MEDIA
PROCESSOR
[InstallGuide_Linux_DA8xx.pdf]
This document provides information
to install DSP/BIOSTM LINK on the development host and setup the development platform.
INSTALLATION GUIDE FOR OMAPL1XX MEDIA
PROCESSOR
[InstallGuide_Linux_OMAPL1xx.pdf]
This document provides information
to install DSP/BIOSTM LINK on the development host and setup the development platform.
INSTALLATION GUIDE FOR OMAPL138 MEDIA
PROCESSOR
[InstallGuide_Linux_OMAPL138.pdf]
This document provides information
to install DSP/BIOSTM LINK on the development host and setup the development platform.
INSTALLATION GUIDE FOR DA850 MEDIA
PROCESSOR
[InstallGuide_Linux_DA850.pdf]
This document provides information
to install DSP/BIOSTM LINK on the development host and setup the development platform.
PLATFORM GUIDE FOR OMAP3530 EVM
[PlatformGuide_OMAP3530.pdf]
This document provides
platform and device-specific information for the OMAP3530 platform
PLATFORM GUIDE FOR OMAP2530 EVM
[PlatformGuide_OMAP2530.pdf
This document provides
platform and device-specific information for the OMAP2530 platform.
PLATFORM GUIDE FOR DM64466 AND DM6467
MEDIA PROCESSOR
[PlatformGuide_DM6446_DM6467.pdf]
This document provides
platform-specific information for DM6446 and DM6467 Media Processor.
PLATFORM
GUIDE FOR DM357 MEDIA PROCESSOR
[PlatformGuide_DM357.pdf]
This document provides
platform-specific information for DM357 .
[PlatformGuide_PCI.pdf]
This document provides
platform-specific information for the DM6437 Processor.
[PlatformGuide_PCI.pdf]
This document provides
platform-specific information for the DM648 Processor.
PLATFORM
GUIDE FOR DA8XX MEDIA PROCESSOR
[PlatformGuide_DA8xx.pdf]
This document provides platform-specific
information for DA8XX.
PLATFORM
GUIDE FOR OMAPL1XX MEDIA PROCESSOR
[PlatformGuide_OMAPL1xx.pdf]
This document provides platform-specific
information for OMAPL1xx platform
PLATFORM GUIDE FOR OMAPL138 EVM
[PlatformGuide_OMAPL138.pdf]
This document provides
platform and device-specific information for the OMAPL138 platform
[PlatformGuide_DA850.pdf]
This document provides
platform and device-specific information for the DA850 platform
DESIGN DOCUMENTS
[LNK_010_DES.pdf]
This document describes the detailed
design of the Processor Manager component.
[LNK_012_DES.pdf]
This document describes the detailed
design of the Link Driver component.
[LNK_031_DES.pdf]
This document describes the detailed
design of the messaging component based on MSGQ module of DSP/BIOSTM.
[LNK_129_DES.pdf]
This document describes the design of the
RingIO component that provides a ring-buffer as a data transport across GPP and
DSP.TM.
[LNK_040_DES.pdf]
This document describes the overall design and architecture of the
Loader used to parse and load DSP binaries. It lists the interfaces exposed by
the loader and also describes the overall design for implementation of these
interfaces.
It would be the starting point for users trying to implement their own parser
and/ or loader.
[LNK_082_DES.pdf]
This document describes the overall design
of POOL APIs and interfaces. This component provides an interface to the buffer
pools for memory allocation and free operations.
[LNK_128_DES.pdf]
This document describes the overall design of IPS and Notify components.
Notify component allows applications to register for notification of events
occurring on the remote processor and send event notification to the remote
processor.
[LNK_131_DES.pdf]
This document describes the overall design of the MPLIST component.
MPLIST component provides a doubly-linked circular linked list based transport
mechanism between GPP and DSP. DSP.
[LNK_133_DES.pdf]
This document describes the overall design of the MPCS component.
This component allows applications to achieve mutually exclusive access to
shared data structures through a multi-processor critical section (MPCS) between
GPP and DSP.
[LNK_137_DES.pdf]
This document describes the overall design of dynamic configuration of
DSP/BIOSTM
LINK
This feature allows applications to modify the DSP/BIOS LINK configuration
without having to rebuild the DSP/BIOS LINK GPP-side kernel module and DSP-side
libraries.
[LNK_157_DES.pdf]
This document describes the design of enhanced multi-process support for
DSP/BIOSTMLINK.
This feature allows multiple applications/processes to use DSP/BIOSTMLINK independently, and without
being aware of each other.
[LNK_181_DES.pdf]
This document describes the design of dynamic entry creation in TLB.
[LNK_182_DES.pdf]
This document describes the design of multi-DSP support in for DSP/BIOSTMLINK.
This feature allows applications on host to communicate with multiple DSPs.
OS
SPECIFIC DOCUMENTS
[LNK_024_DES.pdf]
This document describes the overall design
and architecture of the OS Adaptation Layer for Linux.
HARDWARE SPECIFIC DOCUMENTS
[LNK_041_DES.pdf]
This document describes the overall design
of the shared memory based zero copy driver message and data transfer.
API
REFERENCE GUIDE
[index.html]
Provides doxygen generated API reference
guide for the developers.