8.8.1.1.1.2.18. DebugSession

interface DebugSession()

Encapsulates the debugger operations for the a given target. This interface is returned by initScripting.

If the debugger is de-configured, any current Session objects will automatically be invalidated and will refuse any further operations.

armAdvancedFeatures: ArmAdvancedFeatures
breakpoints: Breakpoints
callstack: Callstack
clock: Clock
cio: Cio
expressions: Expressions
flash: Flash
globalBreakpoint: GlobalBreakpoint
memory: Memory
registers: Registers
settings: Settings
symbols: Symbols
target: Target
getName()

Returns the name of this target. This is the same name for the target that is returned by listCores.

const name = session.getName();
console.log(`This is the session for ${name}`);
Returns:

the name of this target

Return type:

string

getPartNum()

Returns the part number of this target's device.

// get the part number
let partNum = session.getPartNum();
Returns:

the part number

Return type:

string

registerCallback(name: str, callback): void()

Register a callback with the debugger. The function will be callable from the debugger's GEL (General Extension Language) interpreter.

function read_reg(ds, session, reg) {
    return session.registers.read(reg);
}

session1.registerCallback("foo", read_reg);
session2.registerCallback("foo", read_reg);

session1.expressions.evaluate('foo("PC")'); // returns PC for CPU 1
session2.expressions.evaluate('foo("PC")'); // returns PC for CPU 2

The debugger will invoke certain GEL functions, if they exist, in response to changes in the state of the target. For example, OnHalt() will be called whenever target execution halts. A full list of the callbacks that can be triggered by the debugger can be found in the list of GEL functions in the CCS User's Guide.

If a GEL function of the same name already exists, an exception will be thrown. Many devices have GEL scripts preloaded by the debugger that define some of these special GEL functions to perform certain device-specific operations. We recommend exercising caution should you attempt to modify those files. This feature is intended for advanced users.

function on_halt(ds, session) {
    const pc = session.registers.read("PC");
    console.log(`execution halted at 0x${pc.toString(16)}");
}

session.registerCallback("OnHalt", on_halt);

session.target.stepOver();
// The output should show "execution halted at <pc value>"
Parameters:
  • name (string) -- The name of the callback function to create.

  • callback ((ds: DebuggerScripting, session: DebugSession, ...args: (boolean | bigint | string)[]) => boolean | float | bigint | string) -- The function to invoke. This function will be passed the DebuggerScripting object, the DebugSession object, followed by any arguments provided by the caller. The function may return a boolean, numerical, or string value.

Return type:

void

registerMenuCallback(name: str, menu: str, callback): void()

Like registerCallback but the callback will also appear in the CCS scripts menu (accessible from the menu bar).

Parameters:
  • name (string) -- The name of the callback function to create.

  • menu (string) -- A '/'-separated path to the menu containing the callback. For example: "OuterMenu/InnerMenu".

  • callback ((ds: DebuggerScripting, session: DebugSession, ...args: (boolean | bigint | string)[]) => boolean | float | bigint | string) -- The function to invoke. This function will be passed the DebuggerScripting object, the DebugSession object, followed by any arguments provided by the caller. The function may return a boolean, numerical, or string value.

Return type:

void

unregisterCallback(name: str): void()

Unregister a callback that was registered by this DebugSession object.

function foo1(ds, session, x) {
    return x + 1;
}

function foo2(ds, session, x) {
    return x + 2;
}

session.registerCallback("foo", foo1);
session.expressions.evaluate("foo(3)"); // returns 4
session.registerCallback("foo", foo2); // error: foo already exists
session.unregisterCallback("foo");
session.registerCallback("foo", foo2);
session.expressions.evaluate("foo(3)"); // returns 5
close(): void()

Closes the connection between this DebugSession object and the debugger. No further communication between this object and the debugger will be possible. Note that this is not the same thing as disconnect. A new DebugSession for the same core can still be created by openSession to continue interactions with the target.

session = ds.openSession();
session.target.connect();
session.registers.read("PC"); // reads the PC
session.close();

session.registers.read("PC"); // error: Module Closed

session = ds.openSession();
session.target.isConnected(); // true (still connected)
session.registers.read("PC"); // reads the PC
Return type:

void