8.8.1. Scripting¶
CCS Scripting (a.k.a. "Scripting") is a synchronous scripting interface available from the debugger. This allows for users to automate debugger actions from a script. While JavaScript is the default (and recommended) scripting language supported by CCS Scripting, it is also possible to use Python. For more information on using CCS Scripting with Python, please refer to the Python section below.
Note
CCS Scripting is a new scripting solution independent of DSS. DSS (also referred to as Legacy Scripting) is still available with CCStudio™ IDE. Most of the syntax for the CCS Scripting APIs remains unchanged from DSS. See Scripting API for the full API.
Warning
Note that the CCS Scripting interface from CCS Theia versions 1.2 and earlier was asynchronous in behavior and required the use of the await operator to wait for the completion of operations. This is no longer the case with CCS Theia 1.3, which is synchronous in behavior. Hence the await operator is no longer needed.
8.8.1.1. Scripting API¶
The full API documentation can also be found in <CCS INSTALL DIR>/ccs/scripting/docs.
8.8.1.2. Getting Started¶
To launch the debugger, initScripting must be called. This returns the main scripting interface.
// usual usage
const ds = initScripting();
// providing an optional object with additional configuration options
const ds = initScripting({ inProcess: true });
Note
To support 64-bit addressable targets and 64-bit values in general, the scripting environment will accept and return BigInts. This is a JavaScript type that can represent arbitrary-sized integers. Regular JavaScript numbers and strings will also be accepted, but using BigInts is recommended.
8.8.1.2.1. Configuring and Launching a Debug Session¶
To debug a given target, the debugger must be configured using configure. The Target Configuration File needs to be specified to the scripting environment before attempting to start a debug session. This is done by passing in a target configuration (.ccxml) file to the configure API.
let { cores, nonDebugCores } = ds.configure("my_configuration.ccxml");
To open a debug session with the target, openSession must be called with the core name. You can open multiple debug sessions for multi-core debugging.
// Specifying an exact name
let session = ds.openSession("Texas Instruments XDS110 USB Debug Probe_0/Cortex_M4_0")
// The first core with CortexM or CortexR anywhere in the name
let session = ds.openSession("Cortex(M|R)")
// equivalently
let session = ds.openSession(/Cortex(M|R)/)
// The first core
let session = ds.openSession()
Tip
A list of the currently configured cores can be found by:
let { cores, nonDebugCores } = ds.listCores();
8.8.1.2.2. Connecting and Disconnecting a Target¶
A target can be connected or disconnected using target.connect and target.disconnect.
// connect and disconnect from the target
session.target.connect()
session.target.disconnect()
8.8.1.2.3. Loading and Running a Program¶
First, a program file must be loaded to the target.
session.memory.loadProgram("C:/my_project/Debug/example.out");
The loaded program can then be run.
session.target.run()
8.8.1.2.4. Shutting Down the Debug Session¶
To deconfigure the debugger and close the connection to the debugger, call shutdown. This should be called at the end of a script.
ds.shutdown();
8.8.1.2.5. Breakpoints¶
Breakpoints can be added or removed using session.breakpoints.add() and session.breakpoints.remove().
// Adds a breakpoint at 0x2400
let id = session.breakpoints.add(0x2400n);
// Adds a breakpoint at symbol 'main'
let id = session.breakpoints.add("main");
// Adds a breakpoint at an offset from symbol 'main'
let id = session.breakpoints.add("main + 0x8");
// Adds a breakpoint at line 24 of main.c
let id = session.breakpoints.add("C:/my_project/source/main.c", 24);
// Removes the breakpoint at line 24 of main.c
session.breakpoints.remove(id);
8.8.1.2.5.1. Advanced Breakpoints¶
In addition to the basic breakpoints, advanced breakpoints can be set with properties that allow for more control over the breakpoint behavior. These properties can be used to set intrusive or non-intrusive breakpoints, execute GEL commands, control profiling, etc.
Advanced breakpoints can be set by creating a breakpoint property object. Breakpoint properties are set via the setProperty() API. To get the property name and allowed values, refer to Breakpoint Properties.
Property names are directly derived from the properties displayed along with their hierarchy.
"Hardware Configuration.Location"
"Debugger Response.Action.Expression"
"Debugger Response.Skip Count"
Note
The available names and hierarchy can vary depending on the type of breakpoint and the target being used.
Example script to set a software breakpoint with a skip count of 5:
const propsId = session.breakpoints.createProperties(0); // Set a SW breakpoint
session.breakpoints.setProperty(propsId, "Hardware Configuration.Location", 0x8000); // Breakpoint at address 0x8000
session.breakpoints.setProperty(propsId, "Debugger Response.Skip Count", 5); // Skip count of 5
id = session.breakpoints.addWithProperties(propsId); // Add breakpoint
An example script demonstrating the usage of breakpoint properties to configure advanced breakpoints is provided in examples/debugger/breakpoint-properties.js.
8.8.1.3. Example Script¶
Below is a full example script. It is strongly encouraged for new users to slowly walk through this example to get an understanding of how CCS Scripting works. The example is well commented and should give you an understanding of the basic steps needed to create the scripting environment and start a debug session for a specified target, in addition to highlighting some of the APIs available. It is also useful to use this script as a baseline for creating your own scripts (by referencing it or simply copying and then "gutting" it to use as a template).
This example script also ships with CCStudio IDE and can be found in <CCS INSTALL DIR>/ccs/scripting/examples/debugger/breakpoints.js.
// Since we don't know where CCS will be installed, we must find files relative
// to this script. To this end, we will need access to node.js's path.join function.
const { join } = require("path");
// Initialize scripting and obtain the main debugger scripting interface
const ds = initScripting();
// Configure a 10 second timeout on all operations (by default there is no timeout)
ds.setScriptingTimeout(10000);
// Configure the debugger and open a debug session to the cortex M core
ds.configure(join(__dirname, "mspm0g3507/mspm0g3507.ccxml"));
const session = ds.openSession(/cortex/i);
session.target.connect();
// Load program
// The path provided must be an absolute path. Here we use the current script's location
// to resolve the location.
session.memory.loadProgram(join(__dirname, "mspm0g3507/modem.out"));
// Set a breakpoint at ReadNextData
const bp1 = session.breakpoints.add("ReadNextData");
// Set a second breakpoint using the address of the function ShapingFilter
const bp2Addr = session.expressions.evaluate("ShapingFilter");
const bp2 = session.breakpoints.add(bp2Addr);
// Let's define a function to run the target and check if it halts at the correct symbol
function expectRunToHaltAt(symbol) {
// Run the target and wait for it to halt
session.target.run();
const symbolAddr = session.expressions.evaluate(symbol);
const pc = session.registers.read("PC");
if (pc === symbolAddr) {
console.log(`Success: target is halted at ${symbol} as expected.`);
} else {
console.error(
`Failure: Expected target to be halted at 0x${symbolAddr.toString(16)}, `
`but is actually halted at 0x${pc.toString(16)}.`
);
process.exit(1);
}
}
// If we run, we should hit our first breakpoint at ReadNextData
expectRunToHaltAt("ReadNextData");
// If we run a second time, we expect to halt at our second breakpoint
expectRunToHaltAt("ShapingFilter");
// Remove our first breakpoint
session.breakpoints.remove(bp1);
// The program runs in an infinite loop, so running a third time should, once again, halt at the second breakpoint
expectRunToHaltAt("ShapingFilter");
// If we remove our second breakpoint as well, we expect to run in a loop until we time out
session.breakpoints.remove(bp2);
// We expect the next run to timeout, let's reduce the timeout duration so we don't have to wait as long
ds.setScriptingTimeout(2000);
try {
console.log("Expecting target to not halt for 2 seconds");
session.target.run();
console.error("Failure: Halted unexpectedly after removing both breakpoints.");
} catch (err) {
// Check if we actually timed out, or if some other error occurred
if (err instanceof ScriptingTimeoutError) {
console.log("Success: we timed out while waiting for the target to halt");
session.target.halt();
} else {
console.error(`Failure: unexpected error while running ${err}`);
}
}
// shutdown the debugger
ds.shutdown();
Tip
You can send messages from your script to the console by using console.log(). For more information, visit https://developer.mozilla.org/en-US/docs/Web/API/console.
8.8.1.4. Running a Script¶
Navigate to <CCS INSTALL DIR>/ccs/scripting and use the run.bat and run.sh scripts with your script path as an argument:
run.bat examples/debugger/breakpoints.js
8.8.1.5. Debugging a Script¶
Please also refer to the Debugging Your Script section in the full Scripting API documentation.
An example launch configuration for a Node debug session would look like:
{
"name": "Debug Script",
"type": "node",
"runtimeExecutable": "C:/ti/ccs2040/ccs/tools/node/node",
"request": "launch",
"program": "C:/Users/user/workspace_ccstheia/led_ex1_blinky_cpu1/example_scripting_f28379d.js",
"skipFiles": [
"<node_internals>/**"
]
}
Note that CCStudio IDE comes with Node and the above launch configuration example leverages this.
Note that since the script is not being run from inside the standard CCS Scripting environment (using either the provided shell script or the Scripting Console View), an extra step is needed in the script to configure the scripting environment and obtain the main scripting interface as shown below:
const ccsPath = "C:/ti/ccs2040"; // Change this to your CCS installation path
// load CCS Scripting modules, needed when debugging script in VS Code / Theia
const { initScripting } = require(ccsPath + '/ccs/scripting/node_modules/scripting');
// Initialize scripting and obtain the main debugger scripting interface
const ds = initScripting();
The script can then be launched like any launch configuration. It is important to set a breakpoint in the script before launching; otherwise, it will just run the script to the end. Below is an example of debugging a script using CCStudio IDE as a JavaScript debugger using the JavaScript Debugger extension:
Note that the above example uses CCStudio IDE for debugging the script. This is not required, and any IDE that supports JavaScript debugging (such as VS Code) can be used instead.
8.8.1.5.1. IDE Visibility¶
Sometimes it is not enough to simply debug the script to identify automation errors. Target state visibility may also be needed to properly diagnose the cause of issues. In such cases, it is possible to attach the CCStudio IDE to a running debug instance created by the script using the launchCCS() API:
launchCCS(mode: "detached" | "waitUntilLaunch" | "waitUntilExit"): void;
The launchCCS() API takes an optional argument that controls the behavior of the launched IDE. The possible values are:
detached: Wait until the CCStudio IDE instance is launched, then continue. This is the default behavior if an argument is not provided.
waitUntilLaunch: Wait until the CCStudio IDE instance is launched, then continue. Additionally, Code Composer Studio will be closed when the script calls
shutdown().waitUntilExit: Wait until the CCStudio IDE instance exits, then continue.
This call can be added anywhere after the main debugger scripting instance is created:
// Initialize scripting and obtain the main debugger scripting interface
const ds = initScripting();
// Launch an instance of CCS side-by-side with this instance of the debugger.
ds.launchCCS("waitUntilLaunch");
Below is an example of such a setup using VS Code to debug the script while CCStudio IDE is launched side-by-side for target debug visibility:
Tip
It is recommended to use some other IDE (such as VS Code) to debug the script while using CCStudio IDE for target debug visibility.
8.8.1.6. Using GEL with Scripting¶
You can call GEL expressions from Scripting by using expressions.evaluate().
// Adds 8 to the address of the main symbol, returns a BigInt
let result = session.expressions.evaluate("main + 8");
// Returns a (floating point) number
let result = session.expressions.evaluate("1.0 / 2");
// Call a GEL function (assuming that this function is either defined in a loaded GEL script or a built-in GEL function)
session.expressions.evaluate("userDefinedGelFunction()");
8.8.1.7. Debugger Properties¶
There are Scripting APIs to get and set various debugger/flash options:
Some options that are supported are:
auto-run to main on program load/restart/reset
enable real-time mode
...
Use the following API to print the full list of supported options in CCS Scripting:
getDetailedSettings(): DebugSetting[]
This will return a list of objects which detail each debugger setting which can be printed to the console using console.log().
A single object will look like:
{
id: 'AutoRunToLabelOnRestart',
name: 'On a program load or restart',
type: 'bool',
value: true
}
id: The id for the option.
name: The name of the option. This should match the name of the option in the Debug Properties.
type: The option type. It is either a number, string, or boolean.
value: The default/current value of the option.
The API to get the value of a specific option is:
get(settingId): string | number | boolean
Pass in the option id for the settingId as described above.
The API to set the value of specific options is:
set(settingId, value): void
Example of setting a debugger property to disable auto-run on program load or restart:
// disable auto-run to main
session.settings.set("AutoRunToLabelOnRestart", false);
8.8.1.8. Recommended Extensions¶
To set up CCStudio IDE to edit scripts with support for suggestions and documentation, you can install the following extensions:
For Debugging a Script with CCStudio IDE, you can install the following extension:
8.8.1.9. Console¶
8.8.1.9.1. Scripting Console¶
The Scripting Console View allows users to interactively call Scripting API from within the CCStudio IDE. Please refer to the Scripting Console View section for more details.
8.8.1.9.2. System Console¶
The example script interactive.mjs can be used to interactively call the scripting APIs from the system console. This script is located at <CCS INSTALL DIR>/ccs/scripting/examples/debugger/interactive.mjs.
When the script is run, it will prompt the user for input. The system console can now be used like the above Scripting Console to interactively call Scripting API from the system console. Unlike the Scripting Console, there is no IDE dependency.
8.8.1.10. Python¶
CCS Scripting can also be used with Python. This allows users to write scripts in Python to automate debugger actions. The Python scripting interface is similar to the JavaScript interface, but there are some differences in syntax and usage.
To run a Python script, navigate to <CCS INSTALL DIR>/ccs/scripting/python and use the run.bat and run.sh scripts with your script path as an argument:
run.bat examples/debugger/breakpoints.py
Note
CCS includes Python version 3.14 to run scripts.
A few example Python scripts are provided in the <CCS INSTALL DIR>/ccs/scripting/python/examples/debugger directory. Among them, the breakpoints.py example script is a Python version of the JavaScript Example Script provided above. There are a few key items of note in the Python example script:
8.8.1.10.1. Importing the Scripting Package¶
While the JavaScript/TypeScript implementation implicitly imports the scripting module in most cases, in Python the module must be explicitly imported.
from scripting import initScripting, ScriptingTimeoutError
8.8.1.10.2. Logging¶
Logging can be configured using the Python logging module:
import logging
logger = logging.getLogger("TI.scripting")
The log level can be set as desired:
logger.setLevel(logging.INFO)
logger.setLevel(logging.DEBUG)
An example script named logging.py demonstrating a more detailed logging configuration is also provided.
8.8.1.10.3. Return Types¶
Where the JavaScript/TypeScript implementation returns objects, the Python implementation returns dictionaries. In addition, automatic unpacking is not yet supported. For instance, in the JavaScript/TypeScript version, you might have:
core_lists = ds.listCores()
cores = core_lists.cores
nonDebugCores = core_lists.nonDebugCores
or even:
{cores, nonDebugCores} = ds.listCores()
In Python, you would have to do the following:
core_lists = ds.listCores()
cores = core_lists["cores"]
nonDebugCores = core_lists["nonDebugCores"]
Additionally, where the JavaScript/TypeScript implementation accepts or returns bigints, the Python equivalent uses the standard int.
8.8.1.10.4. Providing Arguments to initScripting¶
Options can be provided to initScripting in a single dictionary. This is very similar to what is supported in JavaScript/TypeScript implementation:
ds = initScripting({"ccsRoot":"/home/user/ti/ccs2030/ccs", "logFile":"/home/user/log.txt"})
Passing options as keyword arguments is also supported:
from scripting import initScripting, ScriptingTimeoutError
ds = initScripting(ccsRoot="/home/user/ti/ccs2030/ccs", logFile="/home/user/log.txt")
8.8.1.10.5. Using your own Python Interpreter¶
You can use your own Python interpreter provided it is version 3.10 or later, and you install the required packages. We recommend installing the package(s) as follows:
python -m pip install -e <CCS INSTALL DIR>/ccs/scripting/python/site-packages/scripting
Note
If you omit the -e flag, you will need to use the ccsRoot parameter when calling initScripting() and you will need to repeat the pip install command when you update CCS.
Once this is complete, CCS Scripting Python scripts can be run like any other python files. For example, to run a script named example.py, you would execute:
python example.py
Note
We recommend using a Python virtual environment, especially if you are using your distribution's included Python installation on Ubuntu.