8.8.1.1.1.2.7. Expressions¶
- interface Expressions()¶
- evaluate(expression: string)¶
Evaluates a GEL expression and returns the resulting value, if numerical or a string. All standard rules for GEL expressions apply. If the result of evaluating the expression is an integral value, a BigInt will be returned if using JavaScript. If the value is a floating point value, a standard floating point number will be returned. For any other value, like a reference to a c++ object, we return without a value.
// Adds 8 to the address of the main symbol, returns a BigInt let result = session.expressions.evaluate("main + 8"); // Returns a (floating point) number let result = session.expressions.evaluate("1.0 / 2"); // Call a GEL function (assuming that this function is defined in a loaded GEL script) session.expressions.evaluate('userDefinedGelFunction()');
- Parameters:
expression (
string) -- The GEL expression to evaluate.
- Returns:
The value resulting from the evaluation of the expression, if numerical or a string.
- Return type:
void | bigint | number | string