8.8.1.1.1.2.8. Flash¶
- interface Flash()¶
- isFlashSupported()¶
Determines if flash is supported for the current device.
if (session.flash.isFlashSupported()) { // perform flash operations... }
- Returns:
true if flash is supported on the current device, false otherwise.
- Return type:
boolean
- performOperation(operation: string)¶
Performs the specified flash operation. A list of all available operations for the current device can be obtained by calling
listSupportedOperations.// Erases the flash (assuming the operation is supported and named "Erase") session.flash.performOperation("Erase");
- Parameters:
operation (
string) -- The operation to be performed.
- Return type:
void
- listSupportedOperations()¶
Queries the list of flash operations supported for the current device.
// Print the list of supported operations console.log(session.flash.listSupportedOperations());
- Return type:
string
- multiLoadStart()¶
Should be called to start a multi-load operation. The flash manager will only erase the flash on the first program load. Once the Flash Manger receives this call, users will be free to call
loadProgramandloadBinaryProgramas many times as needed to write to the Flash.session.flash.multiLoadStart(); // multiple program loads... session.flash.multiLoadEnd();
- Return type:
void
- multiLoadEnd()¶
Called to finish a multi-load operation. The flash manager will return to default mode (erasing flash based on user settings).
session.flash.multiLoadStart(); // multiple program loads... session.flash.multiLoadEnd();
- Return type:
void