8.8.1.1.1.2.1. ArmAdvancedFeatures¶
- interface ArmAdvancedFeatures()¶
- listSupportedActions()¶
Returns a list of all supported actions. If no actions are supported, the list is empty.
// Print the supported actions const supportedActions = session.armAdvancedFeatures.listSupportedActions(); console.log("Supported actions:"); for (const action of supportedActions) { console.log(` ${action.action} - ${action.description}`); }
- Returns:
The list of supported actions.
- Return type:
ArmAdvancedFeaturesAction[]
- performAction(action: string)¶
Performs the specified action.
session.armAdvancedFeatures.performAction("FlushAllCaches");
- Parameters:
action (
string) -- The unique identifier of the action to perform. UselistSupportedActionsto get a list of supported actions.
- Return type:
void
- refresh()¶
The Arm Advanced Features settings displayed in the some GUIs can become out-of-sync with the state of the target's registers. This function forces all settings to update themselves to reflect the target's current state.
A script should not need to call this prior to calling querying the setting's value with something like
get.session.settings.set("MPUEnabled", false); // Suppose we are on Cortex R5 // Enable MPU by writing to the register directly SCTLR = "CP15_SYSTEM_CONTROL"; session.registers.write(SCTLR, session.registers.read(SCTLR) | 1); // Settings in tools like the CCS IDE may not reflect the updated // register value yet. session.armAdvancedFeatures.refresh(); // Settings should now reflect the updated values
- Return type:
void