MAVRK Embedded Software 0.91
Software Libraries for the MAVRK motherboard and related components

File List

Here is a list of all files with brief descriptions:
ADS123x.h [code]
ADS123x_PC_Interface.h [code]
ADS123x_PC_Interface_Command_Decode.cSetup the interface from the MAVRK board to the PC Application for ADS123x devices
ADS123x_PC_Interface_Functions.cPerforms PC Interface functions between an ADS1x3x and the PC Interface
ADS123x_SPI_Functions.cPerforms SPI Communication for ADS1x3x Devices
ADS1248_constants.c
ADS1259.h [code]
ADS1259_Device_Interface.h [code]
ADS1259_Device_Status.c
ADS1259_Functions.c
ADS1259_PC_Interface.h [code]
ADS1259_PC_Interface_Command_Decode.cSetup the interface from the MAVRK board to the PC Application for ADS1x48 devices
ADS1259_PC_Interface_Functions.cPerforms PC Interface functions between an ADS1x48 and the PC Interface
ADS1259_SPI_Functions.c
ADS1x3x_Device_Interface.h [code]
ADS1x48_PC_Interface.h [code]
ADS1x48_PC_Interface_Command_Decode.cSetup the interface from the MAVRK board to the PC Application for ADS1x48 devices
ADS1x48_PC_Interface_Functions.cPerforms PC Interface functions between an ADS1x48 and the PC Interface
ADS1x4x.h [code]
ADS1x4x_Device_Interface.h [code]
ADS1x4x_Device_Status.cFunctions that gather the status for ADS1x48 devices
ADS1x4x_Functions.cFunctions that setup the ADS1x4x device for operations
ADS1x4x_SPI_Functions.cPerforms SPI Communication for ADS1x4x Devices
ADS1x9x.h [code]
ADS1x9x_Constant_Tables.cPredefined constant tables for ASD1298 DAC
ADS1x9x_Device_Interface.h [code]
ADS1x9x_Device_Status.cFunctions that gather the status for ADS1x9x devices
ADS1x9x_Functions.cFunctions that setup the ADS1x9x device for operations
ADS1x9x_PC_Interface.h [code]
ADS1x9x_PC_Interface_Command_Decode.cSetup the interface from the MAVRK board to the PC Application for ADS1x9x devices
ADS1x9x_PC_Interface_Functions.cPerforms PC Interface functions between an ADS1x9x and the PC Interface
ADS1x9x_SPI_Functions.cPerforms SPI Communication for ADS1x9x Devices
ADS78xx_ADS83xx.h [code]
ADS78xx_ADS83xx_PC_Interface.h [code]
ADS78xx_ADS83xx_PC_Interface_Functions.cPerforms PC Interface functions between an ADS83xx and the PC Interface
ADS7924.h [code]
ADS7924_Functions.cFunctions that setup the ADS7924 device for operations
ADS7924_I2C_Functions.cPerforms I2C Communication for ADS7924 Devices
ADS7924_PC_Interface.h [code]
ADS7924_PC_Interface_Command_Decode.cSetup the interface from the MAVRK board to the PC Application for ADS7924 devices
ADS7924_PC_Interface_Functions.cPerforms PC Interface functions between an ADS7924 and the PC Interface
Board_to_Board_Passthrough.h [code]
Board_to_Board_Passthrough_Functions.cFunctions that setup and control the I/O and flags for Board to Board communication on the MAVRK system
BootLoader_Interface.h [code]
BootLoader_Interface_Functions.cPerforms generic Interface functions between the standard MAVRK device and the Boot Loader Software
BQ24765_MultiCell_Battery_Charger.cPerforms
BQ24765_MultiCell_Battery_Charger.h [code]
BQ24765_PC_Interface.h [code]
BQ24765_PC_Interface_Command_Decode.cSetup the interface from the MAVRK component to the PC Application for BQ24765 Multi-Cell Battery Charger
BQ24765_PC_Interface_Functions.cPerforms PC Interface functions between the PMU-BAT-MVK or PMU-CARRIER-MVK modules and the PC Interface
BQ25504_PC_Interface.h [code]
BQ25504_PC_Interface_Functions.cPerforms PC Interface functions for the BQ25504 module
BQ27410_Fuel_Gauge.cPerforms read and write I2C commands to BQ27410 Fuel Gauge device
BQ27410_Fuel_Gauge.h [code]
BQ27410_Fuel_Gauge_Data_Flash.cPerforms read and write I2C commands to BQ27410 Data Flash
BQ27410_PC_Interface.h [code]
BQ27410_PC_Interface_Command_Decode.cSetup the interface from the MAVRK component to the PC Application for BQ27410 Battery Fuel Gauge
BQ27410_PC_Interface_Functions.cPerforms PC Interface functions between the BQ27410 modules and the PC Interface
CC1100_constants.c
CC1100_unmodulated_carrier.cStructure of register settings to set up system registers of the cc1100
CC1101_constants.c
CC1120_constants.c
cc2500_constants.c
CC2500_unmodulated_carrier.c
cc2550_constants.c
CC430F5137_constants.c
CC_Channel_Functions.c
CC_Device_Processor_Interface.h [code]
CC_Device_Status.cRead the status of registers on the Chipcon Radio
CC_Device_unmodulated_carrier.cStructure of register settings to set up system registers of the cc2500 and cc1100
CC_FIFO_Functions.cFunctions that interact with the FIFOs on the TI Chipcon Radio
CC_Modem_Functions.cFunctions that interact with CC based modems in the RF Slot
CC_Primary_Settings.cFunctions that discover and initialize the TI Chipcon Radio
cc_radio.h [code]
CC_Radio_API.cHigh Level Functions related to transmitting and receiving using the TI Chipcon Radios
CC_Radio_Functions.cFunctions related to controlling radio TX/RX functions of the TI Chipcon Radios
CC_Radio_PC_Interface.h [code]
CC_Radio_PC_Interface_Command_Decode.cSetup the interface between the Chipcon Radio part and the PC Application
CC_Radio_PC_Interface_Functions.cPerforms PC Interface functions between an Chipcon Radio and the PC Interface
CC_SPI_Functions.cFunctions that Control the SPI Interface on the Chipcon Radio
CDCE913.h [code]
CDCE913_Constant_Tables.cSome predefined constant tables for CDCE913 Programmable 1-PLL VCXO Clock Synthesizer
CDCE913_Device_Interface.h [code]
CDCE913_Functions.cFunctions that allow changes in the CDCE913 Programmable 1-PLL VCXO Clock Synthesizer configuration
CDCE913_PC_Interface.h [code]
CDCE913_PC_Interface_Command_Decode.cSetup the interface from the MAVRK board to the PC Application for ADS1x48 devices
CDCE913_PC_Interface_Functions.c
crc.h [code]
crc_algs.cFunctions that perform the equivalent CRC16 and CRC32 to the hardware components
DAC7563_DAC8563_DAC8163.h [code]
diskio.h [code]
doxygen_mainpage.h [code]
DRV8814_DRV8825_MCU_Interface.h [code]
DRV8814_DRV8825_Motor_Drive.h [code]
DRV8814_MCU_Interface_Functions.cPerforms MCU Interface style of functions between a DRV8814 Motor Driver and the MCU Slot
DRV8814_Motor_Drive.cFunctions that setup and control the I/O (GPIOs and LEDs) for the DRV8814 with an MSP430F2234
DRV8814_Motor_Drive.h [code]
DRV8814_Motor_Drive_API.c
DRV8814_PC_Interface.h [code]
DRV8814_PC_Interface_Command_Decode.cSetup the interface from the MAVRK board to the PC Application for DRV8814 motor drive
DRV8814_PC_Interface_Functions.cPerforms PC Interface functions between a DRV8814 Motor Driver and the PC Interface
DRV8825_MCU_Interface_Functions.cPerforms MCU Interface style of functions between a DRV8825 Motor Driver and the MCU Slot
DRV8825_Motor_Drive.cFunctions that setup and control the I/O (GPIOs and LEDs) for the DRV8825 with an MSP430F2234
DRV8825_Motor_Drive.h [code]
DRV8825_Motor_Drive_API.c
DRV8825_PC_Interface.h [code]
DRV8825_PC_Interface_Command_Decode.cSetup the interface from the MAVRK board to the PC Application for DRV8814 motor drive
DRV8825_PC_Interface_Functions.cPerforms PC Interface functions between a DRV8825 Motor Driver and the PC Interface
DRV8830_I2C_Functions.cPerforms low level I2C communications with the DRV8830 Low Voltage Motor Driver
DRV8830_Motor_Drive.cFunctions that setup and control the DRV8830
DRV8830_Motor_Drive.h [code]
DRV8830_Motor_Drive_API.cFunctions that setup and allow the use of the DRV8830
DRV8830_PC_Interface.h [code]
DRV8830_PC_Interface_Functions.cPerforms PC Interface functions between a DRV8830 Motor Driver and the PC Interface
DRV8833_Motor_Drive.h [code]
DRV8833_Motor_Drive_API.cFunctions that setup and allow the use of the DRV8833
DRV8833_PC_Interface.h [code]
DRV8833_PC_Interface_Command_Decode.cSetup the interface from the MAVRK board to the PC Application for DRV8833 motor drive
DRV8833_PC_Interface_Functions.cPerforms PC Interface functions between a DRV8833 Motor Driver and the PC Interface
EEPROM24xx128.cFunctions that setup and controls the EEPROM on the MAVRK Pro Motherboard
EEPROM24xx128.h [code]
F22x4_ADC10.h [code]
F22x4_Basic_Clock_Plus.h [code]
F22x4_CPU.h [code]
F22x4_DRV8814_DRV8825_Com_Port_Functions.cFunctions that setup and controls the communication interfaces on the MSP430F22x4 on the MAVRK Pro motherboard
F22x4_DRV8814_DRV8825_Modular_EVM_IO_Functions.cFunctions that setup and control the I/O (GPIOs and LEDs) for the DRV8814-MVK with an MSP430F22x4
F22x4_DRV8833_Motor_Drive.c
F22x4_interrupts.h [code]
F22x4_io.h [code]
F22x4_Modular_EVM_IO.h [code]
F22x4_system.h [code]
F22x4_Timer.h [code]
F22x4_Timer_A.h [code]
F22x4_Timer_B.h [code]
F22x4_usci.h [code]
F22x4_USCI_Defs.h [code]
F22x4_WDT.h [code]
F5137_ADC12.h [code]
F5137_BQ25504_Device_Interface.h [code]
F5137_Com_Port_Functions.c
F5137_Comparator.h [code]
F5137_CPU.h [code]
F5137_CRC16.cFunctions that setup the CRC Operations for the MSP430F5438
F5137_CRC16.h [code]
F5137_DMA.h [code]
F5137_DRV8830_Motor_Drive.cFunctions that setup and control the I/O (GPIOs and LEDs) for the DRV8833 with the CC430F5137
F5137_DRV8833_Motor_Drive.cFunctions that setup and control the I/O (GPIOs and LEDs) for the DRV8833 with the CC430F5137
F5137_Hardware_Multiplier.h [code]
F5137_interrupts.h [code]
F5137_io.h [code]
F5137_Modular_EVM_IO.h [code]
F5137_Modular_EVM_IO_Functions.cFunctions that setup and controls the I/O (GPIOs and LEDs) for the Modular EVM Board
F5137_Modular_EVM_LED_Functions.c
F5137_Power_Management.h [code]
F5137_REF.h [code]
F5137_RF1A.h [code]
F5137_RF1A_Device_Interface.cFunctions that setup and controls the Chipcon Radio CC430F5137 (F5137 MCU + CC1101 Radio)
F5137_RF1A_Device_Interface.h [code]
F5137_RF_Micro_Debug_Device_Interface.cFunctions that manage the part specific Device Interface between the MSP430F5438 and the RF_UDEBUG_MVK board
F5137_RTC.h [code]
F5137_system.h [code]
F5137_TCA8418_Device_Interface.cFunctions that setup the TI TCA8418 Keypad Scan IC Device with the MSP430F5137 processor
F5137_Timer.h [code]
F5137_Timer_A.h [code]
F5137_Unified_Clock_system.h [code]
F5137_US_BQ25504_Interface.cFunctions that setup the microMAVRK sensors
F5137_US_DIG_Temp_Interface.cFunctions that interface the micro MAVRK CC430F5137 processor to the US-DIG-TEMP-MVK board with 7 temperature sensors, along with light and humidity sensors
F5137_US_DIG_Temp_Interface.h [code]
F5137_usci.h [code]
F5137_usci_Defs.h [code]
F5137_WDT.h [code]
F5438_ADC12.h [code]
F5438_ADS123x_Device_Interface.cFunctions that manage the part specific Device Interface between the MSP430F5438 and the family of ADS1x3x parts
F5438_ADS1259_Device_Interface.c
F5438_ADS1x4x_Device_Interface.cFunctions that setup and controls the interfaces for ADS1x4x devices
F5438_ADS1x9x_Device_Interface.cFunctions that manage the part specific Device Interface between the MSP430F5438 and the family of ADS1x9x parts
F5438_AFE_CARRIER_Device_Interface.cFunctions that setup and controls the AFE Carrier interfaces
F5438_AFE_CARRIER_Device_Interface.h [code]
F5438_CC_Device_Interface.cFunctions that setup the Chipcon Radio with the MSP430F5438 processor
F5438_CDCE913_Device_Interface.cFunctions that setup and controls the interfaces for ADS1x4x devices
F5438_CPU.h [code]
F5438_CRC16.cFunctions that setup the CRC Operations for the MSP430F5438
F5438_CRC16.h [code]
F5438_DMA.h [code]
F5438_Hardware_Multiplier.h [code]
F5438_interrupts.h [code]
F5438_io.h [code]
F5438_PC_Interface.h [code]
F5438_PC_Interface_Functions.cPerforms PC Interface functions between an TMP Sensors and the PC Interface
F5438_Power_Management.h [code]
F5438_ProMB_Com_Port_Functions.cFunctions that setup and controls the communication interfaces on the MSP430F5438 on the MAVRK Pro motherboard
F5438_ProMB_LED_Functions.cFunctions that setup and control the LED's present on the MSP430 MCU, RF Breakout and AFE Breakout boards when used on the MAVRK Pro Motherboard
F5438_ProMB_Modular_EVM_IO.h [code]
F5438_ProMB_Modular_EVM_IO_Functions.cFunctions that setup and control the I/O (GPIOs and LEDs) for the MAVRK Pro Motherboard & F5438 Modular EVM Board combination
F5438_REF.h [code]
F5438_RF_Micro_Debug_Device_Interface.cFunctions that manage the part specific Device Interface between the MSP430F5438 and the RF_UDEBUG_MVK board
F5438_RTC.h [code]
F5438_system.h [code]
F5438_TCA8418_Device_Interface.cFunctions that setup the TI TCA8418 Keypad Scan IC Device with the MSP430F5438 processor
F5438_TCA8418_Device_Interface.h [code]
F5438_Timer.h [code]
F5438_Timer_A.h [code]
F5438_Timer_B.h [code]
F5438_Unified_Clock_system.h [code]
F5438_usci.h [code]
F5438_usci_Defs.h [code]
F5438_WDT.h [code]
ff.c
ff.h [code]
ffconf.h [code]
Flash_Programming.cFunctions that allow to write and read flash memory
Flash_Programming.h [code]
Generic_Temp_Sensor.h [code]
Generic_Temp_Sensor_Functions.cFunctions related to TMP20 sensor functionality
Generic_Temp_Sensor_PC_Interface_Command_Decode.cDecodes command coming from the PC
Humidity_Sensor.h [code]
Humidity_Sensor_Functions.cFunctionality pertaining to humidity sensor
Humidity_Sensor_PC_Interface_Command_Decode.cUsed to decode the commands coming from the PC QT GUI for the humidity sensor
I2C_Functions.cFunctions that perform standard read and write to slave devices on the I2C bus
I2C_Functions.h [code]
INA220_Current_Power_Monitor.cPerforms
INA220_Current_Power_Monitor.h [code]
INA226_Current_Power_Monitor.cPerforms
INA226_Current_Power_Monitor.h [code]
init_ADS123x.cPerforms initialization for ADS123x Devices
init_ADS1259.cPerforms initialization for ADS1259 Devices
init_ADS1x48.cPerforms initialization for ADS1x4x Devices
init_ADS1x9x.cPerforms initialization for ADS1x9x Devices
init_ADS78xx_ADS83xx.cPerforms initialization for ADS78xx and ADS83xx Devices
init_ADS7924.c
init_CC430F5137.c
init_CC_Device.cFunctions that discover and initialize the TI Chipcon Radio
init_CDCE913.cPerforms initialization for CDCE913 Programmable 1-PLL VCXO Clock Synthesizer
init_DAC7563.c
init_F22x4_ADC10.c
init_F22x4_Basic_Clock_Plus.c
init_F22x4_CPU.cFunctions that setup the MSP430 CPU system
init_F22x4_io.c
init_F22x4_Timer_A.cSet's up the MSP430 Timer A Clock
init_F22x4_Timer_B.cFunctions that setup and control the MSP430 Timer B
init_F22x4_USCI.c
init_F22x4_USCI_0.c
init_F22x4_WDT.cFunctions that setup the MSP430F22x4 Watch Dog Timer (WDT)
init_F5137_ADC12.c
init_F5137_Comparator.cFunctions that setup the MSP430F5137 uC comparator peripheral
init_F5137_CPU.cFunctions that setup the MSP430 CPU system
init_F5137_DMA.cFunctions that setup the MSP430 DMA system
init_F5137_Hardware_Multiplier.cFunctions that setup the MSP430 Multiplier system
init_F5137_io.cFunctions that setup the MSP430 GPIO ports
init_F5137_Power_Management.cFunctions that setup the MSP430F5137 Power System
init_F5137_RF1A.cFunctions that setup the CC430 Radio System
init_F5137_RTC.cFunctions that setup the MSP430 Real Time Clock
init_F5137_Timer_A_0.cFunctions that setup the MSP430 Timer A0 Clock
init_F5137_Timer_A_1.cFunctions that setup the MSP430 Timer A1 Clock
init_F5137_Unified_Clock_system.cFunctions that setup the CC430F5137 Unified Clock System
init_F5137_USCI.cFunctions that setup the CC430F5137 USCI UART/SPI/I2C port
init_F5137_USCI_0.cFunctions that setup the CC430F5137 USCI_0 UART/SPI/I2C port
init_F5137_WDT.cFunctions that setup the CC430F5137 Watch Dog Timer (WDT)
init_F5438.cFunctions that setup the MSP430F5438A uC peripherals
init_F5438_ADC12.cFunctions that setup the MSP430 ADC system
init_F5438_BootLoader.cFunctions that setup the MAVRK BootLoader Software
init_F5438_CPU.cFunctions that setup the MSP430 CPU system
init_F5438_DMA.cFunctions that setup the MSP430 DMA system
init_F5438_Hardware_Multiplier.cFunctions that setup the MSP430 Multiplier system
init_F5438_io.cFunctions that setup the MSP430 GPIO ports
init_F5438_Power_Management.cFunctions that setup the MSP430F5438A Power System
init_F5438_RTC.cFunctions that setup the MSP430 Real Time Clock
init_F5438_Timer_A_0.cFunctions that setup the MSP430 Timer A0 Clock
init_F5438_Timer_A_1.cFunctions that setup the MSP430 Timer A1 Clock
init_F5438_Timer_B_0.cFunctions that setup the MSP430 Timer B0 Clock
init_F5438_Unified_Clock_system.cFunctions that setup the MSP430F5438A Unified Clock System
init_F5438_USCI.cFunctions that setup the MSP430F5438A USCI UART/SPI/I2C port
init_F5438_USCI_0.cFunctions that setup the MSP430F5438A USCI_0 UART/SPI/I2C port
init_F5438_USCI_1.cFunctions that setup the MSP430F5438A USCI_1 UART/SPI/I2C port
init_F5438_USCI_2.cFunctions that setup the MSP430F5438A USCI_2 UART/SPI/I2C port
init_F5438_USCI_3.cFunctions that setup the MSP430F5438A USCI_3 UART/SPI/I2C port
init_F5438_WDT.cFunctions that setup the MSP430F5438A Watch Dog Timer (WDT)
init_INA220.cPerforms initialization of the INA220 Current and Power Monitoring device
init_INA226.cPerforms initialization of the INA226 Current and Power Monitoring device
init_MSP430F22x4.cFunctions that setup the MSP430F22x4 uC peripherals
init_MSP430F5438.cFunctions that setup the MSP430F5137 uC peripherals
init_PGA280.cPerforms initialization for PGA280 Devices
init_TCA8418.c
init_TMP112.cPerforms initialization for TMP112 Temperature Sensor Device
init_TPA2038.cPerforms initialization for TPA2038 Devices
integer.h [code]
Light_Sensor.h [code]
Light_Sensor_Functions.cUsed for light sensor functions that perform various light sensor tasks
Light_Sensor_PC_Interface_Command_Decode.cUsed to decode commands comming from the PC QT interface, specifically for the lights sensor
MAVRK_Arch.h [code]
MAVRK_Common.cFunctions that perform the common functions to collect error and perform timed delay loops
MAVRK_Common.h [code]
MAVRK_Network.h [code]
MAVRK_Network_API.cHigh level functions interfacing to various network types
MAVRK_Return_Error_Codes.h [code]
MAVRK_Test_Utilities.c
MAVRK_Test_Utilities.h [code]
MICRO_MAVRK_Device_Interface.h [code]
MICRO_MAVRK_PC_Interface_Command_Decode.c
MICRO_MAVRK_PC_Interface_Functions.c
mmc.c
mmc.h [code]
Motor_Drive_Command_Interface.h [code]
Motor_Drive_Command_Interface_Functions.cPerforms PC Interface functions between an TMP Sensors and the PC Interface
Packet_Sniffer_API.cHigh Level Functions related to the Packet Sniffer
Packet_Sniffer_Command_Decode.cSetup the interface between the Chipcon Radio part and the PC Application
Packet_Sniffer_PC_Interface.h [code]
Packet_Sniffer_PC_Interface_Functions.cPerforms PC Interface functions between an Chipcon Radio and the PC Interface
Passive_Sensor.h [code]
Passive_Sensor_API.cPerforms PC Interface functions between a Passive Sensor part and the PC Interface
PC_Interface.h [code]
PC_Interface_Functions.cPerforms generic PC Interface functions between a standard MAVRK device and the PC Interface
PC_Interface_Radio_Encapsulation.cContains functions for encapsulating PC interface packets by radio network packets for transmission wirelessly
PGA280.h [code]
PGA280_Functions.cFunctions that setup the PGA280 device for operations
PGA280_PC_Interface_Command_Decode.cSetup the interface from the MAVRK board to the PC Application for PGA280 Programmable Gain Amplifier
PGA280_PC_Interface_Functions.cPerforms PC Interface functions between an PGA280 and the PC Interface
PGA280_SPI_Functions.c
PMU_Seven_Segment.h [code]
PMU_Seven_Segment_LED_Functions.cFunctions that setup and control the Seven Segment LED driver for the PMU BAT Board
RF_1A_constants.c
RF_1A_Device_Status.c
RF_1A_Interface_Functions.c
RF_1A_Radio_Functions.c
RF_Micro_Debug_Device_Interface.h [code]
RS485_Network.h [code]
RS485_RS232_Functions.cFunctions for using the RS485 and RS232 devices on the SCI-RS485-232-MVK module
RSSI_Scanner.h [code]
RSSI_Scanner_Functions.cHigh Level Functions related to the RSSI scanner
SCI_Carrier.h [code]
SCI_Carrier_API.cAPI's for setting up the SCI Carrier
SD_Hardware.h [code]
SD_Hardware_Layer_F5137.cFunction for low level interface to memory
SD_Hardware_Layer_F5438.cFunction for low level interface to memory
SD_Memory.h [code]
SD_Memory_API.cFunctions for high level interface to memory
Serial_Cooperative_Threader.c
Serial_Cooperative_Threader.h [code]
SPI_Functions.cFunctions that perform standard read or writes to devices on the SPI bus
SPI_Functions.h [code]
stdef.h [code]
TCA8418_Key_Scan.cAPI's for the MAVRK RF-TCA8418-MVK Module (TCA8418 I2C CONTROLLED KEYPAD SCAN IC)
TCA8418_Key_Scan.h [code]
TCA8418_Key_Scan_API.cHigh Level Functions related to the TCA8418 Keyboard Scanner
TCA8418_PC_Interface.h [code]
TCA8418_PC_Interface_Command_Decode.cSetup the interface from the MAVRK board to the PC Application for TCA8418 key scanner
TCA8418_PC_Interface_Functions.cPerforms PC Interface functions between an TCA8418 Keypad Scanner and the PC Interface
TCA_PCA_I2C_IO_Expander.cAPI's for the TCA_PCA I2C -> GPIO Expander
TCA_PCA_I2C_IO_Expander.h [code]
TMP103_Temp_Sensor.cPerform interactions with the TMP103 via the I2C bus
TMP103_Temp_Sensor.h [code]
TMP106_Temp_Sensor.cPerform interactions with the TMP106 via the I2C bus
TMP106_Temp_Sensor.h [code]
TMP112_PC_Interface.h [code]
TMP112_PC_Interface_Command_Decode.cSetup the interface from the MAVRK board to the PC Application for TMP112 TMP Sensors
TMP112_PC_Interface_Functions.cPerforms PC Interface functions between an TMP112 Sensors and the PC Interface
TMP112_Temp_Sensor.cPerform interactions with the TMP112 via the I2C bus
TMP112_Temp_Sensor.h [code]
TMP_Sensor_PC_Interface.h [code]
TMP_Sensor_PC_Interface_Functions.cPerforms PC Interface functions between an TMP Sensors and the PC Interface
TPA2038.h [code]
TPA2038_Constant_Tables.c
TPA2038_Functions.cFunctions that setup the TPA2038 device for operations
TPA2038_PC_Interface.h [code]
TPA2038_PC_Interface_Command_Decode.cSetup the interface from the MAVRK board to the PC Application for TPA2038 Audio Amplifier
TPA2038_PC_Interface_Functions.cPerforms PC Interface functions between a TPA2038 Audio Amplifier and the PC Interface
TPL0401.h [code]
TPL0401_Functions.cFunctions that setup the TPL0401 device for operations
UART_PC_Int_Threader.cRegister File to set up UART that is intended to talk back and forth with the PC based GUI software
UART_State_Machine.cRegister File to set up UART State Machine
UART_State_Machine.h [code]
US_DIG_Temp_Interface.cGeneral functions that interface the US-DIG-TEMP-MVK board with 7 temperature sensors along with light and humidity sensors to the project routines
US_DIG_Temp_Interface.h [code]
Wired_Serial_Half_Duplex_Network.cFunctionality for a wired serial half duplex network implemented currently using the RS485 transceiver
Wired_Serial_Network.h [code]
Wireless_Frequency_Hopping.h [code]
Wireless_Frequency_Hopping_Network.cAPI for wireless frequency hopping systems
Wireless_Network.cFunctionality for the original radio network
Wireless_Network.h [code]
Wireless_Network_Common.cCommon functions for the wireless network
Wireless_Network_Common.h [code]
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines