|
MAVRK Embedded Software 0.91
Software Libraries for the MAVRK motherboard and related components
|
00001 /*---------------------------------------------------------------------------/ 00002 / FatFs - FAT file system module configuration file R0.08b (C)ChaN, 2011 00003 /----------------------------------------------------------------------------/ 00004 / 00005 / CAUTION! Do not forget to make clean the project after any changes to 00006 / the configuration options. 00007 / 00008 /----------------------------------------------------------------------------*/ 00009 #ifndef _FFCONF 00010 #define _FFCONF 8237 /* Revision ID */ 00011 00012 00013 /*---------------------------------------------------------------------------/ 00014 / Function and Buffer Configurations 00015 /----------------------------------------------------------------------------*/ 00016 00017 #define _FS_TINY 1 /* 0:Normal or 1:Tiny */ 00018 /* When _FS_TINY is set to 1, FatFs uses the sector buffer in the file system 00019 / object instead of the sector buffer in the individual file object for file 00020 / data transfer. This reduces memory consumption 512 unsigned chars each file object. */ 00021 00022 00023 #define _FS_READONLY 0 /* 0:Read/Write or 1:Read only */ 00024 /* Setting _FS_READONLY to 1 defines read only configuration. This removes 00025 / writing functions, f_write, f_sync, f_unlink, f_mkdir, f_chmod, f_rename, 00026 / f_truncate and useless f_getfree. */ 00027 00028 00029 #define _FS_MINIMIZE 0 /* 0 to 3 */ 00030 /* The _FS_MINIMIZE option defines minimization level to remove some functions. 00031 / 00032 / 0: Full function. 00033 / 1: f_stat, f_getfree, f_unlink, f_mkdir, f_chmod, f_truncate and f_rename 00034 / are removed. 00035 / 2: f_opendir and f_readdir are removed in addition to 1. 00036 / 3: f_lseek is removed in addition to 2. */ 00037 00038 00039 #define _USE_STRFUNC 0 /* 0:Disable or 1/2:Enable */ 00040 /* To enable string functions, set _USE_STRFUNC to 1 or 2. */ 00041 00042 00043 #define _USE_MKFS 0 /* 0:Disable or 1:Enable */ 00044 /* To enable f_mkfs function, set _USE_MKFS to 1 and set _FS_READONLY to 0 */ 00045 00046 00047 #define _USE_FORWARD 0 /* 0:Disable or 1:Enable */ 00048 /* To enable f_forward function, set _USE_FORWARD to 1 and set _FS_TINY to 1. */ 00049 00050 00051 #define _USE_FASTSEEK 0 /* 0:Disable or 1:Enable */ 00052 /* To enable fast seek feature, set _USE_FASTSEEK to 1. */ 00053 00054 00055 00056 /*---------------------------------------------------------------------------/ 00057 / Locale and Namespace Configurations 00058 /----------------------------------------------------------------------------*/ 00059 00060 #define _CODE_PAGE 932 00061 /* The _CODE_PAGE specifies the OEM code page to be used on the target system. 00062 / Incorrect setting of the code page can cause a file open failure. 00063 / 00064 / 932 - Japanese Shift-JIS (DBCS, OEM, Windows) 00065 / 936 - Simplified Chinese GBK (DBCS, OEM, Windows) 00066 / 949 - Korean (DBCS, OEM, Windows) 00067 / 950 - Traditional Chinese Big5 (DBCS, OEM, Windows) 00068 / 1250 - Central Europe (Windows) 00069 / 1251 - Cyrillic (Windows) 00070 / 1252 - Latin 1 (Windows) 00071 / 1253 - Greek (Windows) 00072 / 1254 - Turkish (Windows) 00073 / 1255 - Hebrew (Windows) 00074 / 1256 - Arabic (Windows) 00075 / 1257 - Baltic (Windows) 00076 / 1258 - Vietnam (OEM, Windows) 00077 / 437 - U.S. (OEM) 00078 / 720 - Arabic (OEM) 00079 / 737 - Greek (OEM) 00080 / 775 - Baltic (OEM) 00081 / 850 - Multilingual Latin 1 (OEM) 00082 / 858 - Multilingual Latin 1 + Euro (OEM) 00083 / 852 - Latin 2 (OEM) 00084 / 855 - Cyrillic (OEM) 00085 / 866 - Russian (OEM) 00086 / 857 - Turkish (OEM) 00087 / 862 - Hebrew (OEM) 00088 / 874 - Thai (OEM, Windows) 00089 / 1 - ASCII only (Valid for non LFN cfg.) 00090 */ 00091 00092 00093 #define _USE_LFN 0 /* 0 to 3 */ 00094 #define _MAX_LFN 255 /* Maximum LFN length to handle (12 to 255) */ 00095 /* The _USE_LFN option switches the LFN support. 00096 / 00097 / 0: Disable LFN feature. _MAX_LFN and _LFN_UNICODE have no effect. 00098 / 1: Enable LFN with static working buffer on the BSS. Always NOT reentrant. 00099 / 2: Enable LFN with dynamic working buffer on the STACK. 00100 / 3: Enable LFN with dynamic working buffer on the HEAP. 00101 / 00102 / The LFN working buffer occupies (_MAX_LFN + 1) * 2 unsigned chars. To enable LFN, 00103 / Unicode handling functions ff_convert() and ff_wtoupper() must be added 00104 / to the project. When enable to use heap, memory control functions 00105 / ff_memalloc() and ff_memfree() must be added to the project. */ 00106 00107 00108 #define _LFN_UNICODE 0 /* 0:ANSI/OEM or 1:Unicode */ 00109 /* To switch the character code set on FatFs API to Unicode, 00110 / enable LFN feature and set _LFN_UNICODE to 1. */ 00111 00112 00113 #define _FS_RPATH 0 /* 0 to 2 */ 00114 /* The _FS_RPATH option configures relative path feature. 00115 / 00116 / 0: Disable relative path feature and remove related functions. 00117 / 1: Enable relative path. f_chdrive() and f_chdir() are available. 00118 / 2: f_getcwd() is available in addition to 1. 00119 / 00120 / Note that output of the f_readdir fnction is affected by this option. */ 00121 00122 00123 00124 /*---------------------------------------------------------------------------/ 00125 / Physical Drive Configurations 00126 /----------------------------------------------------------------------------*/ 00127 00128 #define _VOLUMES 1 00129 /* Number of volumes (logical drives) to be used. */ 00130 00131 00132 #define _MAX_SS 512 /* 512, 1024, 2048 or 4096 */ 00133 /* Maximum sector size to be handled. 00134 / Always set 512 for memory card and hard disk but a larger value may be 00135 / required for on-board flash memory, floppy disk and optical disk. 00136 / When _MAX_SS is larger than 512, it configures FatFs to variable sector size 00137 / and GET_SECTOR_SIZE command must be implememted to the disk_ioctl function. */ 00138 00139 00140 #define _MULTI_PARTITION 0 /* 0:Single partition or 1:Multiple partition */ 00141 /* When set to 0, each volume is bound to the same physical drive number and 00142 / it can mount only first primaly partition. When it is set to 1, each volume 00143 / is tied to the partitions listed in VolToPart[]. */ 00144 00145 00146 #define _USE_ERASE 0 /* 0:Disable or 1:Enable */ 00147 /* To enable sector erase feature, set _USE_ERASE to 1. CTRL_ERASE_SECTOR command 00148 / should be added to the disk_ioctl functio. */ 00149 00150 00151 00152 /*---------------------------------------------------------------------------/ 00153 / System Configurations 00154 /----------------------------------------------------------------------------*/ 00155 00156 #define _WORD_ACCESS 0 /* 0 or 1 */ 00157 /* Set 0 first and it is always compatible with all platforms. The _WORD_ACCESS 00158 / option defines which access method is used to the word data on the FAT volume. 00159 / 00160 / 0: unsigned char-by-unsigned char access. 00161 / 1: Word access. Do not choose this unless following condition is met. 00162 / 00163 / When the unsigned char order on the memory is big-endian or address miss-aligned word 00164 / access results incorrect behavior, the _WORD_ACCESS must be set to 0. 00165 / If it is not the case, the value can also be set to 1 to improve the 00166 / performance and code size. */ 00167 00168 00169 /* A header file that defines sync object types on the O/S, such as 00170 / windows.h, ucos_ii.h and semphr.h, must be included prior to ff.h. */ 00171 00172 #define _FS_REENTRANT 0 /* 0:Disable or 1:Enable */ 00173 #define _FS_TIMEOUT 1000 /* Timeout period in unit of time ticks */ 00174 #define _SYNC_t HANDLE /* O/S dependent type of sync object. e.g. HANDLE, OS_EVENT*, ID and etc.. */ 00175 00176 /* The _FS_REENTRANT option switches the reentrancy (thread safe) of the FatFs module. 00177 / 00178 / 0: Disable reentrancy. _SYNC_t and _FS_TIMEOUT have no effect. 00179 / 1: Enable reentrancy. Also user provided synchronization handlers, 00180 / ff_req_grant, ff_rel_grant, ff_del_syncobj and ff_cre_syncobj 00181 / function must be added to the project. */ 00182 00183 00184 #define _FS_SHARE 0 /* 0:Disable or >=1:Enable */ 00185 /* To enable file shareing feature, set _FS_SHARE to 1 or greater. The value 00186 defines how many files can be opened simultaneously. */ 00187 00188 00189 #endif /* _FFCONFIG */
1.7.3