5.9. WDG
5.9.1. Types
Base type |
Type Name |
Brief |
|---|---|---|
enum |
This is a Watchdog status type value. |
|
enum |
Watchdog module Reaction if watchdog counter reaches the maximum value. |
|
enum |
Wdg_PreDivider determines the watchdog clock pre-divider, which is the first of the two dividers between INTOSC1 and the watchdog counter clock (WDCLK) |
|
enum |
Wdg_PreScaler determines the watchdog clock prescaler, which is the second of the two dividers between INTOSC1 and the watchdog counter clock (WDCLK). |
5.9.1.1. enum Wdg_StatusType
Enumerator |
Value |
Description |
|---|---|---|
WDG_UNINIT |
0U |
Watchdog driver is uninitialized. State on power on before invoking Wdg_Init() |
WDG_IDLE |
1U |
Watchdog driver is in idle state. Default state when WDG timer regs are not being programmed. |
WDG_BUSY |
2U |
Watchdog driver is reprogramming the WD to trigger the watchdog. |
Brief: This is a Watchdog status type value.
5.9.1.2. enum Wdg_Reaction
Enumerator |
Value |
Description |
|---|---|---|
WDG_GENERATE_RESET |
0U |
Watchdog can generate a reset signal. |
WDG_GENERATE_INTERRUPT |
1U |
Watchdog can generate an interrupt signal; reset signal is disabled. |
Brief: Watchdog module Reaction if watchdog counter reaches the maximum value.
5.9.1.3. enum Wdg_PreDivider
Enumerator |
Value |
Description |
|---|---|---|
WDG_PREDIV_2 |
0x800 |
PREDIVCLK = INTOSC1 / 2. |
WDG_PREDIV_4 |
0x900 |
PREDIVCLK = INTOSC1 / 4. |
WDG_PREDIV_8 |
0xA00 |
PREDIVCLK = INTOSC1 / 8. |
WDG_PREDIV_16 |
0xB00 |
PREDIVCLK = INTOSC1 / 16. |
WDG_PREDIV_32 |
0xC00 |
PREDIVCLK = INTOSC1 / 32. |
WDG_PREDIV_64 |
0xD00 |
PREDIVCLK = INTOSC1 / 64. |
WDG_PREDIV_128 |
0xE00 |
PREDIVCLK = INTOSC1 / 128. |
WDG_PREDIV_256 |
0xF00 |
PREDIVCLK = INTOSC1 / 256. |
WDG_PREDIV_512 |
0x000 |
PREDIVCLK = INTOSC1 / 512. |
WDG_PREDIV_1024 |
0x100 |
PREDIVCLK = INTOSC1 / 1024. |
WDG_PREDIV_2048 |
0x200 |
PREDIVCLK = INTOSC1 / 2048. |
WDG_PREDIV_4096 |
0x300 |
PREDIVCLK = INTOSC1 / 4096. |
Brief: Wdg_PreDivider determines the watchdog clock pre-divider, which is the first of the two dividers between INTOSC1 and the watchdog counter clock (WDCLK)
5.9.1.4. enum Wdg_PreScaler
Enumerator |
Value |
Description |
|---|---|---|
WDG_PRESCALE_1 |
1U |
WDCLK = PREDIVCLK / 1. |
WDG_PRESCALE_2 |
2U |
WDCLK = PREDIVCLK / 2. |
WDG_PRESCALE_4 |
3U |
WDCLK = PREDIVCLK / 4. |
WDG_PRESCALE_8 |
4U |
WDCLK = PREDIVCLK / 8. |
WDG_PRESCALE_16 |
5U |
WDCLK = PREDIVCLK / 16. |
WDG_PRESCALE_32 |
6U |
WDCLK = PREDIVCLK / 32. |
WDG_PRESCALE_64 |
7U |
WDCLK = PREDIVCLK / 64. |
Brief: Wdg_PreScaler determines the watchdog clock prescaler, which is the second of the two dividers between INTOSC1 and the watchdog counter clock (WDCLK).
5.9.2. Structures
Name |
Brief |
|---|---|
WDG driver object structure. |
|
Mode Information Type. |
|
WDG config root structure. |
5.9.3. Defines
Name |
Brief |
|---|---|
WDG_SW_MAJOR_VERSION |
Driver Implementation Major Version. |
WDG_SW_MINOR_VERSION |
Driver Implementation Minor Version. |
WDG_SW_PATCH_VERSION |
Driver Implementation Patch Version. |
WDG_AR_RELEASE_MAJOR_VERSION |
AUTOSAR Major version specification implemented by WDG Driver. |
WDG_AR_RELEASE_MINOR_VERSION |
AUTOSAR Minor version specification implemented by WDG Driver. |
WDG_AR_RELEASE_REVISION_VERSION |
AUTOSAR Patch version specification implemented by WDG Driver. |
WDG_VENDOR_ID |
Texas Instruments Vendor ID. |
WDG_MODULE_ID |
WDG Driver Module ID. |
WDG_INSTANCE_ID |
WDG Instance ID. |
WDG_SID_INIT |
Service ID for Wdg_Init. |
WDG_SID_SET_MODE |
Service ID for Wdg_SetMode. |
WDG_SID_SET_TRIGGER_CONDITION |
Service ID for Wdg_SetTriggerCondition. |
WDG_SID_GET_VERSION_INFO |
Service ID for Wdg_GetVersionInfo. |
WDG_E_DRIVER_STATE |
Invalid driver state. |
WDG_E_PARAM_MODE |
Invalid mode param. |
WDG_E_PARAM_CONFIG |
Invalid config param. |
WDG_E_PARAM_TIMEOUT |
Invalid timeout value. |
WDG_E_PARAM_POINTER |
Invalid NULL ptr param. |
WDG_E_INIT_FAILED |
Invalid Configuration set selection. |
5.9.4. Functions
Return type |
Function Name |
Brief |
|---|---|---|
void |
Wdg_GetVersionInfo(Std_VersionInfoType * Versioninfo) |
This service returns the version information of WDG module. |
void |
Wdg_Init(const Wdg_ConfigType * CfgPtr) |
This service initializes the WDG driver. |
Std_ReturnType |
Wdg_SetMode(WdgIf_ModeType Mode) |
Switches the watchdog into Mode type off mode, slow mode, fast mode. |
void |
Wdg_SetTriggerCondition(uint16 Timeout) |
Sets the timeout value for the trigger counter. |
5.9.4.1. function Wdg_GetVersionInfo
void Wdg_GetVersionInfo(
Std_VersionInfoType * Versioninfo
)
Brief: This service returns the version information of WDG module.
Parameters:
Versioninfo - Pointer to store the WDG driver version information.
Returns:
None
Return: None
Precondition: This API is available only if WDG_GET_VERSION_INFO_API is STD_ON
Postcondition: None
5.9.4.2. function Wdg_Init
void Wdg_Init(
const Wdg_ConfigType * CfgPtr
)
Brief: This service initializes the WDG driver.
This API is used to configure WDG Mode settings Pre-divider and Pre-scalers etc.
Parameters:
CfgPtr - Pointer to WDG driver configuration set.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.9.4.3. function Wdg_SetMode
Std_ReturnType Wdg_SetMode(
WdgIf_ModeType Mode
)
Brief: Switches the watchdog into Mode type off mode, slow mode, fast mode.
Parameters:
Mode One of the following statically configured modes OFF_MODE, SLOW_MODE, FAST_MODE
Returns:
E_OK command has been accepted.
E_NOT_OK command has not been accepted
Return: Std_ReturnType
Precondition: None
Postcondition: None
5.9.4.4. function Wdg_SetTriggerCondition
void Wdg_SetTriggerCondition(
uint16 Timeout
)
Brief: Sets the timeout value for the trigger counter.
Parameters:
Timeout Timeout value (milliseconds) for setting the trigger counter
Returns:
None
Return: None
Precondition: None
Postcondition: None