5.5. LIN
5.5.1. Types
Base type |
Type Name |
Brief |
|---|---|---|
enum |
Enum of Lin Interrupt line number, 0 or 1. |
|
enum |
Enum of Lin Loopbackmode, Internal/External/Disabled Type selection. |
5.5.1.1. enum Lin_InterruptLineNum
Enumerator |
Value |
Description |
|---|---|---|
LIN_INTERRUPT_LINE_NUM_0 |
0x0U |
Use Interrupt Line 0. |
LIN_INTERRUPT_LINE_NUM_1 |
0x1U |
Use Interrupt Line 1. |
Brief: Enum of Lin Interrupt line number, 0 or 1.
5.5.1.2. enum Lin_LoopbackModeType
Enumerator |
Value |
Description |
|---|---|---|
LIN_LOOPBACK_DISABLED |
Loopback disabled. |
|
LIN_LOOPBACK_INTERNAL |
Loopback internal. |
|
LIN_LOOPBACK_EXTERNAL |
Loopback external. |
Brief: Enum of Lin Loopbackmode, Internal/External/Disabled Type selection.
5.5.2. Structures
Name |
Brief |
|---|---|
Lin Channel type structure. |
|
LIN Channel Configuration structure. |
|
Lin Controller Configuration structure. |
|
Lin Controller BaudRate Configuration. |
5.5.3. Defines
Name |
Brief |
|---|---|
LIN_SW_MAJOR_VERSION |
Driver Implementation Major Version. |
LIN_SW_MINOR_VERSION |
Driver Implementation Minor Version. |
LIN_SW_PATCH_VERSION |
Driver Implementation Patch Version. |
LIN_AR_RELEASE_MAJOR_VERSION |
AUTOSAR Major version specification implemented by LIN Driver. |
LIN_AR_RELEASE_MINOR_VERSION |
AUTOSAR Minor version specification implemented by LIN Driver. |
LIN_AR_RELEASE_REVISION_VERSION |
AUTOSAR Patch version specification implemented by LIN Driver. |
LIN_VENDOR_ID |
Texas Instruments Vendor ID. |
LIN_MODULE_ID |
LIN Driver Module ID. |
LIN_INSTANCE_ID |
LIN Driver Instance ID. |
LIN_E_UNINIT |
API service used without module initialization. |
LIN_E_INVALID_CHANNEL |
API service used with an invalid or inactive channel parameter. |
LIN_E_INVALID_POINTER |
API service called with invalid configuration pointer. |
LIN_E_STATE_TRANSITION |
Invalid state transition for the current state. |
LIN_E_PARAM_POINTER |
API service called with a NULL pointer. |
LIN_SID_INIT |
Service ID - Lin_Init(). |
LIN_SID_GET_VERSION_INFO |
Service ID - Lin_GetVersionInfo(). |
LIN_SID_SEND_FRAME |
Service ID - Lin_SendFrame(). |
LIN_SID_GOTO_SLEEP |
Service ID - Lin_GoToSleep(). |
LIN_SID_WAKEUP |
Service ID - Lin_Wakeup(). |
LIN_SID_GET_STATUS |
Service ID - Lin_GetStatus(). |
LIN_SID_GOTO_SLEEP_INTERNAL |
Service ID - Lin_GoToSleepInternal(). |
LIN_SID_CHECK_WAKEUP |
Service ID - Lin_CheckWakeup(). |
LIN_SID_WAKEUP_INTERNAL |
Service ID - Lin_WakeupInternal(). |
LIN_ISR_CAT1_RTINT |
Category 1 RT ISR type. |
LIN_ISR_CAT1_INT |
Category 1 ISR type. |
LIN_ISR_CAT2 |
Category 2 ISR type. |
5.5.4. Functions
Return type |
Function Name |
Brief |
|---|---|---|
void |
Lin_GetVersionInfo(Std_VersionInfoType * versioninfo) |
Service to get the version information of the module. |
void |
Lin_Init(const Lin_ConfigType * Config) |
Lin_Init - Initializes the LIN module. |
Std_ReturnType |
Lin_CheckWakeup(uint8 Channel) |
Lin_CheckWakeup - This function checks if a wakeup has occurred on the addressed LIN channel. |
Std_ReturnType |
Lin_SendFrame(uint8 Channel, const Lin_PduType * PduInfoPtr) |
Lin_SendFrame - Sends a LIN header and a LIN response, if necessary. The direction of the frame response (master response, slave response, slave-to-slave communication) is provided by the PduInfoPtr. |
Std_ReturnType |
Lin_GoToSleep(uint8 Channel) |
Lin_GoToSleep - The service instructs the driver to transmit a go-to-sleep-command on the addressed LIN channel. |
Std_ReturnType |
Lin_GoToSleepInternal(uint8 Channel) |
Lin_GoToSleepInternal - Sets the channel state to LIN_CH_SLEEP, enables the wake-up detection and optionally sets the LIN hardware unit to reduced power operation mode. |
Std_ReturnType |
Lin_Wakeup(uint8 Channel) |
Lin_Wakeup - Generates a wake up pulse and sets the channel state to LIN_CH_OPERATIONAL. |
Std_ReturnType |
Lin_WakeupInternal(uint8 Channel) |
Lin_WakeupInternal - Generates a wake up pulse and sets the channel state to LIN_CH_OPERATIONAL without generating a wake up pulse. |
Lin_StatusType |
Lin_GetStatus(uint8 Channel, uint8 ** Lin_SduPtr) |
Lin_GetStatus - Gets the status of the LIN driver. |
5.5.4.1. function Lin_GetVersionInfo
void Lin_GetVersionInfo(
Std_VersionInfoType * versioninfo
)
Brief: Service to get the version information of the module.
This service writes the version information of this module into the data structure referenced by the parameter. If this parameter references NULL_PTR, a development error is reported to Det. This service is only available if the pre-compile configuration parameter LIN_GET_VERSION_INFO_API is enabled.
Parameters:
versioninfo structure that contains the version information parameters.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.5.4.2. function Lin_Init
void Lin_Init(
const Lin_ConfigType * Config
)
Brief: Lin_Init - Initializes the LIN module.
Parameters:
Config Pointer to LIN driver configuration set.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.5.4.3. function Lin_CheckWakeup
Std_ReturnType Lin_CheckWakeup(
uint8 Channel
)
Brief: Lin_CheckWakeup - This function checks if a wakeup has occurred on the addressed LIN channel.
Parameters:
Channel LIN channel to be addressed.
Returns:
E_OK No error has occurred during execution of the API
E_NOT_OK An error has occurred during execution of the API
Return: return_value
Precondition: None
Postcondition: None
5.5.4.4. function Lin_SendFrame
Std_ReturnType Lin_SendFrame(
uint8 Channel,
const Lin_PduType * PduInfoPtr
)
Brief: Lin_SendFrame - Sends a LIN header and a LIN response, if necessary. The direction of the frame response (master response, slave response, slave-to-slave communication) is provided by the PduInfoPtr.
Parameters:
Channel LIN channel to be addressed.
PduInfoPtr Pointer to PDU containing the PID, checksum model, response type, Dl and SDU data pointer
Returns:
E_OK Send command has been accepted.
E_NOT_OK Send command has not been accepted, development or production error occurred.
Return: return_value
Precondition: None
Postcondition: None
5.5.4.5. function Lin_GoToSleep
Std_ReturnType Lin_GoToSleep(
uint8 Channel
)
Brief: Lin_GoToSleep - The service instructs the driver to transmit a go-to-sleep-command on the addressed LIN channel.
Parameters:
Channel LIN channel to be addressed.
Returns:
E_OK Sleep command has been accepted.
E_NOT_OK Sleep command has not been accepted, development or production error occurred.
Return: return_value
Precondition: None
Postcondition: None
5.5.4.6. function Lin_GoToSleepInternal
Std_ReturnType Lin_GoToSleepInternal(
uint8 Channel
)
Brief: Lin_GoToSleepInternal - Sets the channel state to LIN_CH_SLEEP, enables the wake-up detection and optionally sets the LIN hardware unit to reduced power operation mode.
Parameters:
Channel LIN channel to be addressed.
Returns:
E_OK Command has been accepted.
E_NOT_OK Command has not been accepted, development or production error occurred.
Return: return_value
Precondition: None
Postcondition: None
5.5.4.7. function Lin_Wakeup
Std_ReturnType Lin_Wakeup(
uint8 Channel
)
Brief: Lin_Wakeup - Generates a wake up pulse and sets the channel state to LIN_CH_OPERATIONAL.
Parameters:
Channel LIN channel to be addressed.
Returns:
E_OK Wake-up request has been accepted
E_NOT_OK Wake-up request has not been accepted, development or production error occurred.
Return: return_value
Precondition: None
Postcondition: None
5.5.4.8. function Lin_WakeupInternal
Std_ReturnType Lin_WakeupInternal(
uint8 Channel
)
Brief: Lin_WakeupInternal - Generates a wake up pulse and sets the channel state to LIN_CH_OPERATIONAL without generating a wake up pulse.
Parameters:
Channel LIN channel to be addressed.
Returns:
E_OK Wake-up request has been accepted
E_NOT_OK Wake-up request has not been accepted, development or production error occurred.
Return: return_value
Precondition: None
Postcondition: None
5.5.4.9. function Lin_GetStatus
Lin_StatusType Lin_GetStatus(
uint8 Channel,
uint8 ** Lin_SduPtr
)
Brief: Lin_GetStatus - Gets the status of the LIN driver.
Parameters:
Channel LIN channel to be addressed.
Lin_SduPtr Pointer to pointer to a shadow buffer or memory mapped LIN Hardware receive buffer where the current SDU is stored.
Returns:
LIN_NOT_OK Development or production error occurred
LIN_TX_OK Successful transmission
LIN_TX_BUSY Ongoing transmission (Header or Response)
LIN_TX_HEADER_ERROR Erroneous header transmission such as:
Mismatch between sent and read back data
Identifier parity error or Physical bus error
LIN_TX_ERROR Erroneous response transmission such as:
Mismatch between sent and read back data
Physical bus error
LIN_RX_OK Reception of correct response
LIN_RX_BUSY Ongoing reception: at least one response byte has been received, but the checksum byte has not been received
LIN_RX_ERROR Erroneous response reception such as:
Framing error
Overrun error
Checksum error or Short response
LIN_RX_NO_RESPONSE No response byte has been received so far
LIN_OPERATIONAL Normal operation; the related LIN channel is woken up from the LIN_CH_SLEEP and no data has been sent.
LIN_CH_SLEEP Sleep state operation; in this state wake-up detection from slave nodes is enabled.
Return: return_value
Precondition: None
Postcondition: None