5.7. PORT
5.7.1. Types
Base type |
Type Name |
Brief |
|---|---|---|
enum |
Enum of Port Direction. |
|
enum |
Enum of Port Pin Level. |
|
enum |
Enum of Port Pin Pad, Up/Down Type selection. |
|
enum |
Values that can be passed to set qualification parameter to initialize MCU module. |
|
enum |
Values that can be passed to select master core for MCU module. |
|
enum |
Values that can be passed to set the mode in which Pin should operate. |
|
typedef uint32 |
Type for symbolic name of Port pins. |
|
typedef uint32 |
Pin Mode type structure. |
|
typedef uint8 |
Type for Pin Config Flag. Pin config flags Bit 0 - Is Pin configurable? Bit 1 - Does Pin support Analog Mode? Bit 2 - Does Pin operate in AGPIO mode? Bit 3 - Does Pin operate in AIO mode? Bit 4 - Does Pin operate in GPIO mode? |
5.7.1.1. enum Port_PinDirectionType
Enumerator |
Value |
Description |
|---|---|---|
PORT_PIN_IN |
Direction IN. |
|
PORT_PIN_OUT |
Direction OUT. |
|
PORT_PIN_NA |
NA Direction. |
Brief: Enum of Port Direction.
5.7.1.2. enum Port_PinLevelValueType
Enumerator |
Value |
Description |
|---|---|---|
PORT_PIN_LEVEL_HIGH |
Pin Level HIGH. |
|
PORT_PIN_LEVEL_LOW |
Pin Level LOW. |
|
PORT_PIN_LEVEL_NA |
Pin Level NA. |
Brief: Enum of Port Pin Level.
5.7.1.3. enum Port_PinPadConfigType
Enumerator |
Value |
Description |
|---|---|---|
PORT_PIN_TYPE_STD |
1U |
Standard pad configuration with pull up disable. |
PORT_PIN_TYPE_PULLUP |
2U |
Enable pull up for the pin. |
PORT_PIN_TYPE_STD_PULLUP |
3U |
Standard pad configuration with pull up enable. |
PORT_PIN_TYPE_OPEN_DRAIN |
4U |
Open Drain pad configuration with pull up disable. |
PORT_PIN_TYPE_OPEN_DRAIN_PULLUP |
6U |
Open Drain pad configuration with pull up enable. |
PORT_PIN_TYPE_NA |
255U |
No pad configuration. |
Brief: Enum of Port Pin Pad, Up/Down Type selection.
5.7.1.4. enum Port_PinQualificationMode
Enumerator |
Value |
Description |
|---|---|---|
PORT_QUAL_SYNC |
Synchronization to SYSCLKOUT. |
|
PORT_QUAL_3SAMPLE |
Qualified with 3 samples. |
|
PORT_QUAL_6SAMPLE |
Qualified with 6 samples. |
|
PORT_QUAL_ASYNC |
No synchronization. |
|
PORT_QUAL_NA |
Invalid synchronization. |
Brief: Values that can be passed to set qualification parameter to initialize MCU module.
5.7.1.5. enum Port_PinCoreSelect
Enumerator |
Value |
Description |
|---|---|---|
PORT_CORE_CPU1 |
CPU1 selected as master core. |
|
PORT_CORE_CPU2 |
CPU2 selected as master core. |
|
PORT_CORE_CPU3 |
CPU3 selected as master core. |
Brief: Values that can be passed to select master core for MCU module.
5.7.1.6. enum Port_AnalogModeType
Enumerator |
Value |
Description |
|---|---|---|
PORT_ANALOG_DISABLED |
Pin is in digital mode. |
|
PORT_ANALOG_ENABLED |
Pin is in analog mode. |
Brief: Values that can be passed to set the mode in which Pin should operate.
5.7.1.7. typedef Port_PinType
typedef uint32 Port_PinType;
Brief: Type for symbolic name of Port pins.
5.7.1.8. typedef Port_PinModeType
typedef uint32 Port_PinModeType;
Brief: Pin Mode type structure.
5.7.1.9. typedef Port_PinConfigFlagType
typedef uint8 Port_PinConfigFlagType;
Brief: Type for Pin Config Flag. Pin config flags Bit 0 - Is Pin configurable? Bit 1 - Does Pin support Analog Mode? Bit 2 - Does Pin operate in AGPIO mode? Bit 3 - Does Pin operate in AIO mode? Bit 4 - Does Pin operate in GPIO mode?
5.7.2. Structures
Name |
Brief |
|---|---|
Pin Mux Mode Config type structure. |
|
Pin Configuration structure. |
|
PORT Module ROOT configuration. |
|
Controller Specific structure. |
5.7.3. Defines
Name |
Brief |
|---|---|
PORT_SW_MAJOR_VERSION |
Driver Implementation Major Version. |
PORT_SW_MINOR_VERSION |
Driver Implementation Minor Version. |
PORT_SW_PATCH_VERSION |
Driver Implementation Patch Version. |
PORT_AR_RELEASE_MAJOR_VERSION |
AUTOSAR Major version specification implemented by PORT Driver. |
PORT_AR_RELEASE_MINOR_VERSION |
AUTOSAR Minor version specification implemented by PORT Driver. |
PORT_AR_RELEASE_REVISION_VERSION |
AUTOSAR Patch version specification implemented by PORT Driver. |
PORT_VENDOR_ID |
Texas Instruments Vendor ID. |
PORT_MODULE_ID |
PORT Driver Module ID. |
PORT_INSTANCE_ID |
PORT Driver Instance ID. |
PORT_E_PARAM_PIN |
Invalid Port Pin ID requested. |
PORT_E_DIRECTION_UNCHANGEABLE |
Port Pin not configured as changeable. |
PORT_E_INIT_FAILED |
API Port_Init service called with wrong parameter. |
PORT_E_PARAM_INVALID_MODE |
API Port_SetPinMode service called when mode is unchangeable. |
PORT_E_MODE_UNCHANGEABLE |
API Port_SetPinMode service called when mode is unchangeable. |
PORT_E_UNINIT |
API service called without module initialization. |
PORT_E_PARAM_POINTER |
APIs called with a Null pointer. |
PORT_SID_INIT |
Service ID - Port_Init(). |
PORT_SID_SET_PIN_DIR |
Service ID - Port_SetPinDirection(). |
PORT_SID_REFRESH_PORT_DIR |
Service ID - Port_RefreshPortDirection() |
PORT_SID_GET_VERSION_INFO |
Service ID - Port_GetVersionInfo(). |
PORT_SID_SET_PIN_MODE |
Service ID - Port_SetPinMode(). |
PORT_SID_COMMIT_CONFIGURATION |
Service ID - Port_CommitConfiguration(). |
5.7.4. Functions
Return type |
Function Name |
Brief |
|---|---|---|
void |
Port_Init(const Port_ConfigType * CfgPtr) |
Initializes the Port Driver module. |
void |
Port_SetPinDirection(Port_PinType Pin, Port_PinDirectionType Direction) |
Sets the port pin direction. |
void |
Port_RefreshPortDirection(void ) |
Refreshes port direction. |
void |
Port_GetVersionInfo(Std_VersionInfoType * versioninfo) |
Service to get the version information of the module. |
void |
Port_SetPinMode(Port_PinType Pin, Port_PinModeType Mode) |
Sets the port pin mode. |
void |
Port_CommitConfiguration(void ) |
Commits the locked Critical Configuration registers for the current Configuration. |
5.7.4.1. function Port_Init
void Port_Init(
const Port_ConfigType * CfgPtr
)
Brief: Initializes the Port Driver module.
This function is called by user to initialize the Port pins of the microcontroller
Parameters:
CfgPtr is the configuration pointer for Port module.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.7.4.2. function Port_SetPinDirection
void Port_SetPinDirection(
Port_PinType Pin,
Port_PinDirectionType Direction
)
Brief: Sets the port pin direction.
This function is used to change the direction of the pin during runtime.
Parameters:
Pin is the symbolic name of the pin.
Direction is the direction to which pin is to be set.
Returns:
None
Return: None
Precondition: Port_Init should be called before calling this function
Postcondition: None
5.7.4.3. function Port_RefreshPortDirection
void Port_RefreshPortDirection(
void
)
Brief: Refreshes port direction.
This function refreshes the Port pins to their initial direction. Pins whose direction can be changed during runtime are excluded from this action.
Returns:
None
Return: None
Precondition: Port_Init should be called before calling this function
Postcondition: None
5.7.4.4. function Port_GetVersionInfo
void Port_GetVersionInfo(
Std_VersionInfoType * versioninfo
)
Brief: Service to get the version information of the module.
This service writes the version information of this module into the data structure referenced by the parameter. If this parameter references NULL_PTR, a development error is reported to Det. This service is only available if the pre-compile configuration parameter PORT_CFG_GET_VERSION_INFO_API is enabled.
Parameters:
versioninfo structure that contains the version information parameters.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.7.4.5. function Port_SetPinMode
void Port_SetPinMode(
Port_PinType Pin,
Port_PinModeType Mode
)
Brief: Sets the port pin mode.
This function is used to change the Mode of the pin during runtime.
Parameters:
Pin is the symbolic name of the pin.
Mode is desired functionality of the Pin e.g. PORT_PIN_MODE_ADC, PORT_PIN_MODE_DIO etc.
Returns:
None
Return: None
Precondition: Port_Init should be called before calling this function
Postcondition: None
5.7.4.6. function Port_CommitConfiguration
void Port_CommitConfiguration(
void
)
Brief: Commits the locked Critical Configuration registers for the current Configuration.
This function Commits the locked Critical Configuration registers for the current Configuration
Returns:
None
Return: None
Precondition: Port_Init should be called before calling this function
Postcondition: None