5.2. DIO
5.2.1. Types
Base type |
Type Name |
Brief |
|---|---|---|
typedef uint32 |
Numeric ID of a DIO channel. |
|
typedef uint32 |
Numeric ID of a DIO port. |
|
typedef uint8 |
These are the possible levels a DIO channel can have (input or output). |
|
typedef uint32 |
If the uC owns ports of different port widths Dio_PortLevelType inherits the size of the largest port. |
5.2.1.1. typedef Dio_ChannelType
typedef uint32 Dio_ChannelType;
Brief: Numeric ID of a DIO channel.
5.2.1.2. typedef Dio_PortType
typedef uint32 Dio_PortType;
Brief: Numeric ID of a DIO port.
5.2.1.3. typedef Dio_LevelType
typedef uint8 Dio_LevelType;
Brief: These are the possible levels a DIO channel can have (input or output).
5.2.1.4. typedef Dio_PortLevelType
typedef uint32 Dio_PortLevelType;
Brief: If the uC owns ports of different port widths Dio_PortLevelType inherits the size of the largest port.
5.2.2. Structures
Name |
Brief |
|---|---|
Type definition for identifying channel groups (meaning a set of pins in one port). |
5.2.3. Defines
Name |
Brief |
|---|---|
DIO_SW_MAJOR_VERSION |
Driver Implementation Major Version. |
DIO_SW_MINOR_VERSION |
Driver Implementation Minor Version. |
DIO_SW_PATCH_VERSION |
Driver Implementation Patch Version. |
DIO_AR_RELEASE_MAJOR_VERSION |
AUTOSAR Major version specification implemented by DIO Driver. |
DIO_AR_RELEASE_MINOR_VERSION |
AUTOSAR Minor version specification implemented by DIO Driver. |
DIO_AR_RELEASE_REVISION_VERSION |
AUTOSAR Patch version specification implemented by DIO Driver. |
DIO_VENDOR_ID |
Texas Instruments Vendor ID. |
DIO_MODULE_ID |
DIO Driver Module ID. |
DIO_INSTANCE_ID |
DIO Driver Instance ID. |
DIO_E_PARAM_INVALID_CHANNEL_ID |
API service called with invalid channel ID. |
DIO_E_PARAM_INVALID_PORT_ID |
API service called with invalid port ID. |
DIO_E_PARAM_INVALID_GROUP |
API service called with invalid channel group ID. |
DIO_E_PARAM_POINTER |
Dio_GetVersionInfo() called with NULL_PTR as parameter. |
DIO_SID_READ_CHANNEL |
Dio_ReadChannel() |
DIO_SID_WRITE_CHANNEL |
Dio_WriteChannel() |
DIO_SID_READ_PORT |
Dio_ReadPort() |
DIO_SID_WRITE_PORT |
Dio_WritePort() |
DIO_SID_READ_CHANNEL_GROUP |
Dio_ReadChannelGroup() |
DIO_SID_WRITE_CHANNEL_GROUP |
Dio_WriteChannelGroup() |
DIO_SID_FLIP_CHANNEL |
Dio_FlipChannel() |
DIO_SID_GET_VERSION_INFO |
Dio_GetVersionInfo() |
GPIO_PORT_A |
GPIO PORT A identifier. |
GPIO_PORT_B |
GPIO PORT B identifier. |
GPIO_PORT_C |
GPIO PORT C identifier. |
GPIO_PORT_D |
GPIO PORT D identifier. |
GPIO_PORT_E |
GPIO PORT E identifier. |
GPIO_PORT_F |
GPIO PORT F identifier. |
GPIO_PORT_G |
GPIO PORT G identifier. |
GPIO_PORT_H |
GPIO PORT H identifier. |
5.2.4. Functions
Return type |
Function Name |
Brief |
|---|---|---|
void |
Dio_GetVersionInfo(Std_VersionInfoType * Versioninfo) |
Service to get the version information of the module. |
Dio_ReadChannel(Dio_ChannelType ChannelId) |
Returns the value of the specified DIO channel. |
|
void |
Dio_WriteChannel(Dio_ChannelType ChannelId, Dio_LevelType Level) |
Service to set a level of a channel. |
Dio_ReadPort(Dio_PortType PortId) |
Returns the level of all channels of that port. |
|
void |
Dio_WritePort(Dio_PortType PortId, Dio_PortLevelType Level) |
Service to set a value of the port. |
Dio_ReadChannelGroup(const Dio_ChannelGroupType * ChannelGroupIdPtr) |
This Service reads a subset of the adjoining bits of a port. |
|
void |
Dio_WriteChannelGroup(const Dio_ChannelGroupType * ChannelGroupIdPtr, Dio_PortLevelType Level) |
Service to set a subset of the adjoining bits of a port to a specified level. |
Dio_FlipChannel(Dio_ChannelType ChannelId) |
Service to flip the value of a DIO channel. |
5.2.4.1. function Dio_GetVersionInfo
void Dio_GetVersionInfo(
Std_VersionInfoType * Versioninfo
)
Brief: Service to get the version information of the module.
This service writes the version information of this module into the data structure referenced by the parameter. If this parameter references NULL_PTR, a development error is reported to Det. This service is only available if the pre-compile configuration parameter DIO_VERSION_INFO_API is enabled.
Parameters:
Versioninfo structure that contains the version information parameters.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.2.4.2. function Dio_ReadChannel
Dio_LevelType Dio_ReadChannel(
Dio_ChannelType ChannelId
)
Brief: Returns the value of the specified DIO channel.
This service is to read from a specified DIO channel. If the channel specified is not valid, a development error is reported to Det. The value for the DIO channel is read and returned.
Parameters:
ChannelId specifies the ID of the general-purpose digital input/output pin.
Returns:
STD_HIGH logic level 1
STD_LOW logic level 0
Return: Returns the logic level(value) on a specified DIO pin of type Dio_LevelType.
Precondition: None
Postcondition: None
5.2.4.3. function Dio_WriteChannel
void Dio_WriteChannel(
Dio_ChannelType ChannelId,
Dio_LevelType Level
)
Brief: Service to set a level of a channel.
This service is to set a specified level of a particular DIO channel. If the channel specified is not valid, a development error is reported to Det. The value is written to the specified DIO channel.
Parameters:
ChannelId specifies the ID of the general-purpose digital input/output pin.
Level specifies the value to be written to the channel. Value can be STD_HIGH or STD_LOW.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.2.4.4. function Dio_ReadPort
Dio_PortLevelType Dio_ReadPort(
Dio_PortType PortId
)
Brief: Returns the level of all channels of that port.
This service reads the value of a DIO port. If the port is not enabled, a development error is reported to Det. The value of the port of which the ID is specified is read and returned.
Parameters:
PortId specifies the ID of the grouped Input/Output channels.
Returns:
Value of type Dio_PortLevelType
Return: level of all the channels of the specified port
Precondition: None
Postcondition: None
5.2.4.5. function Dio_WritePort
void Dio_WritePort(
Dio_PortType PortId,
Dio_PortLevelType Level
)
Brief: Service to set a value of the port.
This service sets a specified value of a DIO port. If the port is not enabled, a development error is reported to Det. The value is written to the specified DIO port.
Parameters:
PortId specifies the ID of the grouped Input/Output channels.
Level Value consisting of level of all the channels of the specified port.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.2.4.6. function Dio_ReadChannelGroup
Dio_PortLevelType Dio_ReadChannelGroup(
const Dio_ChannelGroupType * ChannelGroupIdPtr
)
Brief: This Service reads a subset of the adjoining bits of a port.
This service reads the value of the subset of the bits of a port. If this parameter references NULL_PTR, a development error is reported to Det. The value of the level of the channel group is read and returned.
Parameters:
ChannelGroupIdPtr for referencing channel group structures.
Returns:
value of type Dio_PortLevelType
Return: levels of the specified channel group.
Precondition: None
Postcondition: None
5.2.4.7. function Dio_WriteChannelGroup
void Dio_WriteChannelGroup(
const Dio_ChannelGroupType * ChannelGroupIdPtr,
Dio_PortLevelType Level
)
Brief: Service to set a subset of the adjoining bits of a port to a specified level.
This service writes the specified value to a subset of the bits of a port. If this parameter references NULL_PTR, a development error is reported to Det. The information of the channel group is in the referenced channel group structure.The data is then written to the port.
Parameters:
ChannelGroupIdPtr for referencing channel group structures.
Level Value consisting of levels of the specified channel group.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.2.4.8. function Dio_FlipChannel
Dio_LevelType Dio_FlipChannel(
Dio_ChannelType ChannelId
)
Brief: Service to flip the value of a DIO channel.
This service is to change the value of the corresponding DIO channel.If the channel specified is not valid, a development error is reported to Det. The value of the specified channel is flipped.This service is only available if the pre-compile configuration parameter DIO_FLIP_CHANNEL_API is enabled.
Parameters:
ChannelId specifies the ID of the general-purpose digital input/output pin.
Returns:
STD_HIGH logic level 1 STD_LOW: logic level 0
Return: Value consisting of level of the specified channel after flip of type Dio_LevelType.
Precondition: None
Postcondition: None