6.2. DIO

6.2.1. Types

Base type

Type Name

Brief

typedef uint32

Dio_ChannelType

Numeric ID of a DIO channel.

typedef uint32

Dio_PortType

Numeric ID of a DIO port.

typedef uint8

Dio_LevelType

These are the possible levels a DIO channel can have (input or output).

typedef uint32

Dio_PortLevelType

If the uC owns ports of different port widths Dio_PortLevelType inherits the size of the largest port.

6.2.1.1. typedef Dio_ChannelType

typedef uint32 Dio_ChannelType;

Brief: Numeric ID of a DIO channel.

6.2.1.2. typedef Dio_PortType

typedef uint32 Dio_PortType;

Brief: Numeric ID of a DIO port.

6.2.1.3. typedef Dio_LevelType

typedef uint8 Dio_LevelType;

Brief: These are the possible levels a DIO channel can have (input or output).

6.2.1.4. typedef Dio_PortLevelType

typedef uint32 Dio_PortLevelType;

Brief: If the uC owns ports of different port widths Dio_PortLevelType inherits the size of the largest port.

6.2.2. Structures

Name

Brief

Dio_ChannelGroupType

Type definition for identifying channel groups (meaning a set of pins in one port).

6.2.3. Defines

Name

Brief

DIO_SW_MAJOR_VERSION

Driver Implementation Major Version.

DIO_SW_MINOR_VERSION

Driver Implementation Minor Version.

DIO_SW_PATCH_VERSION

Driver Implementation Patch Version.

DIO_AR_RELEASE_MAJOR_VERSION

AUTOSAR Major version specification implemented by DIO Driver.

DIO_AR_RELEASE_MINOR_VERSION

AUTOSAR Minor version specification implemented by DIO Driver.

DIO_AR_RELEASE_REVISION_VERSION

AUTOSAR Patch version specification implemented by DIO Driver.

DIO_VENDOR_ID

Texas Instruments Vendor ID.

DIO_MODULE_ID

DIO Driver Module ID.

DIO_INSTANCE_ID

DIO Driver Instance ID.

DIO_E_PARAM_INVALID_CHANNEL_ID

API service called with invalid channel ID.

DIO_E_PARAM_INVALID_PORT_ID

API service called with invalid port ID.

DIO_E_PARAM_INVALID_GROUP

API service called with invalid channel group ID.

DIO_E_PARAM_POINTER

Dio_GetVersionInfo() called with NULL_PTR as parameter.

DIO_SID_READ_CHANNEL

Dio_ReadChannel()

DIO_SID_WRITE_CHANNEL

Dio_WriteChannel()

DIO_SID_READ_PORT

Dio_ReadPort()

DIO_SID_WRITE_PORT

Dio_WritePort()

DIO_SID_READ_CHANNEL_GROUP

Dio_ReadChannelGroup()

DIO_SID_WRITE_CHANNEL_GROUP

Dio_WriteChannelGroup()

DIO_SID_FLIP_CHANNEL

Dio_FlipChannel()

DIO_SID_GET_VERSION_INFO

Dio_GetVersionInfo()

GPIO_PORT_A

GPIO PORT A identifier.

GPIO_PORT_B

GPIO PORT B identifier.

GPIO_PORT_C

GPIO PORT C identifier.

GPIO_PORT_D

GPIO PORT D identifier.

GPIO_PORT_E

GPIO PORT E identifier.

GPIO_PORT_F

GPIO PORT F identifier.

GPIO_PORT_G

GPIO PORT G identifier.

GPIO_PORT_H

GPIO PORT H identifier.

6.2.4. Functions

Return type

Function Name

Brief

void

Dio_GetVersionInfo(Std_VersionInfoType * Versioninfo)

Service to get the version information of the module.

Dio_LevelType

Dio_ReadChannel(Dio_ChannelType ChannelId)

Returns the value of the specified DIO channel.

void

Dio_WriteChannel(Dio_ChannelType ChannelId, Dio_LevelType Level)

Service to set a level of a channel.

Dio_PortLevelType

Dio_ReadPort(Dio_PortType PortId)

Returns the level of all channels of that port.

void

Dio_WritePort(Dio_PortType PortId, Dio_PortLevelType Level)

Service to set a value of the port.

Dio_PortLevelType

Dio_ReadChannelGroup(const Dio_ChannelGroupType * ChannelGroupIdPtr)

This Service reads a subset of the adjoining bits of a port.

void

Dio_WriteChannelGroup(const Dio_ChannelGroupType * ChannelGroupIdPtr, Dio_PortLevelType Level)

Service to set a subset of the adjoining bits of a port to a specified level.

Dio_LevelType

Dio_FlipChannel(Dio_ChannelType ChannelId)

Service to flip the value of a DIO channel.

6.2.4.1. function Dio_GetVersionInfo

void Dio_GetVersionInfo(
    Std_VersionInfoType * Versioninfo
)

Brief: Service to get the version information of the module.

This service writes the version information of this module into the data structure referenced by the parameter. If this parameter references NULL_PTR, a development error is reported to Det. This service is only available if the pre-compile configuration parameter DIO_VERSION_INFO_API is enabled.

Parameters:

  • Versioninfo structure that contains the version information parameters.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.2.4.2. function Dio_ReadChannel

Dio_LevelType Dio_ReadChannel(
    Dio_ChannelType ChannelId
)

Brief: Returns the value of the specified DIO channel.

This service is to read from a specified DIO channel. If the channel specified is not valid, a development error is reported to Det. The value for the DIO channel is read and returned.

Parameters:

  • ChannelId specifies the ID of the general-purpose digital input/output pin.

Returns:

  • STD_HIGH logic level 1

  • STD_LOW logic level 0

Return: Returns the logic level(value) on a specified DIO pin of type Dio_LevelType.

Precondition: None

Postcondition: None

6.2.4.3. function Dio_WriteChannel

void Dio_WriteChannel(
    Dio_ChannelType ChannelId,
    Dio_LevelType Level
)

Brief: Service to set a level of a channel.

This service is to set a specified level of a particular DIO channel. If the channel specified is not valid, a development error is reported to Det. The value is written to the specified DIO channel.

Parameters:

  • ChannelId specifies the ID of the general-purpose digital input/output pin.

  • Level specifies the value to be written to the channel. Value can be STD_HIGH or STD_LOW.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.2.4.4. function Dio_ReadPort

Dio_PortLevelType Dio_ReadPort(
    Dio_PortType PortId
)

Brief: Returns the level of all channels of that port.

This service reads the value of a DIO port. If the port is not enabled, a development error is reported to Det. The value of the port of which the ID is specified is read and returned.

Parameters:

  • PortId specifies the ID of the grouped Input/Output channels.

Returns:

  • Value of type Dio_PortLevelType

Return: level of all the channels of the specified port

Precondition: None

Postcondition: None

6.2.4.5. function Dio_WritePort

void Dio_WritePort(
    Dio_PortType PortId,
    Dio_PortLevelType Level
)

Brief: Service to set a value of the port.

This service sets a specified value of a DIO port. If the port is not enabled, a development error is reported to Det. The value is written to the specified DIO port.

Parameters:

  • PortId specifies the ID of the grouped Input/Output channels.

  • Level Value consisting of level of all the channels of the specified port.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.2.4.6. function Dio_ReadChannelGroup

Dio_PortLevelType Dio_ReadChannelGroup(
    const Dio_ChannelGroupType * ChannelGroupIdPtr
)

Brief: This Service reads a subset of the adjoining bits of a port.

This service reads the value of the subset of the bits of a port. If this parameter references NULL_PTR, a development error is reported to Det. The value of the level of the channel group is read and returned.

Parameters:

  • ChannelGroupIdPtr for referencing channel group structures.

Returns:

  • value of type Dio_PortLevelType

Return: levels of the specified channel group.

Precondition: None

Postcondition: None

6.2.4.7. function Dio_WriteChannelGroup

void Dio_WriteChannelGroup(
    const Dio_ChannelGroupType * ChannelGroupIdPtr,
    Dio_PortLevelType Level
)

Brief: Service to set a subset of the adjoining bits of a port to a specified level.

This service writes the specified value to a subset of the bits of a port. If this parameter references NULL_PTR, a development error is reported to Det. The information of the channel group is in the referenced channel group structure.The data is then written to the port.

Parameters:

  • ChannelGroupIdPtr for referencing channel group structures.

  • Level Value consisting of levels of the specified channel group.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.2.4.8. function Dio_FlipChannel

Dio_LevelType Dio_FlipChannel(
    Dio_ChannelType ChannelId
)

Brief: Service to flip the value of a DIO channel.

This service is to change the value of the corresponding DIO channel.If the channel specified is not valid, a development error is reported to Det. The value of the specified channel is flipped.This service is only available if the pre-compile configuration parameter DIO_FLIP_CHANNEL_API is enabled.

Parameters:

  • ChannelId specifies the ID of the general-purpose digital input/output pin.

Returns:

  • STD_HIGH logic level 1 STD_LOW: logic level 0

Return: Value consisting of level of the specified channel after flip of type Dio_LevelType.

Precondition: None

Postcondition: None