6.10. CDD_ADC

6.10.1. Types

Base type

Type Name

Brief

enum

Cdd_Adc_StatusType

Status type.

enum

Cdd_Adc_TriggerSrcType

Trigger source type.

enum

Cdd_Adc_StreamBufferModeType

Stream buffer mode type.

enum

Cdd_Adc_GroupAccessModeType

Group access mode type.

enum

Cdd_Adc_GroupConvModeType

Group conversion mode type.

enum

Cdd_Adc_HwUnitType

Specifies the identification (ID) for ADC Hardware instances.

enum

Cdd_Adc_PrescaleType

Defines supported prescaler values.

enum

Cdd_Adc_RefModeType

Defines supported reference voltage modes.

enum

Cdd_Adc_RefVoltType

Defines supported reference voltage types.

enum

Cdd_Adc_SignalModeType

Defines supported signal modes types.

enum

Cdd_Adc_SocPriorityType

Defines supported SOC priority types.

enum

Cdd_Adc_ResolutionType

Defines supported resolution modes.

enum

Cdd_Adc_IntNumType

Defines interrupts supported per ADC instance.

enum

Cdd_Adc_CheckerInputType

Defines possible input types to a safety checker unit.

enum

Cdd_Adc_TriggerType

Defines supported ADC triggers.

enum

Cdd_Adc_RepeaterModeType

Defines modes supported by a trigger repeater.

enum

Cdd_Adc_RepeaterType

Defines repeater instances supported per ADC instance.

enum

Cdd_Adc_PpbIdType

Defines PPB instances supported per ADC instance.

enum

Cdd_Adc_CompSelType

Defines PPB result compare types.

enum

Cdd_Adc_SafetyCheckFlagType

Defines safety checker flag types.

enum

Cdd_Adc_SafetyCheckEvtSrcType

Defines safety checker event sources for interrupt or event generation.

enum

Cdd_Adc_CheckFlagStatusType

Defines possible states of a flag of an event generated from a safety checker.

enum

Cdd_Adc_CheckerEventType

Defines supported events that can be generated from an interrupt event instance.

enum

Cdd_Adc_IntSocTriggerType

Defines interrupt trigger sources to SOCs.

enum

Cdd_Adc_EocPulseType

Defines End-Of-Conversion interrupt pulse modes.

enum

Cdd_Adc_InternalTestNodeType

Defines supported internal nodes that can be connected to ADC.

enum

Cdd_Adc_OsDetectModeType

Specifies open/short circuit modes.

typedef uint8

Cdd_Adc_GroupType

Numeric ID of an ADC channel group.

typedef uint8

Cdd_Adc_PpbType

Numeric ID of the PPB unit.

typedef uint16

Cdd_Adc_ValueGroupType

Type for reading the converted values of a channel group.

typedef uint8

Cdd_Adc_StreamNumSampleType

Type for configuring the number of channel conversions results in streaming access mode (in single access mode, parameter is 1)

typedef uint8

Cdd_Adc_CheckEvtType

Specifies the checker event id.

typedef uint8

Cdd_Adc_GlbTrigType

Specifies ID of the global software trigger

typedef uint8

Cdd_Adc_CheckerType

Numeric ID of an ADC safety result checker.

typedef uint8

Cdd_Adc_CheckerIntEvtType

Numeric ID of a safety checker interrupt event instance.

typedef uint8

Cdd_Adc_HwUnitInstanceType

Hardware unit instance type.

typedef void(*)(void)

Cdd_Adc_GroupEndNotifyType

Group end notification function pointer.

typedef void(*)(void)

Cdd_Adc_PpbNotifyType

Ppb notification function pointer.

6.10.1.1. enum Cdd_Adc_StatusType

Enumerator

Value

Description

CDD_ADC_IDLE

The conversion of the specified group has not been started.

CDD_ADC_BUSY

The conversion of the specified group has been started and is still going on.

CDD_ADC_COMPLETED

A conversion round (not the final one) of the group has been finished.

CDD_ADC_STREAM_COMPLETED

The result buffer is completely filled.

Brief: Status type.

6.10.1.2. enum Cdd_Adc_TriggerSrcType

Enumerator

Value

Description

CDD_ADC_TRIGG_SRC_SW

Group is triggered by a software API call.

CDD_ADC_TRIGG_SRC_HW

Group is triggered by a hardware event.

Brief: Trigger source type.

6.10.1.3. enum Cdd_Adc_StreamBufferModeType

Enumerator

Value

Description

CDD_ADC_STREAM_BUFFER_LINEAR

The ADC Driver stops the conversion as soon as the stream buffer is full (number of samples reached)

CDD_ADC_STREAM_BUFFER_CIRCULAR

The ADC Driver continues the conversion even if the stream buffer is full (number of samples reached) by wrapping around the stream buffer itself.

Brief: Stream buffer mode type.

6.10.1.4. enum Cdd_Adc_GroupAccessModeType

Enumerator

Value

Description

CDD_ADC_ACCESS_MODE_SINGLE

Single value access mode.

CDD_ADC_ACCESS_MODE_STREAMING

Streaming access mode.

Brief: Group access mode type.

6.10.1.5. enum Cdd_Adc_GroupConvModeType

Enumerator

Value

Description

CDD_ADC_CONV_MODE_ONESHOT

Exactly one conversion of each channel in an ADC channel group is performed after the trigger event.

CDD_ADC_CONV_MODE_CONTINUOUS

Repeated conversions of each ADC channel in an ADC channel group are performed.

Brief: Group conversion mode type.

6.10.1.6. enum Cdd_Adc_HwUnitType

Enumerator

Value

Description

CDD_ADCA

0U

CDD_ADCB

1U

CDD_ADCC

2U

CDD_ADCD

3U

CDD_ADCE

4U

Brief: Specifies the identification (ID) for ADC Hardware instances.

6.10.1.7. enum Cdd_Adc_PrescaleType

Enumerator

Value

Description

CDD_ADC_CLK_DIV_1_0

0U

CDD_ADC_CLK_DIV_2_0

2U

CDD_ADC_CLK_DIV_2_5

3U

CDD_ADC_CLK_DIV_3_0

4U

CDD_ADC_CLK_DIV_3_5

5U

CDD_ADC_CLK_DIV_4_0

6U

CDD_ADC_CLK_DIV_4_5

7U

CDD_ADC_CLK_DIV_5_0

8U

CDD_ADC_CLK_DIV_5_5

9U

CDD_ADC_CLK_DIV_6_0

10U

CDD_ADC_CLK_DIV_6_5

11U

CDD_ADC_CLK_DIV_7_0

12U

CDD_ADC_CLK_DIV_7_5

13U

CDD_ADC_CLK_DIV_8_0

14U

CDD_ADC_CLK_DIV_8_5

15U

Brief: Defines supported prescaler values.

6.10.1.8. enum Cdd_Adc_RefModeType

Enumerator

Value

Description

CDD_ADC_REFERENCE_INTERNAL

0U

CDD_ADC_REFERENCE_EXTERNAL

1U

Brief: Defines supported reference voltage modes.

6.10.1.9. enum Cdd_Adc_RefVoltType

Enumerator

Value

Description

CDD_ADC_REFERENCE_3_3V

0U

CDD_ADC_REFERENCE_2_5V

1U

Brief: Defines supported reference voltage types.

6.10.1.10. enum Cdd_Adc_SignalModeType

Enumerator

Value

Description

CDD_ADC_MODE_SINGLE_ENDED

0x00U

CDD_ADC_MODE_DIFFERENTIAL

0x80U

Brief: Defines supported signal modes types.

6.10.1.11. enum Cdd_Adc_SocPriorityType

Enumerator

Value

Description

CDD_ADC_PRI_ALL_ROUND_ROBIN

0U

CDD_ADC_PRI_SOC0_HIPRI

1U

CDD_ADC_PRIHRU_SOC1_HIPRI

2U

CDD_ADC_PRIHRU_SOC2_HIPRI

3U

CDD_ADC_PRIHRU_SOC3_HIPRI

4U

CDD_ADC_PRIHRU_SOC4_HIPRI

5U

CDD_ADC_PRIHRU_SOC5_HIPRI

6U

CDD_ADC_PRIHRU_SOC6_HIPRI

7U

CDD_ADC_PRIHRU_SOC7_HIPRI

8U

CDD_ADC_PRIHRU_SOC8_HIPRI

9U

CDD_ADC_PRIHRU_SOC9_HIPRI

10U

CDD_ADC_PRIHRU_SOC10_HIPRI

11U

CDD_ADC_PRIHRU_SOC11_HIPRI

12U

CDD_ADC_PRIHRU_SOC12_HIPRI

13U

CDD_ADC_PRIHRU_SOC13_HIPRI

14U

CDD_ADC_PRIHRU_SOC14_HIPRI

15U

CDD_ADC_PRIHRU_SOC15_HIPRI

16U

CDD_ADC_PRIHRU_SOC16_HIPRI

17U

CDD_ADC_PRIHRU_SOC17_HIPRI

18U

CDD_ADC_PRIHRU_SOC18_HIPRI

19U

CDD_ADC_PRIHRU_SOC19_HIPRI

20U

CDD_ADC_PRIHRU_SOC20_HIPRI

21U

CDD_ADC_PRIHRU_SOC21_HIPRI

22U

CDD_ADC_PRIHRU_SOC22_HIPRI

23U

CDD_ADC_PRIHRU_SOC23_HIPRI

24U

CDD_ADC_PRIHRU_SOC24_HIPRI

25U

CDD_ADC_PRIHRU_SOC25_HIPRI

26U

CDD_ADC_PRIHRU_SOC26_HIPRI

27U

CDD_ADC_PRIHRU_SOC27_HIPRI

28U

CDD_ADC_PRIHRU_SOC28_HIPRI

29U

CDD_ADC_PRIHRU_SOC29_HIPRI

30U

CDD_ADC_PRIHRU_SOC30_HIPRI

31U

CDD_ADC_PRI_ALL_HIPRI

32U

Brief: Defines supported SOC priority types.

6.10.1.12. enum Cdd_Adc_ResolutionType

Enumerator

Value

Description

CDD_ADC_RESOLUTION_12BIT

0x00U

CDD_ADC_RESOLUTION_16BIT

0x01U

CDD_ADC_RESOLUTION_NONE

Brief: Defines supported resolution modes.

6.10.1.13. enum Cdd_Adc_IntNumType

Enumerator

Value

Description

CDD_ADC_INT1

0U

CDD_ADC_INT2

1U

CDD_ADC_INT3

2U

CDD_ADC_INT4

3U

Brief: Defines interrupts supported per ADC instance.

6.10.1.14. enum Cdd_Adc_CheckerInputType

Enumerator

Value

Description

CDD_ADC_SAFETY_CHECKER_INPUT_DISABLE

0x0U

CDD_ADC_SAFETY_CHECKER_INPUT_SOC

0x1U

CDD_ADC_SAFETY_CHECKER_INPUT_PPB

0x2U

CDD_ADC_SAFETY_CHECKER_INPUT_PPBSUM

0x3U

Brief: Defines possible input types to a safety checker unit.

6.10.1.15. enum Cdd_Adc_TriggerType

Enumerator

Value

Description

CDD_ADC_TRIGGER_SW_ONLY

0x00U

CDD_ADC_TRIGGER_CPU1INT0

0x01U

CDD_ADC_TRIGGER_CPU1INT1

0x02U

CDD_ADC_TRIGGER_CPU1INT2

0x03U

CDD_ADC_TRIGGER_GPIO

0x04U

CDD_ADC_TRIGGER_EPWM1_SOCA

0x05U

CDD_ADC_TRIGGER_EPWM1_SOCB

0x06U

CDD_ADC_TRIGGER_EPWM2_SOCA

0x07U

CDD_ADC_TRIGGER_EPWM2_SOCB

0x08U

CDD_ADC_TRIGGER_EPWM3_SOCA

0x09U

CDD_ADC_TRIGGER_EPWM3_SOCB

0x0AU

CDD_ADC_TRIGGER_EPWM4_SOCA

0x0BU

CDD_ADC_TRIGGER_EPWM4_SOCB

0x0CU

CDD_ADC_TRIGGER_EPWM5_SOCA

0x0DU

CDD_ADC_TRIGGER_EPWM5_SOCB

0x0EU

CDD_ADC_TRIGGER_EPWM6_SOCA

0x0FU

CDD_ADC_TRIGGER_EPWM6_SOCB

0x10U

CDD_ADC_TRIGGER_EPWM7_SOCA

0x11U

CDD_ADC_TRIGGER_EPWM7_SOCB

0x12U

CDD_ADC_TRIGGER_EPWM8_SOCA

0x13U

CDD_ADC_TRIGGER_EPWM8_SOCB

0x14U

CDD_ADC_TRIGGER_EPWM9_SOCA

0x15U

CDD_ADC_TRIGGER_EPWM9_SOCB

0x16U

CDD_ADC_TRIGGER_EPWM10_SOCA

0x17U

CDD_ADC_TRIGGER_EPWM10_SOCB

0x18U

CDD_ADC_TRIGGER_EPWM11_SOCA

0x19U

CDD_ADC_TRIGGER_EPWM11_SOCB

0x1AU

CDD_ADC_TRIGGER_EPWM12_SOCA

0x1BU

CDD_ADC_TRIGGER_EPWM12_SOCB

0x1CU

CDD_ADC_TRIGGER_REPEATER1

0x28U

CDD_ADC_TRIGGER_REPEATER2

0x29U

CDD_ADC_TRIGGER_CLB1_OUT27

0x48U

CDD_ADC_TRIGGER_CLB2_OUT27

0x49U

CDD_ADC_TRIGGER_CLB3_OUT27

0x4AU

CDD_ADC_TRIGGER_CLB4_OUT27

0x4BU

CDD_ADC_TRIGGER_CLB5_OUT27

0x4CU

CDD_ADC_TRIGGER_CLB6_OUT27

0x4DU

CDD_ADC_TRIGGER_ECAP1

0x50U

CDD_ADC_TRIGGER_ECAP2

0x51U

CDD_ADC_TRIGGER_ECAP3

0x52U

CDD_ADC_TRIGGER_ECAP4

0x53U

CDD_ADC_TRIGGER_ECAP5

0x54U

CDD_ADC_TRIGGER_ECAP6

0x55U

CDD_ADC_TRIGGER_EPWM13_SOCA

0x58U

CDD_ADC_TRIGGER_EPWM13_SOCB

0x59U

CDD_ADC_TRIGGER_EPWM14_SOCA

0x5AU

CDD_ADC_TRIGGER_EPWM14_SOCB

0x5BU

CDD_ADC_TRIGGER_EPWM15_SOCA

0x5CU

CDD_ADC_TRIGGER_EPWM15_SOCB

0x5DU

CDD_ADC_TRIGGER_EPWM16_SOCA

0x5EU

CDD_ADC_TRIGGER_EPWM16_SOCB

0x5FU

CDD_ADC_TRIGGER_EPWM17_SOCA

0x60U

CDD_ADC_TRIGGER_EPWM17_SOCB

0x61U

CDD_ADC_TRIGGER_EPWM18_SOCA

0x62U

CDD_ADC_TRIGGER_EPWM18_SOCB

0x63U

CDD_ADC_TRIGGER_CPU2INT0

0x64U

CDD_ADC_TRIGGER_CPU2INT1

0x65U

CDD_ADC_TRIGGER_CPU2INT2

0x66U

CDD_ADC_TRIGGER_CPU3INT0

0x67U

CDD_ADC_TRIGGER_CPU3INT1

0x68U

CDD_ADC_TRIGGER_CPU3INT2

0x69U

Brief: Defines supported ADC triggers.

6.10.1.16. enum Cdd_Adc_RepeaterModeType

Enumerator

Value

Description

CDD_ADC_REPMODE_OVERSAMPLING

0x0U

CDD_ADC_REPMODE_UNDERSAMPLING

0x1U

Brief: Defines modes supported by a trigger repeater.

6.10.1.17. enum Cdd_Adc_RepeaterType

Enumerator

Value

Description

CDD_ADC_REPINST1

0x0U

CDD_ADC_REPINST2

0x1U

Brief: Defines repeater instances supported per ADC instance.

6.10.1.18. enum Cdd_Adc_PpbIdType

Enumerator

Value

Description

CDD_ADC_PPB_NUMBER1

0

CDD_ADC_PPB_NUMBER2

1

CDD_ADC_PPB_NUMBER3

2

CDD_ADC_PPB_NUMBER4

3

Brief: Defines PPB instances supported per ADC instance.

6.10.1.19. enum Cdd_Adc_CompSelType

Enumerator

Value

Description

CDD_ADC_COMPARE_PPBRESULT

0x0U

CDD_ADC_COMPARE_PPBPSUM

0x1U

CDD_ADC_COMPARE_PPBSUM

0x2U

Brief: Defines PPB result compare types.

6.10.1.20. enum Cdd_Adc_SafetyCheckFlagType

Enumerator

Value

Description

CDD_ADC_SAFETY_CHECK_OOT_FLG

0U

CDD_ADC_SAFETY_CHECK_RES1OVF_FLG

8U

CDD_ADC_SAFETY_CHECK_RES2OVF_FLG

16U

Brief: Defines safety checker flag types.

6.10.1.21. enum Cdd_Adc_SafetyCheckEvtSrcType

Enumerator

Value

Description

CDD_ADC_SAFETY_CHECK_RES1OVF

0U

CDD_ADC_SAFETY_CHECK_RES2OVF

4U

CDD_ADC_SAFETY_CHECK_OOT

8U

Brief: Defines safety checker event sources for interrupt or event generation.

6.10.1.22. enum Cdd_Adc_CheckFlagStatusType

Enumerator

Value

Description

CDD_ADC_SAFETY_CHECKER_FLG_NONE

CDD_ADC_SAFETY_CHECKER_RES1OVF_FLG

CDD_ADC_SAFETY_CHECKER_RES2OVF_FLG

CDD_ADC_SAFETY_CHECKER_OOT_FLG

Brief: Defines possible states of a flag of an event generated from a safety checker.

6.10.1.23. enum Cdd_Adc_CheckerEventType

Enumerator

Value

Description

CDD_ADC_CHECKER_EVT_1

CDD_ADC_CHECKER_EVT_2

CDD_ADC_CHECKER_EVT_3

CDD_ADC_CHECKER_EVT_4

Brief: Defines supported events that can be generated from an interrupt event instance.

6.10.1.24. enum Cdd_Adc_IntSocTriggerType

Enumerator

Value

Description

CDD_ADC_INT_SOC_TRIGGER_NONE

0U

CDD_ADC_INT_SOC_TRIGGER_ADCINT1

1U

CDD_ADC_INT_SOC_TRIGGER_ADCINT2

2U

Brief: Defines interrupt trigger sources to SOCs.

6.10.1.25. enum Cdd_Adc_EocPulseType

Enumerator

Value

Description

CDD_ADC_PULSE_END_OF_ACQ_WIN

0x00U

CDD_ADC_PULSE_END_OF_CONV

0x04U

Brief: Defines End-Of-Conversion interrupt pulse modes.

6.10.1.26. enum Cdd_Adc_InternalTestNodeType

Enumerator

Value

Description

CDD_ADC_TEST_NODE_NO_CONN

0U

CDD_ADC_TEST_NODE_VDDCORE

1U

CDD_ADC_TEST_NODE_VDDA

2U

CDD_ADC_TEST_NODE_VSSA

3U

CDD_ADC_TEST_NODE_VREFLOA

4U

CDD_ADC_TEST_NODE_VREFLOB

5U

CDD_ADC_TEST_NODE_CDAC1H

7U

CDD_ADC_TEST_NODE_CDAC1L

8U

CDD_ADC_TEST_NODE_CDAC2H

9U

CDD_ADC_TEST_NODE_CDAC2L

10U

CDD_ADC_TEST_NODE_CDAC3H

11U

CDD_ADC_TEST_NODE_CDAC3L

12U

CDD_ADC_TEST_NODE_CDAC4H

13U

CDD_ADC_TEST_NODE_CDAC4L

14U

CDD_ADC_TEST_NODE_CDAC5H

15U

CDD_ADC_TEST_NODE_CDAC5L

16U

CDD_ADC_TEST_NODE_CDAC6H

17U

CDD_ADC_TEST_NODE_CDAC6L

18U

CDD_ADC_TEST_NODE_CDAC7H

19U

CDD_ADC_TEST_NODE_CDAC7L

20U

CDD_ADC_TEST_NODE_CDAC8H

21U

CDD_ADC_TEST_NODE_CDAC8L

22U

CDD_ADC_TEST_NODE_CDAC9H

23U

CDD_ADC_TEST_NODE_CDAC9L

24U

CDD_ADC_TEST_NODE_CDAC10H

25U

CDD_ADC_TEST_NODE_CDAC10L

26U

CDD_ADC_TEST_NODE_CDAC11H

27U

CDD_ADC_TEST_NODE_CDAC11L

28U

CDD_ADC_TEST_NODE_ENZ_CALIB_GAIN_3P3

29U

CDD_ADC_TEST_NODE_MAX

Brief: Defines supported internal nodes that can be connected to ADC.

6.10.1.27. enum Cdd_Adc_OsDetectModeType

Enumerator

Value

Description

CDD_ADC_OSDETECT_MODE_DISABLED

0x0U

CDD_ADC_OSDETECT_MODE_VSSA

0x1U

CDD_ADC_OSDETECT_MODE_VDDA

0x2U

CDD_ADC_OSDETECT_MODE_5BY12_VDDA

0x3U

CDD_ADC_OSDETECT_MODE_7BY12_VDDA

0x4U

CDD_ADC_OSDETECT_MODE_5K_PULLDOWN_TO_VSSA

0x5U

CDD_ADC_OSDETECT_MODE_5K_PULLUP_TO_VDDA

0x6U

CDD_ADC_OSDETECT_MODE_7K_PULLDOWN_TO_VSSA

0x7U

Brief: Specifies open/short circuit modes.

6.10.1.28. typedef Cdd_Adc_GroupType

typedef uint8 Cdd_Adc_GroupType;

Brief: Numeric ID of an ADC channel group.

6.10.1.29. typedef Cdd_Adc_PpbType

typedef uint8 Cdd_Adc_PpbType;

Brief: Numeric ID of the PPB unit.

6.10.1.30. typedef Cdd_Adc_ValueGroupType

typedef uint16 Cdd_Adc_ValueGroupType;

Brief: Type for reading the converted values of a channel group.

6.10.1.31. typedef Cdd_Adc_StreamNumSampleType

typedef uint8 Cdd_Adc_StreamNumSampleType;

Brief: Type for configuring the number of channel conversions results in streaming access mode (in single access mode, parameter is 1)

6.10.1.32. typedef Cdd_Adc_CheckEvtType

typedef uint8 Cdd_Adc_CheckEvtType;

Brief: Specifies the checker event id.

6.10.1.33. typedef Cdd_Adc_GlbTrigType

typedef uint8 Cdd_Adc_GlbTrigType;

Brief: Specifies ID of the global software trigger

6.10.1.34. typedef Cdd_Adc_CheckerType

typedef uint8 Cdd_Adc_CheckerType;

Brief: Numeric ID of an ADC safety result checker.

6.10.1.35. typedef Cdd_Adc_CheckerIntEvtType

typedef uint8 Cdd_Adc_CheckerIntEvtType;

Brief: Numeric ID of a safety checker interrupt event instance.

6.10.1.36. typedef Cdd_Adc_HwUnitInstanceType

typedef uint8 Cdd_Adc_HwUnitInstanceType;

Brief: Hardware unit instance type.

6.10.1.37. typedef Cdd_Adc_GroupEndNotifyType

typedef void(* Cdd_Adc_GroupEndNotifyType) (void);

Brief: Group end notification function pointer.

6.10.1.38. typedef Cdd_Adc_PpbNotifyType

typedef void(* Cdd_Adc_PpbNotifyType) (void);

Brief: Ppb notification function pointer.

6.10.2. Structures

Name

Brief

Cdd_Adc_PpbValType

PPB value type.

Cdd_Adc_PpbUnitCfgType

PPB unit config type.

Cdd_Adc_ChannelCfgType

Channel config type.

Cdd_Adc_TrigRepCfgType

Trigger repeater config type.

Cdd_Adc_GroupCfgType

Group config type.

Cdd_Adc_HwUnitCfgType

Hardware unit config type.

Cdd_Adc_SelResCfgType

Select result config type.

Cdd_Adc_IntSrcType

Interrupt source type.

Cdd_Adc_CheckerResCfgType

Checker response config type.

Cdd_Adc_CheckerIntEvtCfgType

Checker interrupt event config type.

Cdd_Adc_CheckerCfgType

Checker config type.

Cdd_Adc_GlbSwCfgType

Global software config type.

Cdd_Adc_ConfigType

ADC config type.

6.10.3. Defines

Name

Brief

CDD_ADC_SW_MAJOR_VERSION

Driver Implementation Major Version.

CDD_ADC_SW_MINOR_VERSION

Driver Implementation Minor Version.

CDD_ADC_SW_PATCH_VERSION

Driver Implementation Patch Version.

CDD_ADC_AR_RELEASE_MAJOR_VERSION

AUTOSAR Major version specification implemented by CDD_ADC Driver.

CDD_ADC_AR_RELEASE_MINOR_VERSION

AUTOSAR Minor version specification implemented by CDD_ADC Driver.

CDD_ADC_AR_RELEASE_REVISION_VERSION

AUTOSAR Patch version specification implemented by CDD_ADC Driver.

CDD_ADC_VENDOR_ID

Texas Instruments Vendor ID.

CDD_ADC_MODULE_ID

CDD ADC Driver Module ID.

CDD_ADC_INSTANCE_ID

CDD ADC Instance ID.

CDD_ADC_E_UNINIT

API service used without module initialization.

CDD_ADC_E_BUSY

API service called during ongoing process/conversion.

CDD_ADC_E_IDLE

API service called while no conversion is ongoing.

CDD_ADC_E_ALREADY_INITIALIZED

API Cdd_Adc_Init service called while the ADC driver has already been initialized.

CDD_ADC_E_PARAM_EVENT

API service called with incorrect configuration parameter.

CDD_ADC_E_PARAM_POINTER

API service called with invalid data buffer pointer.

CDD_ADC_E_PARAM_GROUP

API service called with invalid group ID.

CDD_ADC_E_WRONG_RESOLUTION_MODE

API service called with invalid hardware unit ID.

CDD_ADC_E_WRONG_CONV_MODE

API service called on a group with conversion mode configured as continuous.

CDD_ADC_E_WRONG_TRIGG_SRC

API service called for group with wrong trigger source.

CDD_ADC_E_NOTIF_CAPABILITY

Enable/disable notification function for a group whose configuration set has no notification available.

CDD_ADC_E_BUFFER_UNINIT

Conversion started and result buffer pointer is not initialized.

CDD_ADC_E_CHECKER_IDLE

One or more ADC safety checker are IDLE.

CDD_ADC_E_CHECKER_BUSY

One or more ADC safety checker are BUSY.

CDD_ADC_E_ALREADY_SET

API service called when the resolution is already set to the requested resolution for the ADC instance.

CDD_ADC_E_INVALID_ID

API service called with invalid hardware unit ID.

CDD_ADC_E_INVALID_RESOLUTION

API service called with invalid resolution.

CDD_ADC_E_INVALID_INTERRUPT_ID

API service called with invalid interrupt ID.

CDD_ADC_E_WRONG_PROCESSING_MODE

API service called with invalid interrupt ID.

CDD_ADC_E_WRONG_TRIGG_TYPE

API service called for group with wrong trigger source type.

CDD_ADC_SID_INIT

Cdd_Adc_Init() API Service ID.

CDD_ADC_SID_DEINIT

Cdd_Adc_DeInit() API Service ID.

CDD_ADC_SID_START_GROUP_CONVERSION

Cdd_Adc_StartGroupConversion() API Service ID.

CDD_ADC_SID_STOP_GROUP_CONVERSION

Cdd_Adc_StopGroupConversion() API Service ID.

CDD_ADC_SID_READ_GROUP

Cdd_Adc_ReadGroup() API Service ID.

CDD_ADC_SID_ENABLE_HARDWARE_TRIGGER

Cdd_Adc_EnableHardwareTrigger() API Service ID.

CDD_ADC_SID_DISABLE_HARDWARE_TRIGGER

Cdd_Adc_DisableHardwareTrigger() API Service ID.

CDD_ADC_SID_ENABLE_GROUP_NOTIFICATION

Cdd_Adc_EnableGroupNotification() API Service ID.

CDD_ADC_SID_DISABLE_GROUP_NOTIFICATION

Cdd_Adc_DisableGroupNotification() API Service ID.

CDD_ADC_SID_GET_GRP_STATUS

Cdd_Adc_GetGroupStatus() API Service ID.

CDD_ADC_SID_GET_VERSION_INFO

Cdd_Adc_GetVersionInfo() API Service ID.

CDD_ADC_SID_GET_STREAM_LAST_POINTER

Cdd_Adc_GetStreamLastPointer() API Service ID.

CDD_ADC_SID_SETUP_RESULT_BUFFER

Cdd_Adc_SetupResultBuffer() API Service ID.

CDD_ADC_SID_START_RESULT_CHECKER

Cdd_Adc_StartResultChecker service ID.

CDD_ADC_SID_STOP_RESULT_CHECKER

Cdd_Adc_StopResultChecker API service ID.

CDD_ADC_SID_READ_RESULT_CHECKER

Cdd_Adc_ReadCheckerStatus API service ID.

CDD_ADC_SID_CLEAR_CHECKER_EVT

Cdd_Adc_ClearCheckerEvt API service ID.

CDD_ADC_SID_START_GLBSW_TRIG

Cdd_Adc_StartGlobalSwTrig service ID.

CDD_ADC_SID_STOP_GLBSW_TRIG

Cdd_Adc_StopGlobalSwTrig service ID.

CDD_ADC_SID_SET_RESOLUTION

Cdd_Adc_SetResolution() service ID.

CDD_ADC_SID_READ_PARTIAL_PPB_VALUE

Cdd_Adc_ReadPpbValue() service ID.

CDD_ADC_SID_READ_PPB_VALUE

Cdd_Adc_ReadPartialPpbValue() service ID.

CDD_ADC_SID_READ_PPB

Cdd_Adc_ReadPpb() service ID.

CDD_ADC_SID_CLEAR_PPB_EVT

Cdd_Adc_ClearPpbEvt() service ID.

CDD_ADC_SID_GET_DELAY_STAMP

Cdd_Adc_GetDelayStamp() service ID.

CDD_ADC_SID_GET_TEMPERATURE_C

Cdd_Adc_GetTemperatureC() service ID.

CDD_ADC_SID_GET_TEMPERATURE_K

Cdd_Adc_GetTemperatureK() service ID.

CDD_ADC_SID_INTERNAL_TEST_NODE

Cdd_Adc_SetInternalTestNode() service ID.

CDD_ADC_SID_UPDATE_STATUS_THROUGH_DMA

Cdd_Adc_UpdateStatus() service ID.

CDD_ADC_SID_CONFIGURE_PPB_NOTIFICATION

Cdd_Adc_EnablePpbNotification() API Service ID.

CDD_ADC_CFG_MAJOR_VERSION

CDD_ADC_CFG_MINOR_VERSION

CDD_ADC_CFG_PATCH_VERSION

CDD_ADC_PRE_COMPILE_VARIANT

CDD_ADC_CONFIG_PC

CDD_ADC_CHN_COUNT

CDD_ADC_MAX_HW_UNIT_COUNT

CDD_ADC_MAX_INT_COUNT

CDD_ADC_DEV_ERROR_DETECT

CDD_ADC_DEINIT_API

CDD_ADC_ENABLE_START_STOP_GROUP_API

CDD_ADC_GLBSW_TRIG_API

CDD_ADC_GLBSW_TRIG_CNT

CDD_ADC_GROUP_CNT

CDD_ADC_GRP_NOTIF_CAPABILITY_API

CDD_ADC_HW_CNT

CDD_ADC_HW_TRIGGER_API

CDD_ADC_ENABLE_PPB_API

CDD_ADC_LOCK_TEMPERATURE_SENSOR

CDD_ADC_OPEN_SHORT_DETECTION

CDD_ADC_PPB_CNT

CDD_ADC_READ_GROUP_API

CDD_ADC_SAFETY_CHECK_API

CDD_ADC_CHECKER_CNT

CDD_ADC_CHECKER_EVT_CNT

CDD_ADC_CHECKER_INTEVT_CNT

CDD_ADC_SET_RESOLUTION_API

CDD_ADC_TEMPERATURE_SENSOR_ENABLE

CDD_ADC_TRIG_REP_ENABLE

CDD_ADC_TRIG_REP_CNT

CDD_ADC_PPB_NOTIF_CAPABILITY_API

CDD_ADC_VERSION_INFO_API

CddAdcConf_CddAdcHwUnit_CddAdcHwUnit_0

CddAdcConf_CddAdcGroup_CddAdcGroup_0

CddAdcConf_CddAdcGroup_CddAdcGroup_1

CddAdcConf_CddAdcGroup_CddAdcGroup_2

CddAdcConf_CddAdcGroup_CddAdcGroup_3

CddAdcConf_CddAdcPpbConfig_CddAdcPpbConfig_0

CddAdcConf_CddAdcPpbConfig_CddAdcPpbConfig_1

CddAdcConf_CddAdcPpbConfig_CddAdcPpbConfig_2

CddAdcConf_CddAdcHwUnit_CddAdcHwUnit_1

CddAdcConf_CddAdcGroup_CddAdcGroup_4

CddAdcConf_CddAdcGroup_CddAdcGroup_5

CDD_ADC_EXTCHSEL_CAPABILITY

CDD_ADCA_INT1_ENABLE

CDD_ADCA_INT1_ISR_CAT1_RTINT

CDD_ADCA_INT2_ENABLE

CDD_ADCA_INT2_ISR_CAT1_INT

CDD_ADCA_INT3_ENABLE

CDD_ADCA_INT3_ISR_CAT2_INT

CDD_ADCA_INT4_ENABLE

CDD_ADCA_INT4_ISR_CAT1_INT

CDD_ADCA_EVTINT_ENABLE

CDD_ADCA_EVTINT_ISR_CAT1_INT

CDD_ADCD_INT1_ENABLE

CDD_ADCD_INT1_ISR_CAT1_INT

CDD_ADCD_INT2_ENABLE

CDD_ADCD_INT2_ISR_CAT1_INT

6.10.4. Functions

Return type

Function Name

Brief

void

Cdd_Adc_Init(const Cdd_Adc_ConfigType * CfgPtr)

Service to initialize Cdd Adc driver.

Std_ReturnType

Cdd_Adc_SetupResultBuffer(Cdd_Adc_GroupType Group, const Cdd_Adc_ValueGroupType * DataBufferPtr)

This service initializes ADC driver with the group specific result buffer start address where the conversion results will be stored.

void

Cdd_Adc_DeInit(void )

Service to deinitialize Cdd Adc driver.

void

Cdd_Adc_StartGroupConversion(Cdd_Adc_GroupType Group)

Service to start a group conversion.

void

Cdd_Adc_StopGroupConversion(Cdd_Adc_GroupType Group)

Service to stop a group conversion.

Std_ReturnType

Cdd_Adc_StartGlobalSwTrig(Cdd_Adc_GlbTrigType GlbSwTrig)

Service to start the global software trigger.

void

Cdd_Adc_StopGlobalSwTrig(Cdd_Adc_GlbTrigType GlbSwTrig)

Service to stop the global software trigger.

void

Cdd_Adc_EnableHardwareTrigger(Cdd_Adc_GroupType Group)

Service to enables the HW trigger for a group.

void

Cdd_Adc_DisableHardwareTrigger(Cdd_Adc_GroupType Group)

Service to disable the HW trigger for a group.

void

Cdd_Adc_EnableGroupNotification(Cdd_Adc_GroupType Group)

Service to enable the notification for a group.

void

Cdd_Adc_DisableGroupNotification(Cdd_Adc_GroupType Group)

Service to disable the notification for a group.

Cdd_Adc_StatusType

Cdd_Adc_GetGroupStatus(Cdd_Adc_GroupType Group)

Service to get the conversion status of the group.

Std_ReturnType

Cdd_Adc_ReadGroup(Cdd_Adc_GroupType Group, Cdd_Adc_ValueGroupType * DataBufferPtr)

service that reads the group conversion result of the last completed conversion round

Cdd_Adc_StreamNumSampleType

Cdd_Adc_GetStreamLastPointer(Cdd_Adc_GroupType Group, Cdd_Adc_ValueGroupType ** PtrToSamplePtr)

service that returns the number of valid samples per channel, stored in the result buffer.

void

Cdd_Adc_GetVersionInfo(Std_VersionInfoType * VersionInfo)

service that returns the version information of the module.

void

Cdd_Adc_StartResultChecker(Cdd_Adc_CheckerType CheckerId)

service to start the safety result checker.

void

Cdd_Adc_StopResultChecker(Cdd_Adc_CheckerType CheckerId)

service to stop the safety result checker.

void

Cdd_Adc_ReadCheckerStatus(Cdd_Adc_CheckerIntEvtType IntEvt, Cdd_Adc_CheckFlagStatusType * CheckerFlag)

service to get the safety checker status

void

Cdd_Adc_ClearCheckerEvt(Cdd_Adc_CheckerIntEvtType IntEvt, Cdd_Adc_CheckerEventType Event_Id)

service to clears the status flags for the specified event

Cdd_Adc_PpbValType

Cdd_Adc_ReadPpbValue(Cdd_Adc_PpbType PpbId)

service to get the PPB results

Cdd_Adc_PpbValType

Cdd_Adc_ReadPartialPpbValue(Cdd_Adc_PpbType PpbId)

service to get the partial PPB results

sint32

Cdd_Adc_ReadPpb(Cdd_Adc_PpbType PpbId)

service to get the PPB result of the specified PPB

void

Cdd_Adc_ClearPpbEvt(Cdd_Adc_PpbType PpbId)

service to clear the PPB event flags

uint16

Cdd_Adc_GetDelayStamp(Cdd_Adc_PpbType PpbId)

service to get the delay between the the SOC trigger and the actual start of the SOC acquisition

void

Cdd_Adc_ConfigurePpbNotification(Cdd_Adc_PpbType PpbId, boolean Mode)

Enable or disable PPB notification.

Std_ReturnType

Cdd_Adc_SetResolution(Cdd_Adc_HwUnitInstanceType HwUnit, Cdd_Adc_ResolutionType Resolution)

service to set the resolution of the ADC hardware unit.

sint16

Cdd_Adc_GetTemperatureC(Cdd_Adc_HwUnitInstanceType HwUnit, Cdd_Adc_ValueGroupType TempResult)

service to convert the ADC conversion value to Celsius.

sint16

Cdd_Adc_GetTemperatureK(Cdd_Adc_HwUnitInstanceType HwUnit, Cdd_Adc_ValueGroupType TempResult)

service to convert the ADC conversion value to Kelvin.

void

Cdd_Adc_SetInternalTestNode(Cdd_Adc_InternalTestNodeType TestNode)

service to set the internal test node

void

Cdd_Adc_UpdateStatusThroughDma(Cdd_Adc_HwUnitType HwUnitId, Cdd_Adc_IntNumType IntNum)

service to update the group status in DMA mode for the specified group

6.10.4.1. function Cdd_Adc_Init

void Cdd_Adc_Init(
    const Cdd_Adc_ConfigType * CfgPtr
)

Brief: Service to initialize Cdd Adc driver.

This service initializes all the ADC HW units and safety checker units (Cdd_Adc driver).

Parameters:

  • CfgPtr Pointer to configuration set (Varaint PC requires a NULL_PTR)

Returns:

  • None

Return: None

Postcondition: None

6.10.4.2. function Cdd_Adc_SetupResultBuffer

Std_ReturnType Cdd_Adc_SetupResultBuffer(
    Cdd_Adc_GroupType Group,
    const Cdd_Adc_ValueGroupType * DataBufferPtr
)

Brief: This service initializes ADC driver with the group specific result buffer start address where the conversion results will be stored.

This function initializes the group specific result buffer start address with the passed DataBufferPtr parameter where the conversion results will be stored. Note: The application has to ensure that the application buffer, where DataBufferPtr points to, can hold all the conversion results of the specified group. The initialization with Cdd_Adc_SetupResultBuffer is required after reset, before a group conversion can be started.

Parameters:

  • Group Numeric ID of requested ADC Channel group.

  • DataBufferPtr Pointer to result data buffer

Returns:

  • E_OK result buffer pointer initialized correctly

  • E_NOT_OK operation failed or development error occured

Return: Returns if the result buffer setup is successful.

Precondition: None

Postcondition: None

6.10.4.3. function Cdd_Adc_DeInit

void Cdd_Adc_DeInit(
    void 
)

Brief: Service to deinitialize Cdd Adc driver.

This service returns all ADC HW Units to a state comparable to their power on reset state.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.4. function Cdd_Adc_StartGroupConversion

void Cdd_Adc_StartGroupConversion(
    Cdd_Adc_GroupType Group
)

Brief: Service to start a group conversion.

This service starts the conversion of all channels of the requested ADC Channel group.

Parameters:

  • Group Numeric ID of requested ADC Channel group.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.5. function Cdd_Adc_StopGroupConversion

void Cdd_Adc_StopGroupConversion(
    Cdd_Adc_GroupType Group
)

Brief: Service to stop a group conversion.

This service Stops the conversion of the requested ADC Channel group

Parameters:

  • Group Numeric ID of requested ADC Channel group.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.6. function Cdd_Adc_StartGlobalSwTrig

Std_ReturnType Cdd_Adc_StartGlobalSwTrig(
    Cdd_Adc_GlbTrigType GlbSwTrig
)

Brief: Service to start the global software trigger.

This service starts global software trigger and returns E_OK if it is successful.

Parameters:

  • GlbSwTrig Numeric ID of global software trigger configuration.

Returns:

  • E_OK - If the global software trigger is configured successfully E_NOT_OK - If the global software trigger is not configured

Return: Return whether the global software trigger is configured or not

Precondition: None

Postcondition: None

6.10.4.7. function Cdd_Adc_StopGlobalSwTrig

void Cdd_Adc_StopGlobalSwTrig(
    Cdd_Adc_GlbTrigType GlbSwTrig
)

Brief: Service to stop the global software trigger.

This service stops global software trigger.

Parameters:

  • GlbSwTrig Numeric ID of global software trigger configuration.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.8. function Cdd_Adc_EnableHardwareTrigger

void Cdd_Adc_EnableHardwareTrigger(
    Cdd_Adc_GroupType Group
)

Brief: Service to enables the HW trigger for a group.

This service enableS the HW trigger source for the requested ADC channel group.

Parameters:

  • Group Numeric ID of requested ADC Channel group.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.9. function Cdd_Adc_DisableHardwareTrigger

void Cdd_Adc_DisableHardwareTrigger(
    Cdd_Adc_GroupType Group
)

Brief: Service to disable the HW trigger for a group.

This service disables the hardware trigger for the requested ADC Channel group.

Parameters:

  • Group Numeric ID of requested ADC Channel group.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.10. function Cdd_Adc_EnableGroupNotification

void Cdd_Adc_EnableGroupNotification(
    Cdd_Adc_GroupType Group
)

Brief: Service to enable the notification for a group.

This service enables the notification mechanism for the requested ADC Channel group.

Parameters:

  • Group Numeric ID of requested ADC Channel group.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.11. function Cdd_Adc_DisableGroupNotification

void Cdd_Adc_DisableGroupNotification(
    Cdd_Adc_GroupType Group
)

Brief: Service to disable the notification for a group.

This service disables the notification mechanism for the requested ADC Channel group.

Parameters:

  • Group Numeric ID of requested ADC Channel group.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.12. function Cdd_Adc_GetGroupStatus

Cdd_Adc_StatusType Cdd_Adc_GetGroupStatus(
    Cdd_Adc_GroupType Group
)

Brief: Service to get the conversion status of the group.

This service returns the conversion status of the requested ADC Channel group.

Parameters:

  • Group Numeric ID of requested ADC Channel group.

Returns:

  • Cdd_Adc_StatusType CDD_ADC_IDLE: The conversion of the specified group has not been started CDD_ADC_BUSY: The conversion of the specified group has been started and is still going on CDD_ADC_COMPLETED: A conversion round of the specified group has been finished. CDD_ADC_STREAM_COMPLETED: The result buffer is completely filled.

Return: Returns the conversion status of the group

Precondition: None

Postcondition: None

6.10.4.13. function Cdd_Adc_ReadGroup

Std_ReturnType Cdd_Adc_ReadGroup(
    Cdd_Adc_GroupType Group,
    Cdd_Adc_ValueGroupType * DataBufferPtr
)

Brief: service that reads the group conversion result of the last completed conversion round

This service reads the group conversion result of the last completed conversion round of the requested group and stores the channel values starting at the DataBufferPtr address. The group channel values are stored in ascending channel number order (in contrast to the storage layout of the result buffer ifstreaming access is configured).

Parameters:

  • Group Numeric ID of requested ADC Channel group.

  • DataBufferPtr Results of all channels of the group are stored where this pointer points to.

Returns:

  • E_OK Results are available and written to the data buffer

  • E_NOT_OK No results are available or development error occured

Return: Returns if the results are available or not.

Precondition: None

Postcondition: None

6.10.4.14. function Cdd_Adc_GetStreamLastPointer

Cdd_Adc_StreamNumSampleType Cdd_Adc_GetStreamLastPointer(
    Cdd_Adc_GroupType Group,
    Cdd_Adc_ValueGroupType ** PtrToSamplePtr
)

Brief: service that returns the number of valid samples per channel, stored in the result buffer.

This service returns the number of valid samples per channel, stored in the result buffer. Reads a pointer, pointing to a position in the group result buffer. With the pointer position, the results of all groupchannels of the last completed conversion round can be accessed .With the pointer and the return value, all valid group conversion results can be accessed (the user has to take the layout of the result buffer into account).

Parameters:

  • Group Numeric ID of requested ADC Channel group.

  • PtrToSamplePtr Pointer to result buffer pointer.

Returns:

  • Returns the number of valid samples available for the group

Return: Returns the number of valid samples per channel

Precondition: None

Postcondition: None

6.10.4.15. function Cdd_Adc_GetVersionInfo

void Cdd_Adc_GetVersionInfo(
    Std_VersionInfoType * VersionInfo
)

Brief: service that returns the version information of the module.

This service returns the version information of the Adc module.

Parameters:

  • VersionInfo Pointer to where to store the version information of this module

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.16. function Cdd_Adc_StartResultChecker

void Cdd_Adc_StartResultChecker(
    Cdd_Adc_CheckerType CheckerId
)

Brief: service to start the safety result checker.

This service starts the requested safety result checker unit.

Parameters:

  • CheckerId Numeric ID of the result safety checker unit

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.17. function Cdd_Adc_StopResultChecker

void Cdd_Adc_StopResultChecker(
    Cdd_Adc_CheckerType CheckerId
)

Brief: service to stop the safety result checker.

This service stops the requested safety result checker unit.

Parameters:

  • CheckerId Numeric ID of the result safety checker unit

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.18. function Cdd_Adc_ReadCheckerStatus

void Cdd_Adc_ReadCheckerStatus(
    Cdd_Adc_CheckerIntEvtType IntEvt,
    Cdd_Adc_CheckFlagStatusType * CheckerFlag
)

Brief: service to get the safety checker status

This service returns the safety checker status and clears the interrupt flags. This API needs to be called inside ESM ISR. This shouldn’t be called directly.

Parameters:

  • IntEvt is the numeric ID of the interrupt event instance ID

  • CheckerFlag Pointer to the array of the status flag

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.19. function Cdd_Adc_ClearCheckerEvt

void Cdd_Adc_ClearCheckerEvt(
    Cdd_Adc_CheckerIntEvtType IntEvt,
    Cdd_Adc_CheckerEventType Event_Id
)

Brief: service to clears the status flags for the specified event

This service clears the safety checker status flags that generated the specified event from the specified interrupt event instance

Parameters:

  • IntEvt is the numeric ID of the interrupt event instance ID

  • Event_Id is the numeric ID of the event

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.20. function Cdd_Adc_ReadPpbValue

Cdd_Adc_PpbValType Cdd_Adc_ReadPpbValue(
    Cdd_Adc_PpbType PpbId
)

Brief: service to get the PPB results

This service returns the PPB results among multiple conversion results of the specified PPB

Parameters:

  • PpbId Numeric ID of the PPB unit

Returns:

  • Cdd_Adc_PpbValType structure

Return: Returns a structure with final PPB min,max,sum,min index,max index and count values

Precondition: None

Postcondition: None

6.10.4.21. function Cdd_Adc_ReadPartialPpbValue

Cdd_Adc_PpbValType Cdd_Adc_ReadPartialPpbValue(
    Cdd_Adc_PpbType PpbId
)

Brief: service to get the partial PPB results

This service returns the partial PPB results among multiple conversion results of the specified PPB

Parameters:

  • PpbId Numeric ID of the PPB unit

Returns:

  • Cdd_Adc_PpbValType structure

Return: Returns a structure with partial PPB min,max,sum,min index,max index and count values

Precondition: None

Postcondition: None

6.10.4.22. function Cdd_Adc_ReadPpb

sint32 Cdd_Adc_ReadPpb(
    Cdd_Adc_PpbType PpbId
)

Brief: service to get the PPB result of the specified PPB

This service returns the the PPB result of the specified PPB

Parameters:

  • PpbId Numeric ID of the PPB unit

Returns:

  • sint32 signed 32bit value

Return: Returns the ppb result register value

Precondition: None

Postcondition: None

6.10.4.23. function Cdd_Adc_ClearPpbEvt

void Cdd_Adc_ClearPpbEvt(
    Cdd_Adc_PpbType PpbId
)

Brief: service to clear the PPB event flags

This service clears the event flags of the specified PPB results

Parameters:

  • PpbId Numeric ID of the PPB unit

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.24. function Cdd_Adc_GetDelayStamp

uint16 Cdd_Adc_GetDelayStamp(
    Cdd_Adc_PpbType PpbId
)

Brief: service to get the delay between the the SOC trigger and the actual start of the SOC acquisition

This service returns the delay between the the SOC trigger and the actual start of the SOC acquisition of the specified PPB in SYSCLK cycles.

Parameters:

  • PpbId Numeric ID of the PPB unit

Returns:

  • uint16 - Max value is 4095, if the delay exceeds 4096 SYSCLK cycles it overflows

Return: Number of SYSCLK cycles between the trigger and the actual sampling of the SOC linked to the specified PPB.

Precondition: None

Postcondition: None

6.10.4.25. function Cdd_Adc_ConfigurePpbNotification

void Cdd_Adc_ConfigurePpbNotification(
    Cdd_Adc_PpbType PpbId,
    boolean Mode
)

Brief: Enable or disable PPB notification.

This service enables or disables PPB notification for the specified PPB

Parameters:

  • PpbId Numeric ID of the PPB unit

  • Mode Enable/disable select

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.26. function Cdd_Adc_SetResolution

Std_ReturnType Cdd_Adc_SetResolution(
    Cdd_Adc_HwUnitInstanceType HwUnit,
    Cdd_Adc_ResolutionType Resolution
)

Brief: service to set the resolution of the ADC hardware unit.

This service to set the resolution of the specified ADC hardware unit.

Parameters:

  • HwUnit Instance ID of the specified ADC Hw Unit

  • Resolution Resolution to be set for the ADC Hw Unit

Returns:

  • E_OK Resolution update successfully E_NOT_OK: Resolution update failed

Return: Returns if the resolution update is successful.

Precondition: None

Postcondition: None

6.10.4.27. function Cdd_Adc_GetTemperatureC

sint16 Cdd_Adc_GetTemperatureC(
    Cdd_Adc_HwUnitInstanceType HwUnit,
    Cdd_Adc_ValueGroupType TempResult
)

Brief: service to convert the ADC conversion value to Celsius.

This service to convert the ADC conversion value to Celsius.

Parameters:

  • HwUnit ADC hardware unit

  • TempResult ADC conversion result

Returns:

  • sint16 - Value after the result is converted to Celsius

Return: Returns the values converted to Celsius

Precondition: None

Postcondition: None

6.10.4.28. function Cdd_Adc_GetTemperatureK

sint16 Cdd_Adc_GetTemperatureK(
    Cdd_Adc_HwUnitInstanceType HwUnit,
    Cdd_Adc_ValueGroupType TempResult
)

Brief: service to convert the ADC conversion value to Kelvin.

This service to convert the ADC conversion value to Kelvin.

Parameters:

  • HwUnit ADC hardware unit

  • TempResult ADC conversion result

Returns:

  • sint16 - Value after the result is converted to Kelvin

Return: Returns the values converted to Kelvin

Precondition: None

Postcondition: None

6.10.4.29. function Cdd_Adc_SetInternalTestNode

void Cdd_Adc_SetInternalTestNode(
    Cdd_Adc_InternalTestNodeType TestNode
)

Brief: service to set the internal test node

This service to set the internal test node for all the hardware units

Parameters:

  • TestNode Internal test node

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

6.10.4.30. function Cdd_Adc_UpdateStatusThroughDma

void Cdd_Adc_UpdateStatusThroughDma(
    Cdd_Adc_HwUnitType HwUnitId,
    Cdd_Adc_IntNumType IntNum
)

Brief: service to update the group status in DMA mode for the specified group

This service to update the group status in DMA mode for the specified group

Parameters:

  • IntNum Interrupt ID of the ADC instance

  • HwUnitId ADC instance ID

Returns:

  • None

Return: None

Precondition: None

Postcondition: None